HFXO_TypeDef Struct ReferenceDevices > HFXO

HFXO Register Declaration.

Definition at line 46 of file efr32bg21_hfxo.h.

#include <efr32bg21_hfxo.h>

Data Fields

__IOM uint32_t CFG
 
__IOM uint32_t CFG_CLR
 
__IOM uint32_t CFG_SET
 
__IOM uint32_t CFG_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
uint32_t RESERVED0 [3U]
 
uint32_t RESERVED1 [1U]
 
uint32_t RESERVED10 [1U]
 
uint32_t RESERVED11 [1U]
 
uint32_t RESERVED12 [1U]
 
uint32_t RESERVED13 [9U]
 
uint32_t RESERVED14 [1U]
 
uint32_t RESERVED15 [5U]
 
uint32_t RESERVED16 [2U]
 
uint32_t RESERVED17 [991U]
 
uint32_t RESERVED18 [3U]
 
uint32_t RESERVED19 [1U]
 
uint32_t RESERVED2 [1U]
 
uint32_t RESERVED20 [1U]
 
uint32_t RESERVED21 [1U]
 
uint32_t RESERVED22 [9U]
 
uint32_t RESERVED23 [1U]
 
uint32_t RESERVED24 [5U]
 
uint32_t RESERVED25 [2U]
 
uint32_t RESERVED26 [991U]
 
uint32_t RESERVED27 [3U]
 
uint32_t RESERVED28 [1U]
 
uint32_t RESERVED29 [1U]
 
uint32_t RESERVED3 [1U]
 
uint32_t RESERVED30 [1U]
 
uint32_t RESERVED31 [9U]
 
uint32_t RESERVED32 [1U]
 
uint32_t RESERVED33 [5U]
 
uint32_t RESERVED34 [2U]
 
uint32_t RESERVED4 [9U]
 
uint32_t RESERVED5 [1U]
 
uint32_t RESERVED6 [5U]
 
uint32_t RESERVED7 [2U]
 
uint32_t RESERVED8 [991U]
 
uint32_t RESERVED9 [3U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t XTALCFG
 
__IOM uint32_t XTALCFG_CLR
 
__IOM uint32_t XTALCFG_SET
 
__IOM uint32_t XTALCFG_TGL
 
__IOM uint32_t XTALCTRL
 
__IOM uint32_t XTALCTRL_CLR
 
__IOM uint32_t XTALCTRL_SET
 
__IOM uint32_t XTALCTRL_TGL
 

Field Documentation

__IOM uint32_t HFXO_TypeDef::CFG

Configuration Register

Definition at line 53 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CFG_CLR

Configuration Register

Definition at line 91 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CFG_SET

Configuration Register

Definition at line 72 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CFG_TGL

Configuration Register

Definition at line 110 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CMD

Command Register

Definition at line 57 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CMD_CLR

Command Register

Definition at line 95 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CMD_SET

Command Register

Definition at line 76 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CMD_TGL

Command Register

Definition at line 114 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CTRL

Control Register

Definition at line 55 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CTRL_CLR

Control Register

Definition at line 93 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CTRL_SET

Control Register

Definition at line 74 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::CTRL_TGL

Control Register

Definition at line 112 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IEN

Interrupt Enable Register

Definition at line 62 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 100 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 81 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 119 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IF

Interrupt Flag Register

Definition at line 61 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 99 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 80 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 118 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::IPVERSION

IP version ID

Definition at line 47 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::IPVERSION_CLR

IP version ID

Definition at line 85 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::IPVERSION_SET

IP version ID

Definition at line 66 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::IPVERSION_TGL

IP version ID

Definition at line 104 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::LOCK

Configuration Lock Register

Definition at line 64 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::LOCK_CLR

Configuration Lock Register

Definition at line 102 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::LOCK_SET

Configuration Lock Register

Definition at line 83 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::LOCK_TGL

Configuration Lock Register

Definition at line 121 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED0[3U]

Reserved for future use

Definition at line 48 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED1[1U]

Reserved for future use

Definition at line 50 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED10[1U]

Reserved for future use

Definition at line 69 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED11[1U]

Reserved for future use

Definition at line 71 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED12[1U]

Reserved for future use

Definition at line 73 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED13[9U]

Reserved for future use

Definition at line 75 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED14[1U]

Reserved for future use

Definition at line 77 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED15[5U]

Reserved for future use

Definition at line 79 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED16[2U]

Reserved for future use

Definition at line 82 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED17[991U]

Reserved for future use

Definition at line 84 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED18[3U]

Reserved for future use

Definition at line 86 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED19[1U]

Reserved for future use

Definition at line 88 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED2[1U]

Reserved for future use

Definition at line 52 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED20[1U]

Reserved for future use

Definition at line 90 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED21[1U]

Reserved for future use

Definition at line 92 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED22[9U]

Reserved for future use

Definition at line 94 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED23[1U]

Reserved for future use

Definition at line 96 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED24[5U]

Reserved for future use

Definition at line 98 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED25[2U]

Reserved for future use

Definition at line 101 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED26[991U]

Reserved for future use

Definition at line 103 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED27[3U]

Reserved for future use

Definition at line 105 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED28[1U]

Reserved for future use

Definition at line 107 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED29[1U]

Reserved for future use

Definition at line 109 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED3[1U]

Reserved for future use

Definition at line 54 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED30[1U]

Reserved for future use

Definition at line 111 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED31[9U]

Reserved for future use

Definition at line 113 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED32[1U]

Reserved for future use

Definition at line 115 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED33[5U]

Reserved for future use

Definition at line 117 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED34[2U]

Reserved for future use

Definition at line 120 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED4[9U]

Reserved for future use

Definition at line 56 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED5[1U]

Reserved for future use

Definition at line 58 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED6[5U]

Reserved for future use

Definition at line 60 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED7[2U]

Reserved for future use

Definition at line 63 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED8[991U]

Reserved for future use

Definition at line 65 of file efr32bg21_hfxo.h.

uint32_t HFXO_TypeDef::RESERVED9[3U]

Reserved for future use

Definition at line 67 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::STATUS

Status Register

Definition at line 59 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::STATUS_CLR

Status Register

Definition at line 97 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::STATUS_SET

Status Register

Definition at line 78 of file efr32bg21_hfxo.h.

__IM uint32_t HFXO_TypeDef::STATUS_TGL

Status Register

Definition at line 116 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCFG

Crystal Configuration Register

Definition at line 49 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCFG_CLR

Crystal Configuration Register

Definition at line 87 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCFG_SET

Crystal Configuration Register

Definition at line 68 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCFG_TGL

Crystal Configuration Register

Definition at line 106 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCTRL

Crystal Control Register

Definition at line 51 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCTRL_CLR

Crystal Control Register

Definition at line 89 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCTRL_SET

Crystal Control Register

Definition at line 70 of file efr32bg21_hfxo.h.

__IOM uint32_t HFXO_TypeDef::XTALCTRL_TGL

Crystal Control Register

Definition at line 108 of file efr32bg21_hfxo.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_hfxo.h