IADC_CFG_TypeDef Struct ReferenceDevices > IADC

IADC CFG Register Group Declaration.

Definition at line 46 of file efr32bg21_iadc.h.

#include <efr32bg21_iadc.h>

Data Fields

__IOM uint32_t CFG
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t SCALE
 
__IOM uint32_t SCHED
 

Field Documentation

__IOM uint32_t IADC_CFG_TypeDef::CFG

Configuration

Definition at line 47 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().

uint32_t IADC_CFG_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 48 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_CFG_TypeDef::SCALE

Scaling

Definition at line 49 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().

__IOM uint32_t IADC_CFG_TypeDef::SCHED

Scheduling

Definition at line 50 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_iadc.h