IADC_TypeDef Struct ReferenceDevices > IADC

IADC Register Declaration.

Definition at line 59 of file efr32bg21_iadc.h.

#include <efr32bg21_iadc.h>

Data Fields

IADC_CFG_TypeDef CFG [2U]
 
IADC_CFG_TypeDef CFG_CLR [2U]
 
IADC_CFG_TypeDef CFG_SET [2U]
 
IADC_CFG_TypeDef CFG_TGL [2U]
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CMPTHR
 
__IOM uint32_t CMPTHR_CLR
 
__IOM uint32_t CMPTHR_SET
 
__IOM uint32_t CMPTHR_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t MASKREQ
 
__IOM uint32_t MASKREQ_CLR
 
__IOM uint32_t MASKREQ_SET
 
__IOM uint32_t MASKREQ_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [5U]
 
uint32_t RESERVED10 [5U]
 
uint32_t RESERVED11 [2U]
 
uint32_t RESERVED12 [1U]
 
uint32_t RESERVED13 [1U]
 
uint32_t RESERVED14 [1U]
 
uint32_t RESERVED15 [4U]
 
uint32_t RESERVED16 [1U]
 
uint32_t RESERVED17 [963U]
 
uint32_t RESERVED18 [1U]
 
uint32_t RESERVED19 [5U]
 
uint32_t RESERVED2 [2U]
 
uint32_t RESERVED20 [2U]
 
uint32_t RESERVED21 [1U]
 
uint32_t RESERVED22 [1U]
 
uint32_t RESERVED23 [1U]
 
uint32_t RESERVED24 [4U]
 
uint32_t RESERVED25 [1U]
 
uint32_t RESERVED26 [963U]
 
uint32_t RESERVED27 [1U]
 
uint32_t RESERVED28 [5U]
 
uint32_t RESERVED29 [2U]
 
uint32_t RESERVED3 [1U]
 
uint32_t RESERVED30 [1U]
 
uint32_t RESERVED31 [1U]
 
uint32_t RESERVED32 [1U]
 
uint32_t RESERVED33 [4U]
 
uint32_t RESERVED34 [1U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [1U]
 
uint32_t RESERVED6 [4U]
 
uint32_t RESERVED7 [1U]
 
uint32_t RESERVED8 [963U]
 
uint32_t RESERVED9 [1U]
 
__IM uint32_t SCANDATA
 
__IM uint32_t SCANDATA_CLR
 
__IM uint32_t SCANDATA_SET
 
__IM uint32_t SCANDATA_TGL
 
__IOM uint32_t SCANFIFOCFG
 
__IOM uint32_t SCANFIFOCFG_CLR
 
__IOM uint32_t SCANFIFOCFG_SET
 
__IOM uint32_t SCANFIFOCFG_TGL
 
__IM uint32_t SCANFIFODATA
 
__IM uint32_t SCANFIFODATA_CLR
 
__IM uint32_t SCANFIFODATA_SET
 
__IM uint32_t SCANFIFODATA_TGL
 
__IM uint32_t SCANFIFOSTAT
 
__IM uint32_t SCANFIFOSTAT_CLR
 
__IM uint32_t SCANFIFOSTAT_SET
 
__IM uint32_t SCANFIFOSTAT_TGL
 
IADC_SCANTABLE_TypeDef SCANTABLE [16U]
 
IADC_SCANTABLE_TypeDef SCANTABLE_CLR [16U]
 
IADC_SCANTABLE_TypeDef SCANTABLE_SET [16U]
 
IADC_SCANTABLE_TypeDef SCANTABLE_TGL [16U]
 
__IOM uint32_t SINGLE
 
__IOM uint32_t SINGLE_CLR
 
__IOM uint32_t SINGLE_SET
 
__IOM uint32_t SINGLE_TGL
 
__IM uint32_t SINGLEDATA
 
__IM uint32_t SINGLEDATA_CLR
 
__IM uint32_t SINGLEDATA_SET
 
__IM uint32_t SINGLEDATA_TGL
 
__IOM uint32_t SINGLEFIFOCFG
 
__IOM uint32_t SINGLEFIFOCFG_CLR
 
__IOM uint32_t SINGLEFIFOCFG_SET
 
__IOM uint32_t SINGLEFIFOCFG_TGL
 
__IM uint32_t SINGLEFIFODATA
 
__IM uint32_t SINGLEFIFODATA_CLR
 
__IM uint32_t SINGLEFIFODATA_SET
 
__IM uint32_t SINGLEFIFODATA_TGL
 
__IM uint32_t SINGLEFIFOSTAT
 
__IM uint32_t SINGLEFIFOSTAT_CLR
 
__IM uint32_t SINGLEFIFOSTAT_SET
 
__IM uint32_t SINGLEFIFOSTAT_TGL
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IM uint32_t STMASK
 
__IM uint32_t STMASK_CLR
 
__IM uint32_t STMASK_SET
 
__IM uint32_t STMASK_TGL
 
__IOM uint32_t TIMER
 
__IOM uint32_t TIMER_CLR
 
__IOM uint32_t TIMER_SET
 
__IOM uint32_t TIMER_TGL
 
__IOM uint32_t TRIGGER
 
__IOM uint32_t TRIGGER_CLR
 
__IOM uint32_t TRIGGER_SET
 
__IOM uint32_t TRIGGER_TGL
 

Field Documentation

IADC_CFG_TypeDef IADC_TypeDef::CFG[2U]

CFG

Definition at line 74 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().

IADC_CFG_TypeDef IADC_TypeDef::CFG_CLR[2U]

CFG

Definition at line 138 of file efr32bg21_iadc.h.

IADC_CFG_TypeDef IADC_TypeDef::CFG_SET[2U]

CFG

Definition at line 106 of file efr32bg21_iadc.h.

IADC_CFG_TypeDef IADC_TypeDef::CFG_TGL[2U]

CFG

Definition at line 170 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CMD

Command

Definition at line 63 of file efr32bg21_iadc.h.

Referenced by IADC_command(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::CMD_CLR

Command

Definition at line 127 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CMD_SET

Command

Definition at line 95 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CMD_TGL

Command

Definition at line 159 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CMPTHR

Digital Window comparator Threshold

Definition at line 68 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::CMPTHR_CLR

Digital Window comparator Threshold

Definition at line 132 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CMPTHR_SET

Digital Window comparator Threshold

Definition at line 100 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CMPTHR_TGL

Digital Window comparator Threshold

Definition at line 164 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CTRL

Control

Definition at line 62 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::CTRL_CLR

Control

Definition at line 126 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CTRL_SET

Control

Definition at line 94 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::CTRL_TGL

Control

Definition at line 158 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::EN

Enable

Definition at line 61 of file efr32bg21_iadc.h.

Referenced by IADC_setScanMask(), IADC_updateScanEntry(), and IADC_updateSingleInput().

__IOM uint32_t IADC_TypeDef::EN_CLR

Enable

Definition at line 125 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::EN_SET

Enable

Definition at line 93 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::EN_TGL

Enable

Definition at line 157 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::IEN

Interrupt Enable

Definition at line 70 of file efr32bg21_iadc.h.

Referenced by IADC_disableInt(), IADC_enableInt(), and IADC_getEnabledInt().

__IOM uint32_t IADC_TypeDef::IEN_CLR

Interrupt Enable

Definition at line 134 of file efr32bg21_iadc.h.

Referenced by IADC_disableInt().

__IOM uint32_t IADC_TypeDef::IEN_SET

Interrupt Enable

Definition at line 102 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::IEN_TGL

Interrupt Enable

Definition at line 166 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::IF

Interrupt Flags

Definition at line 69 of file efr32bg21_iadc.h.

Referenced by IADC_getEnabledInt(), and IADC_getInt().

__IOM uint32_t IADC_TypeDef::IF_CLR

Interrupt Flags

Definition at line 133 of file efr32bg21_iadc.h.

Referenced by IADC_clearInt().

__IOM uint32_t IADC_TypeDef::IF_SET

Interrupt Flags

Definition at line 101 of file efr32bg21_iadc.h.

Referenced by IADC_setInt().

__IOM uint32_t IADC_TypeDef::IF_TGL

Interrupt Flags

Definition at line 165 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::IPVERSION

IPVERSION

Definition at line 60 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::IPVERSION_CLR

IPVERSION

Definition at line 124 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::IPVERSION_SET

IPVERSION

Definition at line 92 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::IPVERSION_TGL

IPVERSION

Definition at line 156 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::MASKREQ

Mask Request

Definition at line 66 of file efr32bg21_iadc.h.

Referenced by IADC_initScan(), IADC_reset(), and IADC_setScanMask().

__IOM uint32_t IADC_TypeDef::MASKREQ_CLR

Mask Request

Definition at line 130 of file efr32bg21_iadc.h.

Referenced by IADC_updateScanEntry().

__IOM uint32_t IADC_TypeDef::MASKREQ_SET

Mask Request

Definition at line 98 of file efr32bg21_iadc.h.

Referenced by IADC_updateScanEntry().

__IOM uint32_t IADC_TypeDef::MASKREQ_TGL

Mask Request

Definition at line 162 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 72 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED1[5U]

Reserved for future use

Definition at line 73 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED10[5U]

Reserved for future use

Definition at line 105 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED11[2U]

Reserved for future use

Definition at line 107 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED12[1U]

Reserved for future use

Definition at line 116 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED13[1U]

Reserved for future use

Definition at line 117 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED14[1U]

Reserved for future use

Definition at line 119 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED15[4U]

Reserved for future use

Definition at line 121 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED16[1U]

Reserved for future use

Definition at line 122 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED17[963U]

Reserved for future use

Definition at line 123 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED18[1U]

Reserved for future use

Definition at line 136 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED19[5U]

Reserved for future use

Definition at line 137 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED2[2U]

Reserved for future use

Definition at line 75 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED20[2U]

Reserved for future use

Definition at line 139 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED21[1U]

Reserved for future use

Definition at line 148 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED22[1U]

Reserved for future use

Definition at line 149 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED23[1U]

Reserved for future use

Definition at line 151 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED24[4U]

Reserved for future use

Definition at line 153 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED25[1U]

Reserved for future use

Definition at line 154 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED26[963U]

Reserved for future use

Definition at line 155 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED27[1U]

Reserved for future use

Definition at line 168 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED28[5U]

Reserved for future use

Definition at line 169 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED29[2U]

Reserved for future use

Definition at line 171 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED3[1U]

Reserved for future use

Definition at line 84 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED30[1U]

Reserved for future use

Definition at line 180 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED31[1U]

Reserved for future use

Definition at line 181 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED32[1U]

Reserved for future use

Definition at line 183 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED33[4U]

Reserved for future use

Definition at line 185 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED34[1U]

Reserved for future use

Definition at line 186 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 85 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED5[1U]

Reserved for future use

Definition at line 87 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED6[4U]

Reserved for future use

Definition at line 89 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED7[1U]

Reserved for future use

Definition at line 90 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED8[963U]

Reserved for future use

Definition at line 91 of file efr32bg21_iadc.h.

uint32_t IADC_TypeDef::RESERVED9[1U]

Reserved for future use

Definition at line 104 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANDATA

Scan Data

Definition at line 83 of file efr32bg21_iadc.h.

Referenced by IADC_readScanData(), and IADC_readScanResult().

__IM uint32_t IADC_TypeDef::SCANDATA_CLR

Scan Data

Definition at line 147 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANDATA_SET

Scan Data

Definition at line 115 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANDATA_TGL

Scan Data

Definition at line 179 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SCANFIFOCFG

Scan FIFO Configuration

Definition at line 80 of file efr32bg21_iadc.h.

Referenced by IADC_initScan(), IADC_pullScanFifoResult(), IADC_readScanResult(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::SCANFIFOCFG_CLR

Scan FIFO Configuration

Definition at line 144 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SCANFIFOCFG_SET

Scan FIFO Configuration

Definition at line 112 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SCANFIFOCFG_TGL

Scan FIFO Configuration

Definition at line 176 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANFIFODATA

Scan FIFO Read Data

Definition at line 81 of file efr32bg21_iadc.h.

Referenced by IADC_pullScanFifoData(), and IADC_pullScanFifoResult().

__IM uint32_t IADC_TypeDef::SCANFIFODATA_CLR

Scan FIFO Read Data

Definition at line 145 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANFIFODATA_SET

Scan FIFO Read Data

Definition at line 113 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANFIFODATA_TGL

Scan FIFO Read Data

Definition at line 177 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANFIFOSTAT

Scan FIFO Status

Definition at line 82 of file efr32bg21_iadc.h.

Referenced by IADC_getScanFifoCnt().

__IM uint32_t IADC_TypeDef::SCANFIFOSTAT_CLR

Scan FIFO Status

Definition at line 146 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANFIFOSTAT_SET

Scan FIFO Status

Definition at line 114 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SCANFIFOSTAT_TGL

Scan FIFO Status

Definition at line 178 of file efr32bg21_iadc.h.

IADC_SCANTABLE_TypeDef IADC_TypeDef::SCANTABLE[16U]

SCANTABLE

Definition at line 88 of file efr32bg21_iadc.h.

Referenced by IADC_initScan(), IADC_reset(), and IADC_updateScanEntry().

IADC_SCANTABLE_TypeDef IADC_TypeDef::SCANTABLE_CLR[16U]

SCANTABLE

Definition at line 152 of file efr32bg21_iadc.h.

IADC_SCANTABLE_TypeDef IADC_TypeDef::SCANTABLE_SET[16U]

SCANTABLE

Definition at line 120 of file efr32bg21_iadc.h.

IADC_SCANTABLE_TypeDef IADC_TypeDef::SCANTABLE_TGL[16U]

SCANTABLE

Definition at line 184 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SINGLE

Single Queue Port Selection

Definition at line 86 of file efr32bg21_iadc.h.

Referenced by IADC_reset(), and IADC_updateSingleInput().

__IOM uint32_t IADC_TypeDef::SINGLE_CLR

Single Queue Port Selection

Definition at line 150 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SINGLE_SET

Single Queue Port Selection

Definition at line 118 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SINGLE_TGL

Single Queue Port Selection

Definition at line 182 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEDATA

Single Data

Definition at line 79 of file efr32bg21_iadc.h.

Referenced by IADC_readSingleData(), and IADC_readSingleResult().

__IM uint32_t IADC_TypeDef::SINGLEDATA_CLR

Single Data

Definition at line 143 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEDATA_SET

Single Data

Definition at line 111 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEDATA_TGL

Single Data

Definition at line 175 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SINGLEFIFOCFG

Single FIFO Configuration

Definition at line 76 of file efr32bg21_iadc.h.

Referenced by IADC_initSingle(), IADC_pullSingleFifoResult(), IADC_readSingleResult(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::SINGLEFIFOCFG_CLR

Single FIFO Configuration

Definition at line 140 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SINGLEFIFOCFG_SET

Single FIFO Configuration

Definition at line 108 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::SINGLEFIFOCFG_TGL

Single FIFO Configuration

Definition at line 172 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEFIFODATA

Single FIFO Read Data

Definition at line 77 of file efr32bg21_iadc.h.

Referenced by IADC_pullSingleFifoData(), and IADC_pullSingleFifoResult().

__IM uint32_t IADC_TypeDef::SINGLEFIFODATA_CLR

Single FIFO Read Data

Definition at line 141 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEFIFODATA_SET

Single FIFO Read Data

Definition at line 109 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEFIFODATA_TGL

Single FIFO Read Data

Definition at line 173 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEFIFOSTAT

Single FIFO Status

Definition at line 78 of file efr32bg21_iadc.h.

Referenced by IADC_getSingleFifoCnt().

__IM uint32_t IADC_TypeDef::SINGLEFIFOSTAT_CLR

Single FIFO Status

Definition at line 142 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEFIFOSTAT_SET

Single FIFO Status

Definition at line 110 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::SINGLEFIFOSTAT_TGL

Single FIFO Status

Definition at line 174 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::STATUS

Status

Definition at line 65 of file efr32bg21_iadc.h.

Referenced by IADC_getStatus(), and IADC_reset().

__IM uint32_t IADC_TypeDef::STATUS_CLR

Status

Definition at line 129 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::STATUS_SET

Status

Definition at line 97 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::STATUS_TGL

Status

Definition at line 161 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::STMASK

Scan Table Mask

Definition at line 67 of file efr32bg21_iadc.h.

Referenced by IADC_getScanMask().

__IM uint32_t IADC_TypeDef::STMASK_CLR

Scan Table Mask

Definition at line 131 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::STMASK_SET

Scan Table Mask

Definition at line 99 of file efr32bg21_iadc.h.

__IM uint32_t IADC_TypeDef::STMASK_TGL

Scan Table Mask

Definition at line 163 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::TIMER

Timer

Definition at line 64 of file efr32bg21_iadc.h.

Referenced by IADC_init(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::TIMER_CLR

Timer

Definition at line 128 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::TIMER_SET

Timer

Definition at line 96 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::TIMER_TGL

Timer

Definition at line 160 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::TRIGGER

Trigger

Definition at line 71 of file efr32bg21_iadc.h.

Referenced by IADC_initScan(), IADC_initSingle(), and IADC_reset().

__IOM uint32_t IADC_TypeDef::TRIGGER_CLR

Trigger

Definition at line 135 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::TRIGGER_SET

Trigger

Definition at line 103 of file efr32bg21_iadc.h.

__IOM uint32_t IADC_TypeDef::TRIGGER_TGL

Trigger

Definition at line 167 of file efr32bg21_iadc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_iadc.h