LDMA_CH_TypeDef Struct ReferenceDevices > LDMA

LDMA CH Register Group Declaration.

Definition at line 46 of file efr32bg21_ldma.h.

#include <efr32bg21_ldma.h>

Data Fields

__IOM uint32_t CFG
 
__IOM uint32_t CTRL
 
__IOM uint32_t DST
 
__IOM uint32_t LINK
 
__IOM uint32_t LOOP
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [5U]
 
__IOM uint32_t SRC
 

Field Documentation

__IOM uint32_t LDMA_CH_TypeDef::CFG

Channel Configuration Register

Definition at line 48 of file efr32bg21_ldma.h.

__IOM uint32_t LDMA_CH_TypeDef::CTRL

Channel Descriptor Control Word Register

Definition at line 50 of file efr32bg21_ldma.h.

__IOM uint32_t LDMA_CH_TypeDef::DST

Channel Descriptor Destination Data A...

Definition at line 52 of file efr32bg21_ldma.h.

__IOM uint32_t LDMA_CH_TypeDef::LINK

Channel Descriptor Link Structure Add...

Definition at line 53 of file efr32bg21_ldma.h.

__IOM uint32_t LDMA_CH_TypeDef::LOOP

Channel Loop Counter Register

Definition at line 49 of file efr32bg21_ldma.h.

uint32_t LDMA_CH_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 47 of file efr32bg21_ldma.h.

uint32_t LDMA_CH_TypeDef::RESERVED1[5U]

Reserved for future use

Definition at line 54 of file efr32bg21_ldma.h.

__IOM uint32_t LDMA_CH_TypeDef::SRC

Channel Descriptor Source Data Addres...

Definition at line 51 of file efr32bg21_ldma.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_ldma.h