LDMAXBAR_CH_TypeDef Struct ReferenceDevices > LDMAXBAR

LDMAXBAR CH Register Group Declaration.

Definition at line 46 of file efr32bg21_ldmaxbar.h.

#include <efr32bg21_ldmaxbar.h>

Data Fields

__IOM uint32_t REQSEL
 

Field Documentation

__IOM uint32_t LDMAXBAR_CH_TypeDef::REQSEL

Channel Peripheral Request Select Reg...

Definition at line 47 of file efr32bg21_ldmaxbar.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_ldmaxbar.h