LDMAXBAR_TypeDef Struct ReferenceDevices > LDMAXBAR

LDMAXBAR Register Declaration.

Definition at line 51 of file efr32bg21_ldmaxbar.h.

#include <efr32bg21_ldmaxbar.h>

Data Fields

LDMAXBAR_CH_TypeDef CH [8U]
 
LDMAXBAR_CH_TypeDef CH_CLR [8U]
 
LDMAXBAR_CH_TypeDef CH_SET [8U]
 
LDMAXBAR_CH_TypeDef CH_TGL [8U]
 
uint32_t RESERVED0 [1016U]
 
uint32_t RESERVED1 [1016U]
 
uint32_t RESERVED2 [1016U]
 

Field Documentation

LDMAXBAR_CH_TypeDef LDMAXBAR_TypeDef::CH[8U]

DMA Channel Registers

Definition at line 52 of file efr32bg21_ldmaxbar.h.

LDMAXBAR_CH_TypeDef LDMAXBAR_TypeDef::CH_CLR[8U]

DMA Channel Registers

Definition at line 56 of file efr32bg21_ldmaxbar.h.

LDMAXBAR_CH_TypeDef LDMAXBAR_TypeDef::CH_SET[8U]

DMA Channel Registers

Definition at line 54 of file efr32bg21_ldmaxbar.h.

LDMAXBAR_CH_TypeDef LDMAXBAR_TypeDef::CH_TGL[8U]

DMA Channel Registers

Definition at line 58 of file efr32bg21_ldmaxbar.h.

uint32_t LDMAXBAR_TypeDef::RESERVED0[1016U]

Reserved for future use

Definition at line 53 of file efr32bg21_ldmaxbar.h.

uint32_t LDMAXBAR_TypeDef::RESERVED1[1016U]

Reserved for future use

Definition at line 55 of file efr32bg21_ldmaxbar.h.

uint32_t LDMAXBAR_TypeDef::RESERVED2[1016U]

Reserved for future use

Definition at line 57 of file efr32bg21_ldmaxbar.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_ldmaxbar.h