LVGD_TypeDef Struct ReferenceDevices > LVGD

LVGD Register Declaration.

Definition at line 46 of file efr32bg21_lvgd.h.

#include <efr32bg21_lvgd.h>

Data Fields

uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [1023U]
 
uint32_t RESERVED2 [1U]
 
uint32_t RESERVED3 [1023U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [1023U]
 
uint32_t RESERVED6 [1U]
 

Field Documentation

uint32_t LVGD_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 47 of file efr32bg21_lvgd.h.

uint32_t LVGD_TypeDef::RESERVED1[1023U]

Reserved for future use

Definition at line 48 of file efr32bg21_lvgd.h.

uint32_t LVGD_TypeDef::RESERVED2[1U]

Reserved for future use

Definition at line 49 of file efr32bg21_lvgd.h.

uint32_t LVGD_TypeDef::RESERVED3[1023U]

Reserved for future use

Definition at line 50 of file efr32bg21_lvgd.h.

uint32_t LVGD_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 51 of file efr32bg21_lvgd.h.

uint32_t LVGD_TypeDef::RESERVED5[1023U]

Reserved for future use

Definition at line 52 of file efr32bg21_lvgd.h.

uint32_t LVGD_TypeDef::RESERVED6[1U]

Reserved for future use

Definition at line 53 of file efr32bg21_lvgd.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_lvgd.h