MODEM_IRCALCOEFWR_TypeDef Struct ReferenceDevices > MODEM

MODEM IRCALCOEFWR Register Group Declaration.

Definition at line 46 of file efr32bg21_modem.h.

#include <efr32bg21_modem.h>

Data Fields

__IOM uint32_t IRCALCOEFWR
 

Field Documentation

__IOM uint32_t MODEM_IRCALCOEFWR_TypeDef::IRCALCOEFWR

IRCAL COEF WR per antenna

Definition at line 47 of file efr32bg21_modem.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_modem.h