MSC_TypeDef Struct ReferenceDevices > MSC

MSC Register Declaration.

Definition at line 46 of file efr32bg21_msc.h.

#include <efr32bg21_msc.h>

Data Fields

__IOM uint32_t ADDRB
 
__IOM uint32_t ADDRB_CLR
 
__IOM uint32_t ADDRB_SET
 
__IOM uint32_t ADDRB_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
__IOM uint32_t MISCLOCKWORD
 
__IOM uint32_t MISCLOCKWORD_CLR
 
__IOM uint32_t MISCLOCKWORD_SET
 
__IOM uint32_t MISCLOCKWORD_TGL
 
__IOM uint32_t PAGELOCK0
 
__IOM uint32_t PAGELOCK0_CLR
 
__IOM uint32_t PAGELOCK0_SET
 
__IOM uint32_t PAGELOCK0_TGL
 
__IOM uint32_t PAGELOCK1
 
__IOM uint32_t PAGELOCK1_CLR
 
__IOM uint32_t PAGELOCK1_SET
 
__IOM uint32_t PAGELOCK1_TGL
 
__IOM uint32_t PAGELOCK2
 
__IOM uint32_t PAGELOCK2_CLR
 
__IOM uint32_t PAGELOCK2_SET
 
__IOM uint32_t PAGELOCK2_TGL
 
__IOM uint32_t PAGELOCK3
 
__IOM uint32_t PAGELOCK3_CLR
 
__IOM uint32_t PAGELOCK3_SET
 
__IOM uint32_t PAGELOCK3_TGL
 
__IOM uint32_t READCTRL
 
__IOM uint32_t READCTRL_CLR
 
__IOM uint32_t READCTRL_SET
 
__IOM uint32_t READCTRL_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [3U]
 
uint32_t RESERVED10 [3U]
 
uint32_t RESERVED11 [55U]
 
uint32_t RESERVED12 [4U]
 
uint32_t RESERVED13 [4U]
 
uint32_t RESERVED14 [4U]
 
uint32_t RESERVED15 [4U]
 
uint32_t RESERVED16 [12U]
 
uint32_t RESERVED17 [919U]
 
uint32_t RESERVED18 [1U]
 
uint32_t RESERVED19 [3U]
 
uint32_t RESERVED2 [55U]
 
uint32_t RESERVED20 [55U]
 
uint32_t RESERVED21 [4U]
 
uint32_t RESERVED22 [4U]
 
uint32_t RESERVED23 [4U]
 
uint32_t RESERVED24 [4U]
 
uint32_t RESERVED25 [12U]
 
uint32_t RESERVED26 [919U]
 
uint32_t RESERVED27 [1U]
 
uint32_t RESERVED28 [3U]
 
uint32_t RESERVED29 [55U]
 
uint32_t RESERVED3 [4U]
 
uint32_t RESERVED30 [4U]
 
uint32_t RESERVED31 [4U]
 
uint32_t RESERVED32 [4U]
 
uint32_t RESERVED33 [4U]
 
uint32_t RESERVED34 [12U]
 
uint32_t RESERVED4 [4U]
 
uint32_t RESERVED5 [4U]
 
uint32_t RESERVED6 [4U]
 
uint32_t RESERVED7 [12U]
 
uint32_t RESERVED8 [919U]
 
uint32_t RESERVED9 [1U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t TESTCTRL
 
__IOM uint32_t TESTCTRL_CLR
 
__IOM uint32_t TESTCTRL_SET
 
__IOM uint32_t TESTCTRL_TGL
 
__IM uint32_t USERDATASIZE
 
__IM uint32_t USERDATASIZE_CLR
 
__IM uint32_t USERDATASIZE_SET
 
__IM uint32_t USERDATASIZE_TGL
 
__IOM uint32_t WDATA
 
__IOM uint32_t WDATA_CLR
 
__IOM uint32_t WDATA_SET
 
__IOM uint32_t WDATA_TGL
 
__IOM uint32_t WRITECMD
 
__IOM uint32_t WRITECMD_CLR
 
__IOM uint32_t WRITECMD_SET
 
__IOM uint32_t WRITECMD_TGL
 
__IOM uint32_t WRITECTRL
 
__IOM uint32_t WRITECTRL_CLR
 
__IOM uint32_t WRITECTRL_SET
 
__IOM uint32_t WRITECTRL_TGL
 

Field Documentation

__IOM uint32_t MSC_TypeDef::ADDRB

Page Erase/Write Address Buffer

Definition at line 52 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::ADDRB_CLR

Page Erase/Write Address Buffer

Definition at line 106 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::ADDRB_SET

Page Erase/Write Address Buffer

Definition at line 79 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::ADDRB_TGL

Page Erase/Write Address Buffer

Definition at line 133 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::CMD

Command Register

Definition at line 59 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::CMD_CLR

Command Register

Definition at line 113 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::CMD_SET

Command Register

Definition at line 86 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::CMD_TGL

Command Register

Definition at line 140 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IEN

Interrupt Enable Register

Definition at line 56 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 110 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 83 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 137 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IF

Interrupt Flag Register

Definition at line 55 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 109 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 82 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 136 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::IPVERSION

IP version ID

Definition at line 47 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::IPVERSION_CLR

IP version ID

Definition at line 101 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::IPVERSION_SET

IP version ID

Definition at line 74 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::IPVERSION_TGL

IP version ID

Definition at line 128 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::LOCK

Configuration Lock Register

Definition at line 60 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::LOCK_CLR

Configuration Lock Register

Definition at line 114 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::LOCK_SET

Configuration Lock Register

Definition at line 87 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::LOCK_TGL

Configuration Lock Register

Definition at line 141 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::MISCLOCKWORD

Mass erase and User data page lock word

Definition at line 61 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::MISCLOCKWORD_CLR

Mass erase and User data page lock word

Definition at line 115 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::MISCLOCKWORD_SET

Mass erase and User data page lock word

Definition at line 88 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::MISCLOCKWORD_TGL

Mass erase and User data page lock word

Definition at line 142 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK0

Main space page 0-31 lock word

Definition at line 63 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK0_CLR

Main space page 0-31 lock word

Definition at line 117 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK0_SET

Main space page 0-31 lock word

Definition at line 90 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK0_TGL

Main space page 0-31 lock word

Definition at line 144 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK1

Main space page 32-63 lock word

Definition at line 64 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK1_CLR

Main space page 32-63 lock word

Definition at line 118 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK1_SET

Main space page 32-63 lock word

Definition at line 91 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK1_TGL

Main space page 32-63 lock word

Definition at line 145 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK2

Main space page 64-95 lock word

Definition at line 65 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK2_CLR

Main space page 64-95 lock word

Definition at line 119 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK2_SET

Main space page 64-95 lock word

Definition at line 92 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK2_TGL

Main space page 64-95 lock word

Definition at line 146 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK3

Main space page 96-127 lock word

Definition at line 66 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK3_CLR

Main space page 96-127 lock word

Definition at line 120 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK3_SET

Main space page 96-127 lock word

Definition at line 93 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::PAGELOCK3_TGL

Main space page 96-127 lock word

Definition at line 147 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::READCTRL

Read Control Register

Definition at line 49 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::READCTRL_CLR

Read Control Register

Definition at line 103 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::READCTRL_SET

Read Control Register

Definition at line 76 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::READCTRL_TGL

Read Control Register

Definition at line 130 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 48 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED1[3U]

Reserved for future use

Definition at line 57 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED10[3U]

Reserved for future use

Definition at line 84 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED11[55U]

Reserved for future use

Definition at line 89 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED12[4U]

Reserved for future use

Definition at line 94 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED13[4U]

Reserved for future use

Definition at line 95 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED14[4U]

Reserved for future use

Definition at line 96 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED15[4U]

Reserved for future use

Definition at line 97 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED16[12U]

Reserved for future use

Definition at line 98 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED17[919U]

Reserved for future use

Definition at line 100 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED18[1U]

Reserved for future use

Definition at line 102 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED19[3U]

Reserved for future use

Definition at line 111 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED2[55U]

Reserved for future use

Definition at line 62 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED20[55U]

Reserved for future use

Definition at line 116 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED21[4U]

Reserved for future use

Definition at line 121 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED22[4U]

Reserved for future use

Definition at line 122 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED23[4U]

Reserved for future use

Definition at line 123 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED24[4U]

Reserved for future use

Definition at line 124 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED25[12U]

Reserved for future use

Definition at line 125 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED26[919U]

Reserved for future use

Definition at line 127 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED27[1U]

Reserved for future use

Definition at line 129 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED28[3U]

Reserved for future use

Definition at line 138 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED29[55U]

Reserved for future use

Definition at line 143 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED3[4U]

Reserved for future use

Definition at line 67 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED30[4U]

Reserved for future use

Definition at line 148 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED31[4U]

Reserved for future use

Definition at line 149 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED32[4U]

Reserved for future use

Definition at line 150 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED33[4U]

Reserved for future use

Definition at line 151 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED34[12U]

Reserved for future use

Definition at line 152 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED4[4U]

Reserved for future use

Definition at line 68 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED5[4U]

Reserved for future use

Definition at line 69 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED6[4U]

Reserved for future use

Definition at line 70 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED7[12U]

Reserved for future use

Definition at line 71 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED8[919U]

Reserved for future use

Definition at line 73 of file efr32bg21_msc.h.

uint32_t MSC_TypeDef::RESERVED9[1U]

Reserved for future use

Definition at line 75 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::STATUS

Status Register

Definition at line 54 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::STATUS_CLR

Status Register

Definition at line 108 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::STATUS_SET

Status Register

Definition at line 81 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::STATUS_TGL

Status Register

Definition at line 135 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::TESTCTRL

Flash test control register

Definition at line 72 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::TESTCTRL_CLR

Flash test control register

Definition at line 126 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::TESTCTRL_SET

Flash test control register

Definition at line 99 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::TESTCTRL_TGL

Flash test control register

Definition at line 153 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::USERDATASIZE

user data regsion size

Definition at line 58 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::USERDATASIZE_CLR

user data regsion size

Definition at line 112 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::USERDATASIZE_SET

user data regsion size

Definition at line 85 of file efr32bg21_msc.h.

__IM uint32_t MSC_TypeDef::USERDATASIZE_TGL

user data regsion size

Definition at line 139 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WDATA

Write Data Register

Definition at line 53 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WDATA_CLR

Write Data Register

Definition at line 107 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WDATA_SET

Write Data Register

Definition at line 80 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WDATA_TGL

Write Data Register

Definition at line 134 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECMD

Write Command Register

Definition at line 51 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECMD_CLR

Write Command Register

Definition at line 105 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECMD_SET

Write Command Register

Definition at line 78 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECMD_TGL

Write Command Register

Definition at line 132 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECTRL

Write Control Register

Definition at line 50 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECTRL_CLR

Write Control Register

Definition at line 104 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECTRL_SET

Write Control Register

Definition at line 77 of file efr32bg21_msc.h.

__IOM uint32_t MSC_TypeDef::WRITECTRL_TGL

Write Control Register

Definition at line 131 of file efr32bg21_msc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_msc.h