PROTIMER_CC_TypeDef Struct ReferenceDevices > PROTIMER

PROTIMER CC Register Group Declaration.

Definition at line 46 of file efr32bg21_protimer.h.

#include <efr32bg21_protimer.h>

Data Fields

__IOM uint32_t BASE
 
__IOM uint32_t CTRL
 
__IOM uint32_t PRE
 
__IOM uint32_t WRAP
 

Field Documentation

__IOM uint32_t PROTIMER_CC_TypeDef::BASE

CC Channel BASE Value Register

Definition at line 49 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 47 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_CC_TypeDef::PRE

CC Channel PRE Value Register

Definition at line 48 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_CC_TypeDef::WRAP

CC Channel WRAP Value Register

Definition at line 50 of file efr32bg21_protimer.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_protimer.h