PROTIMER_TypeDef Struct ReferenceDevices > PROTIMER

PROTIMER Register Declaration.

Definition at line 54 of file efr32bg21_protimer.h.

#include <efr32bg21_protimer.h>

Data Fields

__IOM uint32_t BASECNT
 
__IOM uint32_t BASECNT_CLR
 
__IOM uint32_t BASECNT_SET
 
__IOM uint32_t BASECNT_TGL
 
__IOM uint32_t BASECNTTOP
 
__IOM uint32_t BASECNTTOP_CLR
 
__IOM uint32_t BASECNTTOP_SET
 
__IOM uint32_t BASECNTTOP_TGL
 
__IM uint32_t BASEPRE
 
__IM uint32_t BASEPRE_CLR
 
__IM uint32_t BASEPRE_SET
 
__IM uint32_t BASEPRE_TGL
 
PROTIMER_CC_TypeDef CC [8U]
 
PROTIMER_CC_TypeDef CC_CLR [8U]
 
PROTIMER_CC_TypeDef CC_SET [8U]
 
PROTIMER_CC_TypeDef CC_TGL [8U]
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t ETSI
 
__IOM uint32_t ETSI_CLR
 
__IOM uint32_t ETSI_SET
 
__IOM uint32_t ETSI_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LBTCTRL
 
__IOM uint32_t LBTCTRL_CLR
 
__IOM uint32_t LBTCTRL_SET
 
__IOM uint32_t LBTCTRL_TGL
 
__IOM uint32_t LBTPRSCTRL
 
__IOM uint32_t LBTPRSCTRL_CLR
 
__IOM uint32_t LBTPRSCTRL_SET
 
__IOM uint32_t LBTPRSCTRL_TGL
 
__IOM uint32_t LBTSTATE
 
__IOM uint32_t LBTSTATE1
 
__IOM uint32_t LBTSTATE1_CLR
 
__IOM uint32_t LBTSTATE1_SET
 
__IOM uint32_t LBTSTATE1_TGL
 
__IOM uint32_t LBTSTATE_CLR
 
__IOM uint32_t LBTSTATE_SET
 
__IOM uint32_t LBTSTATE_TGL
 
__IM uint32_t LWRAPCNT
 
__IM uint32_t LWRAPCNT_CLR
 
__IM uint32_t LWRAPCNT_SET
 
__IM uint32_t LWRAPCNT_TGL
 
__IOM uint32_t PRECNT
 
__IOM uint32_t PRECNT_CLR
 
__IOM uint32_t PRECNT_SET
 
__IOM uint32_t PRECNT_TGL
 
__IOM uint32_t PRECNTTOP
 
__IOM uint32_t PRECNTTOP_CLR
 
__IOM uint32_t PRECNTTOP_SET
 
__IOM uint32_t PRECNTTOP_TGL
 
__IOM uint32_t PRECNTTOPADJ
 
__IOM uint32_t PRECNTTOPADJ_CLR
 
__IOM uint32_t PRECNTTOPADJ_SET
 
__IOM uint32_t PRECNTTOPADJ_TGL
 
__IOM uint32_t PRSCTRL
 
__IOM uint32_t PRSCTRL_CLR
 
__IOM uint32_t PRSCTRL_SET
 
__IOM uint32_t PRSCTRL_TGL
 
__IOM uint32_t RANDOM
 
__IOM uint32_t RANDOM_CLR
 
__IOM uint32_t RANDOM_SET
 
__IOM uint32_t RANDOM_TGL
 
__IOM uint32_t RANDOMFW0
 
__IOM uint32_t RANDOMFW0_CLR
 
__IOM uint32_t RANDOMFW0_SET
 
__IOM uint32_t RANDOMFW0_TGL
 
__IOM uint32_t RANDOMFW1
 
__IOM uint32_t RANDOMFW1_CLR
 
__IOM uint32_t RANDOMFW1_SET
 
__IOM uint32_t RANDOMFW1_TGL
 
__IOM uint32_t RANDOMFW2
 
__IOM uint32_t RANDOMFW2_CLR
 
__IOM uint32_t RANDOMFW2_SET
 
__IOM uint32_t RANDOMFW2_TGL
 
uint32_t RESERVED0 [2U]
 
uint32_t RESERVED1 [28U]
 
uint32_t RESERVED10 [28U]
 
uint32_t RESERVED2 [928U]
 
uint32_t RESERVED3 [2U]
 
uint32_t RESERVED4 [28U]
 
uint32_t RESERVED5 [928U]
 
uint32_t RESERVED6 [2U]
 
uint32_t RESERVED7 [28U]
 
uint32_t RESERVED8 [928U]
 
uint32_t RESERVED9 [2U]
 
__IOM uint32_t RXCTRL
 
__IOM uint32_t RXCTRL_CLR
 
__IOM uint32_t RXCTRL_SET
 
__IOM uint32_t RXCTRL_TGL
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t TOUT0CNT
 
__IOM uint32_t TOUT0CNT_CLR
 
__IOM uint32_t TOUT0CNT_SET
 
__IOM uint32_t TOUT0CNT_TGL
 
__IOM uint32_t TOUT0CNTTOP
 
__IOM uint32_t TOUT0CNTTOP_CLR
 
__IOM uint32_t TOUT0CNTTOP_SET
 
__IOM uint32_t TOUT0CNTTOP_TGL
 
__IOM uint32_t TOUT0COMP
 
__IOM uint32_t TOUT0COMP_CLR
 
__IOM uint32_t TOUT0COMP_SET
 
__IOM uint32_t TOUT0COMP_TGL
 
__IOM uint32_t TOUT1CNT
 
__IOM uint32_t TOUT1CNT_CLR
 
__IOM uint32_t TOUT1CNT_SET
 
__IOM uint32_t TOUT1CNT_TGL
 
__IOM uint32_t TOUT1CNTTOP
 
__IOM uint32_t TOUT1CNTTOP_CLR
 
__IOM uint32_t TOUT1CNTTOP_SET
 
__IOM uint32_t TOUT1CNTTOP_TGL
 
__IOM uint32_t TOUT1COMP
 
__IOM uint32_t TOUT1COMP_CLR
 
__IOM uint32_t TOUT1COMP_SET
 
__IOM uint32_t TOUT1COMP_TGL
 
__IOM uint32_t TXCTRL
 
__IOM uint32_t TXCTRL_CLR
 
__IOM uint32_t TXCTRL_SET
 
__IOM uint32_t TXCTRL_TGL
 
__IOM uint32_t WRAPCNT
 
__IOM uint32_t WRAPCNT_CLR
 
__IOM uint32_t WRAPCNT_SET
 
__IOM uint32_t WRAPCNT_TGL
 
__IOM uint32_t WRAPCNTTOP
 
__IOM uint32_t WRAPCNTTOP_CLR
 
__IOM uint32_t WRAPCNTTOP_SET
 
__IOM uint32_t WRAPCNTTOP_TGL
 

Field Documentation

__IOM uint32_t PROTIMER_TypeDef::BASECNT

Base Counter Value

Definition at line 62 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNT_CLR

Base Counter Value

Definition at line 138 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNT_SET

Base Counter Value

Definition at line 100 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNT_TGL

Base Counter Value

Definition at line 176 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNTTOP

BASECNT Top Value

Definition at line 68 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNTTOP_CLR

BASECNT Top Value

Definition at line 144 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNTTOP_SET

BASECNT Top Value

Definition at line 106 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::BASECNTTOP_TGL

BASECNT Top Value

Definition at line 182 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::BASEPRE

Base and Pre counter values

Definition at line 64 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::BASEPRE_CLR

Base and Pre counter values

Definition at line 140 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::BASEPRE_SET

Base and Pre counter values

Definition at line 102 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::BASEPRE_TGL

Base and Pre counter values

Definition at line 178 of file efr32bg21_protimer.h.

PROTIMER_CC_TypeDef PROTIMER_TypeDef::CC[8U]

Compare/Capture Channel

Definition at line 91 of file efr32bg21_protimer.h.

PROTIMER_CC_TypeDef PROTIMER_TypeDef::CC_CLR[8U]

Compare/Capture Channel

Definition at line 167 of file efr32bg21_protimer.h.

PROTIMER_CC_TypeDef PROTIMER_TypeDef::CC_SET[8U]

Compare/Capture Channel

Definition at line 129 of file efr32bg21_protimer.h.

PROTIMER_CC_TypeDef PROTIMER_TypeDef::CC_TGL[8U]

Compare/Capture Channel

Definition at line 205 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CMD

Command Register

Definition at line 58 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CMD_CLR

Command Register

Definition at line 134 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CMD_SET

Command Register

Definition at line 96 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CMD_TGL

Command Register

Definition at line 172 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CTRL

Control Register

Definition at line 57 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CTRL_CLR

Control Register

Definition at line 133 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CTRL_SET

Control Register

Definition at line 95 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::CTRL_TGL

Control Register

Definition at line 171 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::EN

EN

Definition at line 56 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::EN_CLR

EN

Definition at line 132 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::EN_SET

EN

Definition at line 94 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::EN_TGL

EN

Definition at line 170 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::ETSI

Support ETSI LBT

Definition at line 85 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::ETSI_CLR

Support ETSI LBT

Definition at line 161 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::ETSI_SET

Support ETSI LBT

Definition at line 123 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::ETSI_TGL

Support ETSI LBT

Definition at line 199 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 82 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 158 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 120 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 196 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 80 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 156 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 118 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 194 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::IPVERSION

IPVERSION

Definition at line 55 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::IPVERSION_CLR

IPVERSION

Definition at line 131 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::IPVERSION_SET

IPVERSION

Definition at line 93 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::IPVERSION_TGL

IPVERSION

Definition at line 169 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTCTRL

Listen Before Talk Wait Control

Definition at line 76 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTCTRL_CLR

Listen Before Talk Wait Control

Definition at line 152 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTCTRL_SET

Listen Before Talk Wait Control

Definition at line 114 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTCTRL_TGL

Listen Before Talk Wait Control

Definition at line 190 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTPRSCTRL

PRS Channel selection

Definition at line 77 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTPRSCTRL_CLR

PRS Channel selection

Definition at line 153 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTPRSCTRL_SET

PRS Channel selection

Definition at line 115 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTPRSCTRL_TGL

PRS Channel selection

Definition at line 191 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE

Listen Before Talk State

Definition at line 78 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE1

Listen Before Talk State

Definition at line 86 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE1_CLR

Listen Before Talk State

Definition at line 162 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE1_SET

Listen Before Talk State

Definition at line 124 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE1_TGL

Listen Before Talk State

Definition at line 200 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE_CLR

Listen Before Talk State

Definition at line 154 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE_SET

Listen Before Talk State

Definition at line 116 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::LBTSTATE_TGL

Listen Before Talk State

Definition at line 192 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::LWRAPCNT

Latched Wrap Counter Value

Definition at line 65 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::LWRAPCNT_CLR

Latched Wrap Counter Value

Definition at line 141 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::LWRAPCNT_SET

Latched Wrap Counter Value

Definition at line 103 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::LWRAPCNT_TGL

Latched Wrap Counter Value

Definition at line 179 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNT

Pre Counter Value

Definition at line 61 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNT_CLR

Pre Counter Value

Definition at line 137 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNT_SET

Pre Counter Value

Definition at line 99 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNT_TGL

Pre Counter Value

Definition at line 175 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOP

PRECNT Top Value

Definition at line 67 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOP_CLR

PRECNT Top Value

Definition at line 143 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOP_SET

PRECNT Top Value

Definition at line 105 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOP_TGL

PRECNT Top Value

Definition at line 181 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOPADJ

PRECNT Top Adjust Value

Definition at line 66 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOPADJ_CLR

PRECNT Top Adjust Value

Definition at line 142 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOPADJ_SET

PRECNT Top Adjust Value

Definition at line 104 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRECNTTOPADJ_TGL

PRECNT Top Adjust Value

Definition at line 180 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRSCTRL

PRS Channel selection

Definition at line 59 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRSCTRL_CLR

PRS Channel selection

Definition at line 135 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRSCTRL_SET

PRS Channel selection

Definition at line 97 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::PRSCTRL_TGL

PRS Channel selection

Definition at line 173 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOM

Pseudo Random Generator Value Register

Definition at line 79 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOM_CLR

Pseudo Random Generator Value Register

Definition at line 155 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOM_SET

Pseudo Random Generator Value Register

Definition at line 117 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOM_TGL

Pseudo Random Generator Value Register

Definition at line 193 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW0

GENERATED LINEAR RANDOM VALUE

Definition at line 87 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW0_CLR

GENERATED LINEAR RANDOM VALUE

Definition at line 163 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW0_SET

GENERATED LINEAR RANDOM VALUE

Definition at line 125 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW0_TGL

GENERATED LINEAR RANDOM VALUE

Definition at line 201 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW1

GENERATED LINEAR RANDOM VALUE

Definition at line 88 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW1_CLR

GENERATED LINEAR RANDOM VALUE

Definition at line 164 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW1_SET

GENERATED LINEAR RANDOM VALUE

Definition at line 126 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW1_TGL

GENERATED LINEAR RANDOM VALUE

Definition at line 202 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW2

GENERATED LINEAR RANDOM VALUE

Definition at line 89 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW2_CLR

GENERATED LINEAR RANDOM VALUE

Definition at line 165 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW2_SET

GENERATED LINEAR RANDOM VALUE

Definition at line 127 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RANDOMFW2_TGL

GENERATED LINEAR RANDOM VALUE

Definition at line 203 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED0[2U]

Reserved for future use

Definition at line 81 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED1[28U]

Reserved for future use

Definition at line 90 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED10[28U]

Reserved for future use

Definition at line 204 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED2[928U]

Reserved for future use

Definition at line 92 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED3[2U]

Reserved for future use

Definition at line 119 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED4[28U]

Reserved for future use

Definition at line 128 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED5[928U]

Reserved for future use

Definition at line 130 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED6[2U]

Reserved for future use

Definition at line 157 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED7[28U]

Reserved for future use

Definition at line 166 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED8[928U]

Reserved for future use

Definition at line 168 of file efr32bg21_protimer.h.

uint32_t PROTIMER_TypeDef::RESERVED9[2U]

Reserved for future use

Definition at line 195 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RXCTRL

RX request signal from Protimer

Definition at line 83 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RXCTRL_CLR

RX request signal from Protimer

Definition at line 159 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RXCTRL_SET

RX request signal from Protimer

Definition at line 121 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::RXCTRL_TGL

RX request signal from Protimer

Definition at line 197 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::STATUS

Status Register

Definition at line 60 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::STATUS_CLR

Status Register

Definition at line 136 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::STATUS_SET

Status Register

Definition at line 98 of file efr32bg21_protimer.h.

__IM uint32_t PROTIMER_TypeDef::STATUS_TGL

Status Register

Definition at line 174 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNT

TOUT0CNT Value Register

Definition at line 70 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNT_CLR

TOUT0CNT Value Register

Definition at line 146 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNT_SET

TOUT0CNT Value Register

Definition at line 108 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNT_TGL

TOUT0CNT Value Register

Definition at line 184 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNTTOP

TOUT0CNTTOP Value Register.

Definition at line 71 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNTTOP_CLR

TOUT0CNTTOP Value Register.

Definition at line 147 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNTTOP_SET

TOUT0CNTTOP Value Register.

Definition at line 109 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0CNTTOP_TGL

TOUT0CNTTOP Value Register.

Definition at line 185 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0COMP

TOUT0COMP Register

Definition at line 72 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0COMP_CLR

TOUT0COMP Register

Definition at line 148 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0COMP_SET

TOUT0COMP Register

Definition at line 110 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT0COMP_TGL

TOUT0COMP Register

Definition at line 186 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNT

TOUT1CNT Value Register

Definition at line 73 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNT_CLR

TOUT1CNT Value Register

Definition at line 149 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNT_SET

TOUT1CNT Value Register

Definition at line 111 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNT_TGL

TOUT1CNT Value Register

Definition at line 187 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNTTOP

TOUT1CNTTOP Value Register.

Definition at line 74 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNTTOP_CLR

TOUT1CNTTOP Value Register.

Definition at line 150 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNTTOP_SET

TOUT1CNTTOP Value Register.

Definition at line 112 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1CNTTOP_TGL

TOUT1CNTTOP Value Register.

Definition at line 188 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1COMP

TOUT1COMP Register

Definition at line 75 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1COMP_CLR

TOUT1COMP Register

Definition at line 151 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1COMP_SET

TOUT1COMP Register

Definition at line 113 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TOUT1COMP_TGL

TOUT1COMP Register

Definition at line 189 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TXCTRL

TX request signal from Protimer

Definition at line 84 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TXCTRL_CLR

TX request signal from Protimer

Definition at line 160 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TXCTRL_SET

TX request signal from Protimer

Definition at line 122 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::TXCTRL_TGL

TX request signal from Protimer

Definition at line 198 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNT

Wrap Counter Value

Definition at line 63 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNT_CLR

Wrap Counter Value

Definition at line 139 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNT_SET

Wrap Counter Value

Definition at line 101 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNT_TGL

Wrap Counter Value

Definition at line 177 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNTTOP

WRAPCNT Top Value Register

Definition at line 69 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNTTOP_CLR

WRAPCNT Top Value Register

Definition at line 145 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNTTOP_SET

WRAPCNT Top Value Register

Definition at line 107 of file efr32bg21_protimer.h.

__IOM uint32_t PROTIMER_TypeDef::WRAPCNTTOP_TGL

WRAPCNT Top Value Register

Definition at line 183 of file efr32bg21_protimer.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_protimer.h