RFCRC_TypeDef Struct ReferenceDevices > RFCRC

RFCRC Register Declaration.

Definition at line 46 of file efr32bg21_rfcrc.h.

#include <efr32bg21_rfcrc.h>

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IM uint32_t DATA
 
__IM uint32_t DATA_CLR
 
__IM uint32_t DATA_SET
 
__IM uint32_t DATA_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t INIT
 
__IOM uint32_t INIT_CLR
 
__IOM uint32_t INIT_SET
 
__IOM uint32_t INIT_TGL
 
__IOM uint32_t INPUTDATA
 
__IOM uint32_t INPUTDATA_CLR
 
__IOM uint32_t INPUTDATA_SET
 
__IOM uint32_t INPUTDATA_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t POLY
 
__IOM uint32_t POLY_CLR
 
__IOM uint32_t POLY_SET
 
__IOM uint32_t POLY_TGL
 
uint32_t RESERVED0 [1015U]
 
uint32_t RESERVED1 [1015U]
 
uint32_t RESERVED2 [1015U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 

Field Documentation

__IOM uint32_t RFCRC_TypeDef::CMD

Command Register

Definition at line 51 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CMD_CLR

Command Register

Definition at line 71 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CMD_SET

Command Register

Definition at line 61 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CMD_TGL

Command Register

Definition at line 81 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CTRL

Control Register

Definition at line 49 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CTRL_CLR

Control Register

Definition at line 69 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CTRL_SET

Control Register

Definition at line 59 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::CTRL_TGL

Control Register

Definition at line 79 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::DATA

CRC Data Register

Definition at line 54 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::DATA_CLR

CRC Data Register

Definition at line 74 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::DATA_SET

CRC Data Register

Definition at line 64 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::DATA_TGL

CRC Data Register

Definition at line 84 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::EN

Enable peripheral clock to this module

Definition at line 48 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::EN_CLR

Enable peripheral clock to this module

Definition at line 68 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::EN_SET

Enable peripheral clock to this module

Definition at line 58 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::EN_TGL

Enable peripheral clock to this module

Definition at line 78 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INIT

CRC Initialization Value

Definition at line 53 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INIT_CLR

CRC Initialization Value

Definition at line 73 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INIT_SET

CRC Initialization Value

Definition at line 63 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INIT_TGL

CRC Initialization Value

Definition at line 83 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INPUTDATA

Input Data Register

Definition at line 52 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INPUTDATA_CLR

Input Data Register

Definition at line 72 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INPUTDATA_SET

Input Data Register

Definition at line 62 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::INPUTDATA_TGL

Input Data Register

Definition at line 82 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::IPVERSION

IP Version

Definition at line 47 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::IPVERSION_CLR

IP Version

Definition at line 67 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::IPVERSION_SET

IP Version

Definition at line 57 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::IPVERSION_TGL

IP Version

Definition at line 77 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::POLY

CRC Polynomial Value

Definition at line 55 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::POLY_CLR

CRC Polynomial Value

Definition at line 75 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::POLY_SET

CRC Polynomial Value

Definition at line 65 of file efr32bg21_rfcrc.h.

__IOM uint32_t RFCRC_TypeDef::POLY_TGL

CRC Polynomial Value

Definition at line 85 of file efr32bg21_rfcrc.h.

uint32_t RFCRC_TypeDef::RESERVED0[1015U]

Reserved for future use

Definition at line 56 of file efr32bg21_rfcrc.h.

uint32_t RFCRC_TypeDef::RESERVED1[1015U]

Reserved for future use

Definition at line 66 of file efr32bg21_rfcrc.h.

uint32_t RFCRC_TypeDef::RESERVED2[1015U]

Reserved for future use

Definition at line 76 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::STATUS

Status Register

Definition at line 50 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::STATUS_CLR

Status Register

Definition at line 70 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::STATUS_SET

Status Register

Definition at line 60 of file efr32bg21_rfcrc.h.

__IM uint32_t RFCRC_TypeDef::STATUS_TGL

Status Register

Definition at line 80 of file efr32bg21_rfcrc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_rfcrc.h