RTCC_CC_TypeDef Struct ReferenceDevices > RTCC

RTCC CC Register Group Declaration.

Definition at line 46 of file efr32bg21_rtcc.h.

#include <efr32bg21_rtcc.h>

Data Fields

__IOM uint32_t CTRL
 
__IM uint32_t ICVALUE
 
__IOM uint32_t OCVALUE
 

Field Documentation

__IOM uint32_t RTCC_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 47 of file efr32bg21_rtcc.h.

__IM uint32_t RTCC_CC_TypeDef::ICVALUE

Input Capture Value Register

Definition at line 49 of file efr32bg21_rtcc.h.

__IOM uint32_t RTCC_CC_TypeDef::OCVALUE

Output Compare Value Register

Definition at line 48 of file efr32bg21_rtcc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_rtcc.h