SEMAILBOX_FIFO_TypeDef Struct ReferenceDevices > SEMAILBOX_HOST

SEMAILBOX_HOST FIFO Register Group Declaration.

Definition at line 45 of file efr32bg21_semailbox.h.

#include <efr32bg21_semailbox.h>

Data Fields

__IOM uint32_t DATA
 

Field Documentation

__IOM uint32_t SEMAILBOX_FIFO_TypeDef::DATA

RX/TX FIFO DATA

Definition at line 46 of file efr32bg21_semailbox.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_semailbox.h