SEMAILBOX_HOST_TypeDef Struct ReferenceDevices > SEMAILBOX_HOST

SEMAILBOX_HOST Register Declaration.

Definition at line 50 of file efr32bg21_semailbox.h.

#include <efr32bg21_semailbox.h>

Data Fields

__IOM uint32_t CONFIGURATION
 
SEMAILBOX_FIFO_TypeDef FIFO [16U]
 
__IM uint32_t RX_HEADER
 
__IM uint32_t RX_PROT
 
__IM uint32_t RX_STATUS
 
__IOM uint32_t TX_HEADER
 
__IM uint32_t TX_PROT
 
__IM uint32_t TX_STATUS
 

Field Documentation

__IOM uint32_t SEMAILBOX_HOST_TypeDef::CONFIGURATION

Configuration

Definition at line 58 of file efr32bg21_semailbox.h.

SEMAILBOX_FIFO_TypeDef SEMAILBOX_HOST_TypeDef::FIFO[16U]

RX/TX FIFO

Definition at line 51 of file efr32bg21_semailbox.h.

__IM uint32_t SEMAILBOX_HOST_TypeDef::RX_HEADER

RX Header

Definition at line 57 of file efr32bg21_semailbox.h.

__IM uint32_t SEMAILBOX_HOST_TypeDef::RX_PROT

RX Protection

Definition at line 55 of file efr32bg21_semailbox.h.

__IM uint32_t SEMAILBOX_HOST_TypeDef::RX_STATUS

RX Status

Definition at line 53 of file efr32bg21_semailbox.h.

__IOM uint32_t SEMAILBOX_HOST_TypeDef::TX_HEADER

TX Header

Definition at line 56 of file efr32bg21_semailbox.h.

__IM uint32_t SEMAILBOX_HOST_TypeDef::TX_PROT

TX Protection

Definition at line 54 of file efr32bg21_semailbox.h.

__IM uint32_t SEMAILBOX_HOST_TypeDef::TX_STATUS

TX Status

Definition at line 52 of file efr32bg21_semailbox.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_semailbox.h