SMU_TypeDef Struct ReferenceDevices > SMU

SMU Register Declaration.

Definition at line 46 of file efr32bg21_smu.h.

#include <efr32bg21_smu.h>

Data Fields

__IM uint32_t BMPUFS
 
__IM uint32_t BMPUFS_CLR
 
__IM uint32_t BMPUFS_SET
 
__IM uint32_t BMPUFS_TGL
 
__IM uint32_t BMPUFSADDR
 
__IM uint32_t BMPUFSADDR_CLR
 
__IM uint32_t BMPUFSADDR_SET
 
__IM uint32_t BMPUFSADDR_TGL
 
__IOM uint32_t BMPUPATD0
 
__IOM uint32_t BMPUPATD0_CLR
 
__IOM uint32_t BMPUPATD0_SET
 
__IOM uint32_t BMPUPATD0_TGL
 
__IOM uint32_t BMPUSATD0
 
__IOM uint32_t BMPUSATD0_CLR
 
__IOM uint32_t BMPUSATD0_SET
 
__IOM uint32_t BMPUSATD0_TGL
 
__IOM uint32_t ESAUMRB01
 
__IOM uint32_t ESAUMRB01_CLR
 
__IOM uint32_t ESAUMRB01_SET
 
__IOM uint32_t ESAUMRB01_TGL
 
__IOM uint32_t ESAUMRB12
 
__IOM uint32_t ESAUMRB12_CLR
 
__IOM uint32_t ESAUMRB12_SET
 
__IOM uint32_t ESAUMRB12_TGL
 
__IOM uint32_t ESAUMRB45
 
__IOM uint32_t ESAUMRB45_CLR
 
__IOM uint32_t ESAUMRB45_SET
 
__IOM uint32_t ESAUMRB45_TGL
 
__IOM uint32_t ESAUMRB56
 
__IOM uint32_t ESAUMRB56_CLR
 
__IOM uint32_t ESAUMRB56_SET
 
__IOM uint32_t ESAUMRB56_TGL
 
__IOM uint32_t ESAURTYPES0
 
__IOM uint32_t ESAURTYPES0_CLR
 
__IOM uint32_t ESAURTYPES0_SET
 
__IOM uint32_t ESAURTYPES0_TGL
 
__IOM uint32_t ESAURTYPES1
 
__IOM uint32_t ESAURTYPES1_CLR
 
__IOM uint32_t ESAURTYPES1_SET
 
__IOM uint32_t ESAURTYPES1_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
__IOM uint32_t M33CTRL
 
__IOM uint32_t M33CTRL_CLR
 
__IOM uint32_t M33CTRL_SET
 
__IOM uint32_t M33CTRL_TGL
 
__IM uint32_t PPUFS
 
__IM uint32_t PPUFS_CLR
 
__IM uint32_t PPUFS_SET
 
__IM uint32_t PPUFS_TGL
 
__IOM uint32_t PPUPATD0
 
__IOM uint32_t PPUPATD0_CLR
 
__IOM uint32_t PPUPATD0_SET
 
__IOM uint32_t PPUPATD0_TGL
 
__IOM uint32_t PPUPATD1
 
__IOM uint32_t PPUPATD1_CLR
 
__IOM uint32_t PPUPATD1_SET
 
__IOM uint32_t PPUPATD1_TGL
 
__IOM uint32_t PPUSATD0
 
__IOM uint32_t PPUSATD0_CLR
 
__IOM uint32_t PPUSATD0_SET
 
__IOM uint32_t PPUSATD0_TGL
 
__IOM uint32_t PPUSATD1
 
__IOM uint32_t PPUSATD1_CLR
 
__IOM uint32_t PPUSATD1_SET
 
__IOM uint32_t PPUSATD1_TGL
 
uint32_t RESERVED0 [3U]
 
uint32_t RESERVED1 [7U]
 
uint32_t RESERVED10 [862U]
 
uint32_t RESERVED11 [3U]
 
uint32_t RESERVED12 [7U]
 
uint32_t RESERVED13 [6U]
 
uint32_t RESERVED14 [54U]
 
uint32_t RESERVED15 [3U]
 
uint32_t RESERVED16 [7U]
 
uint32_t RESERVED17 [55U]
 
uint32_t RESERVED18 [2U]
 
uint32_t RESERVED19 [2U]
 
uint32_t RESERVED2 [6U]
 
uint32_t RESERVED20 [2U]
 
uint32_t RESERVED21 [862U]
 
uint32_t RESERVED22 [3U]
 
uint32_t RESERVED23 [7U]
 
uint32_t RESERVED24 [6U]
 
uint32_t RESERVED25 [54U]
 
uint32_t RESERVED26 [3U]
 
uint32_t RESERVED27 [7U]
 
uint32_t RESERVED28 [55U]
 
uint32_t RESERVED29 [2U]
 
uint32_t RESERVED3 [54U]
 
uint32_t RESERVED30 [2U]
 
uint32_t RESERVED31 [2U]
 
uint32_t RESERVED32 [862U]
 
uint32_t RESERVED33 [3U]
 
uint32_t RESERVED34 [7U]
 
uint32_t RESERVED35 [6U]
 
uint32_t RESERVED36 [54U]
 
uint32_t RESERVED37 [3U]
 
uint32_t RESERVED38 [7U]
 
uint32_t RESERVED39 [55U]
 
uint32_t RESERVED4 [3U]
 
uint32_t RESERVED40 [2U]
 
uint32_t RESERVED41 [2U]
 
uint32_t RESERVED42 [2U]
 
uint32_t RESERVED5 [7U]
 
uint32_t RESERVED6 [55U]
 
uint32_t RESERVED7 [2U]
 
uint32_t RESERVED8 [2U]
 
uint32_t RESERVED9 [2U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 

Field Documentation

__IM uint32_t SMU_TypeDef::BMPUFS

Fault Status

Definition at line 67 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFS_CLR

Fault Status

Definition at line 131 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFS_SET

Fault Status

Definition at line 99 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFS_TGL

Fault Status

Definition at line 163 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFSADDR

Fault Status Address

Definition at line 68 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFSADDR_CLR

Fault Status Address

Definition at line 132 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFSADDR_SET

Fault Status Address

Definition at line 100 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::BMPUFSADDR_TGL

Fault Status Address

Definition at line 164 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUPATD0

Privileged Attribute

Definition at line 63 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUPATD0_CLR

Privileged Attribute

Definition at line 127 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUPATD0_SET

Privileged Attribute

Definition at line 95 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUPATD0_TGL

Privileged Attribute

Definition at line 159 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUSATD0

Secure Attribute

Definition at line 65 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUSATD0_CLR

Secure Attribute

Definition at line 129 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUSATD0_SET

Secure Attribute

Definition at line 97 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::BMPUSATD0_TGL

Secure Attribute

Definition at line 161 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB01

Movable Region Boundary

Definition at line 73 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB01_CLR

Movable Region Boundary

Definition at line 137 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB01_SET

Movable Region Boundary

Definition at line 105 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB01_TGL

Movable Region Boundary

Definition at line 169 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB12

Movable Region Boundary

Definition at line 74 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB12_CLR

Movable Region Boundary

Definition at line 138 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB12_SET

Movable Region Boundary

Definition at line 106 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB12_TGL

Movable Region Boundary

Definition at line 170 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB45

Movable Region Boundary

Definition at line 76 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB45_CLR

Movable Region Boundary

Definition at line 140 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB45_SET

Movable Region Boundary

Definition at line 108 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB45_TGL

Movable Region Boundary

Definition at line 172 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB56

Movable Region Boundary

Definition at line 77 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB56_CLR

Movable Region Boundary

Definition at line 141 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB56_SET

Movable Region Boundary

Definition at line 109 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAUMRB56_TGL

Movable Region Boundary

Definition at line 173 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES0

Region Types 0

Definition at line 70 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES0_CLR

Region Types 0

Definition at line 134 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES0_SET

Region Types 0

Definition at line 102 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES0_TGL

Region Types 0

Definition at line 166 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES1

Region Types 1

Definition at line 71 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES1_CLR

Region Types 1

Definition at line 135 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES1_SET

Region Types 1

Definition at line 103 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::ESAURTYPES1_TGL

Region Types 1

Definition at line 167 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IEN

Interrupt Enable Register

Definition at line 51 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 115 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 83 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 147 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IF

Interrupt Flag Register

Definition at line 50 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 114 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 82 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 146 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::IPVERSION

IP Version

Definition at line 47 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::IPVERSION_CLR

IP Version

Definition at line 111 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::IPVERSION_SET

IP Version

Definition at line 79 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::IPVERSION_TGL

IP Version

Definition at line 143 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::LOCK

Lock Register

Definition at line 49 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::LOCK_CLR

Lock Register

Definition at line 113 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::LOCK_SET

Lock Register

Definition at line 81 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::LOCK_TGL

Lock Register

Definition at line 145 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::M33CTRL

M33 Control Settings

Definition at line 53 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::M33CTRL_CLR

M33 Control Settings

Definition at line 117 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::M33CTRL_SET

M33 Control Settings

Definition at line 85 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::M33CTRL_TGL

M33 Control Settings

Definition at line 149 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::PPUFS

Fault Status

Definition at line 61 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::PPUFS_CLR

Fault Status

Definition at line 125 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::PPUFS_SET

Fault Status

Definition at line 93 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::PPUFS_TGL

Fault Status

Definition at line 157 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD0

Privileged Access

Definition at line 55 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD0_CLR

Privileged Access

Definition at line 119 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD0_SET

Privileged Access

Definition at line 87 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD0_TGL

Privileged Access

Definition at line 151 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD1

Privileged Access

Definition at line 56 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD1_CLR

Privileged Access

Definition at line 120 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD1_SET

Privileged Access

Definition at line 88 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUPATD1_TGL

Privileged Access

Definition at line 152 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD0

Secure Access

Definition at line 58 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD0_CLR

Secure Access

Definition at line 122 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD0_SET

Secure Access

Definition at line 90 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD0_TGL

Secure Access

Definition at line 154 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD1

Secure Access

Definition at line 59 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD1_CLR

Secure Access

Definition at line 123 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD1_SET

Secure Access

Definition at line 91 of file efr32bg21_smu.h.

__IOM uint32_t SMU_TypeDef::PPUSATD1_TGL

Secure Access

Definition at line 155 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED0[3U]

Reserved for future use

Definition at line 52 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED1[7U]

Reserved for future use

Definition at line 54 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED10[862U]

Reserved for future use

Definition at line 78 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED11[3U]

Reserved for future use

Definition at line 84 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED12[7U]

Reserved for future use

Definition at line 86 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED13[6U]

Reserved for future use

Definition at line 89 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED14[54U]

Reserved for future use

Definition at line 92 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED15[3U]

Reserved for future use

Definition at line 94 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED16[7U]

Reserved for future use

Definition at line 96 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED17[55U]

Reserved for future use

Definition at line 98 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED18[2U]

Reserved for future use

Definition at line 101 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED19[2U]

Reserved for future use

Definition at line 104 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED2[6U]

Reserved for future use

Definition at line 57 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED20[2U]

Reserved for future use

Definition at line 107 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED21[862U]

Reserved for future use

Definition at line 110 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED22[3U]

Reserved for future use

Definition at line 116 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED23[7U]

Reserved for future use

Definition at line 118 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED24[6U]

Reserved for future use

Definition at line 121 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED25[54U]

Reserved for future use

Definition at line 124 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED26[3U]

Reserved for future use

Definition at line 126 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED27[7U]

Reserved for future use

Definition at line 128 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED28[55U]

Reserved for future use

Definition at line 130 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED29[2U]

Reserved for future use

Definition at line 133 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED3[54U]

Reserved for future use

Definition at line 60 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED30[2U]

Reserved for future use

Definition at line 136 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED31[2U]

Reserved for future use

Definition at line 139 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED32[862U]

Reserved for future use

Definition at line 142 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED33[3U]

Reserved for future use

Definition at line 148 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED34[7U]

Reserved for future use

Definition at line 150 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED35[6U]

Reserved for future use

Definition at line 153 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED36[54U]

Reserved for future use

Definition at line 156 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED37[3U]

Reserved for future use

Definition at line 158 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED38[7U]

Reserved for future use

Definition at line 160 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED39[55U]

Reserved for future use

Definition at line 162 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED4[3U]

Reserved for future use

Definition at line 62 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED40[2U]

Reserved for future use

Definition at line 165 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED41[2U]

Reserved for future use

Definition at line 168 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED42[2U]

Reserved for future use

Definition at line 171 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED5[7U]

Reserved for future use

Definition at line 64 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED6[55U]

Reserved for future use

Definition at line 66 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED7[2U]

Reserved for future use

Definition at line 69 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED8[2U]

Reserved for future use

Definition at line 72 of file efr32bg21_smu.h.

uint32_t SMU_TypeDef::RESERVED9[2U]

Reserved for future use

Definition at line 75 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::STATUS

Status Register

Definition at line 48 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::STATUS_CLR

Status Register

Definition at line 112 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::STATUS_SET

Status Register

Definition at line 80 of file efr32bg21_smu.h.

__IM uint32_t SMU_TypeDef::STATUS_TGL

Status Register

Definition at line 144 of file efr32bg21_smu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_smu.h