SYNTH_TypeDef Struct ReferenceDevices > SYNTH

SYNTH Register Declaration.

Definition at line 46 of file efr32bg21_synth.h.

#include <efr32bg21_synth.h>

Data Fields

__IOM uint32_t CALOFFSET
 
__IOM uint32_t CALOFFSET_CLR
 
__IOM uint32_t CALOFFSET_SET
 
__IOM uint32_t CALOFFSET_TGL
 
__IOM uint32_t CHCTRL
 
__IOM uint32_t CHCTRL_CLR
 
__IOM uint32_t CHCTRL_SET
 
__IOM uint32_t CHCTRL_TGL
 
__IOM uint32_t CHPDACINIT
 
__IOM uint32_t CHPDACINIT_CLR
 
__IOM uint32_t CHPDACINIT_SET
 
__IOM uint32_t CHPDACINIT_TGL
 
__IOM uint32_t CHSP
 
__IOM uint32_t CHSP_CLR
 
__IOM uint32_t CHSP_SET
 
__IOM uint32_t CHSP_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t DIVCTRL
 
__IOM uint32_t DIVCTRL_CLR
 
__IOM uint32_t DIVCTRL_SET
 
__IOM uint32_t DIVCTRL_TGL
 
__IOM uint32_t DSMCTRLRX
 
__IOM uint32_t DSMCTRLRX_CLR
 
__IOM uint32_t DSMCTRLRX_SET
 
__IOM uint32_t DSMCTRLRX_TGL
 
__IOM uint32_t DSMCTRLTX
 
__IOM uint32_t DSMCTRLTX_CLR
 
__IOM uint32_t DSMCTRLTX_SET
 
__IOM uint32_t DSMCTRLTX_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t FREQ
 
__IOM uint32_t FREQ_CLR
 
__IOM uint32_t FREQ_SET
 
__IOM uint32_t FREQ_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IOM uint32_t IFFREQ
 
__IOM uint32_t IFFREQ_CLR
 
__IOM uint32_t IFFREQ_SET
 
__IOM uint32_t IFFREQ_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCNTCTRL
 
__IOM uint32_t LOCNTCTRL_CLR
 
__IOM uint32_t LOCNTCTRL_SET
 
__IOM uint32_t LOCNTCTRL_TGL
 
__IM uint32_t LOCNTSTATUS
 
__IM uint32_t LOCNTSTATUS_CLR
 
__IM uint32_t LOCNTSTATUS_SET
 
__IM uint32_t LOCNTSTATUS_TGL
 
__IM uint32_t LOCNTTARGET
 
__IM uint32_t LOCNTTARGET_CLR
 
__IM uint32_t LOCNTTARGET_SET
 
__IM uint32_t LOCNTTARGET_TGL
 
__IOM uint32_t LPFCTRL1CAL
 
__IOM uint32_t LPFCTRL1CAL_CLR
 
__IOM uint32_t LPFCTRL1CAL_SET
 
__IOM uint32_t LPFCTRL1CAL_TGL
 
__IOM uint32_t LPFCTRL1RX
 
__IOM uint32_t LPFCTRL1RX_CLR
 
__IOM uint32_t LPFCTRL1RX_SET
 
__IOM uint32_t LPFCTRL1RX_TGL
 
__IOM uint32_t LPFCTRL1TX
 
__IOM uint32_t LPFCTRL1TX_CLR
 
__IOM uint32_t LPFCTRL1TX_SET
 
__IOM uint32_t LPFCTRL1TX_TGL
 
__IOM uint32_t LPFCTRL2RX
 
__IOM uint32_t LPFCTRL2RX_CLR
 
__IOM uint32_t LPFCTRL2RX_SET
 
__IOM uint32_t LPFCTRL2RX_TGL
 
__IOM uint32_t LPFCTRL2TX
 
__IOM uint32_t LPFCTRL2TX_CLR
 
__IOM uint32_t LPFCTRL2TX_SET
 
__IOM uint32_t LPFCTRL2TX_TGL
 
__IOM uint32_t MMDDENOMINIT
 
__IOM uint32_t MMDDENOMINIT_CLR
 
__IOM uint32_t MMDDENOMINIT_SET
 
__IOM uint32_t MMDDENOMINIT_TGL
 
uint32_t RESERVED0 [6U]
 
uint32_t RESERVED1 [1U]
 
uint32_t RESERVED10 [2U]
 
uint32_t RESERVED11 [978U]
 
uint32_t RESERVED12 [6U]
 
uint32_t RESERVED13 [1U]
 
uint32_t RESERVED14 [2U]
 
uint32_t RESERVED15 [7U]
 
uint32_t RESERVED16 [2U]
 
uint32_t RESERVED17 [978U]
 
uint32_t RESERVED18 [6U]
 
uint32_t RESERVED19 [1U]
 
uint32_t RESERVED2 [2U]
 
uint32_t RESERVED20 [2U]
 
uint32_t RESERVED21 [7U]
 
uint32_t RESERVED22 [2U]
 
uint32_t RESERVED3 [7U]
 
uint32_t RESERVED4 [2U]
 
uint32_t RESERVED5 [978U]
 
uint32_t RESERVED6 [6U]
 
uint32_t RESERVED7 [1U]
 
uint32_t RESERVED8 [2U]
 
uint32_t RESERVED9 [7U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t VCDACCTRL
 
__IOM uint32_t VCDACCTRL_CLR
 
__IOM uint32_t VCDACCTRL_SET
 
__IOM uint32_t VCDACCTRL_TGL
 
__IOM uint32_t VCOGAIN
 
__IOM uint32_t VCOGAIN_CLR
 
__IOM uint32_t VCOGAIN_SET
 
__IOM uint32_t VCOGAIN_TGL
 
__IOM uint32_t VCOTUNING
 
__IOM uint32_t VCOTUNING_CLR
 
__IOM uint32_t VCOTUNING_SET
 
__IOM uint32_t VCOTUNING_TGL
 

Field Documentation

__IOM uint32_t SYNTH_TypeDef::CALOFFSET

Calibration offset

Definition at line 60 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CALOFFSET_CLR

Calibration offset

Definition at line 128 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CALOFFSET_SET

Calibration offset

Definition at line 94 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CALOFFSET_TGL

Calibration offset

Definition at line 162 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHCTRL

Frequency Synthesizer Channel Control

Definition at line 58 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHCTRL_CLR

Frequency Synthesizer Channel Control

Definition at line 126 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHCTRL_SET

Frequency Synthesizer Channel Control

Definition at line 92 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHCTRL_TGL

Frequency Synthesizer Channel Control

Definition at line 160 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHPDACINIT

Initial Value for CHP DAC

Definition at line 72 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHPDACINIT_CLR

Initial Value for CHP DAC

Definition at line 140 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHPDACINIT_SET

Initial Value for CHP DAC

Definition at line 106 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHPDACINIT_TGL

Initial Value for CHP DAC

Definition at line 174 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHSP

Channel spacing

Definition at line 59 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHSP_CLR

Channel spacing

Definition at line 127 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHSP_SET

Channel spacing

Definition at line 93 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CHSP_TGL

Channel spacing

Definition at line 161 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CMD

Command Register

Definition at line 50 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CMD_CLR

Command Register

Definition at line 118 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CMD_SET

Command Register

Definition at line 84 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CMD_TGL

Command Register

Definition at line 152 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CTRL

Frequency Synthesizer Control register

Definition at line 51 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CTRL_CLR

Frequency Synthesizer Control register

Definition at line 119 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CTRL_SET

Frequency Synthesizer Control register

Definition at line 85 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::CTRL_TGL

Frequency Synthesizer Control register

Definition at line 153 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DIVCTRL

Frequency division control

Definition at line 57 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DIVCTRL_CLR

Frequency division control

Definition at line 125 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DIVCTRL_SET

Frequency division control

Definition at line 91 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DIVCTRL_TGL

Frequency division control

Definition at line 159 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLRX

DSM Control register for RX mode

Definition at line 78 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLRX_CLR

DSM Control register for RX mode

Definition at line 146 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLRX_SET

DSM Control register for RX mode

Definition at line 112 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLRX_TGL

DSM Control register for RX mode

Definition at line 180 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLTX

DSM Control register for TX mode

Definition at line 79 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLTX_CLR

DSM Control register for TX mode

Definition at line 147 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLTX_SET

DSM Control register for TX mode

Definition at line 113 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::DSMCTRLTX_TGL

DSM Control register for TX mode

Definition at line 181 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::EN

Enable peripheral clock to this module

Definition at line 48 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::EN_CLR

Enable peripheral clock to this module

Definition at line 116 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::EN_SET

Enable peripheral clock to this module

Definition at line 82 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::EN_TGL

Enable peripheral clock to this module

Definition at line 150 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::FREQ

Frequency Word

Definition at line 55 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::FREQ_CLR

Frequency Word

Definition at line 123 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::FREQ_SET

Frequency Word

Definition at line 89 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::FREQ_TGL

Frequency Word

Definition at line 157 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IEN

Interrupt Enable Register

Definition at line 67 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 135 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 101 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 169 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IF

Interrupt Flag Register

Definition at line 65 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 133 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 99 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 167 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IFFREQ

IF frequency

Definition at line 56 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IFFREQ_CLR

IF frequency

Definition at line 124 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IFFREQ_SET

IF frequency

Definition at line 90 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::IFFREQ_TGL

IF frequency

Definition at line 158 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::IPVERSION

IP Version

Definition at line 47 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::IPVERSION_CLR

IP Version

Definition at line 115 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::IPVERSION_SET

IP Version

Definition at line 81 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::IPVERSION_TGL

IP Version

Definition at line 149 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LOCNTCTRL

LO Counter Control Register

Definition at line 68 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LOCNTCTRL_CLR

LO Counter Control Register

Definition at line 136 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LOCNTCTRL_SET

LO Counter Control Register

Definition at line 102 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LOCNTCTRL_TGL

LO Counter Control Register

Definition at line 170 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTSTATUS

LO Counter Status Register

Definition at line 69 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTSTATUS_CLR

LO Counter Status Register

Definition at line 137 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTSTATUS_SET

LO Counter Status Register

Definition at line 103 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTSTATUS_TGL

LO Counter Status Register

Definition at line 171 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTTARGET

LO Counter Target Value

Definition at line 70 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTTARGET_CLR

LO Counter Target Value

Definition at line 138 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTTARGET_SET

LO Counter Target Value

Definition at line 104 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::LOCNTTARGET_TGL

LO Counter Target Value

Definition at line 172 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1CAL

LPF control register 1 for CAL mode

Definition at line 73 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1CAL_CLR

LPF control register 1 for CAL mode

Definition at line 141 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1CAL_SET

LPF control register 1 for CAL mode

Definition at line 107 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1CAL_TGL

LPF control register 1 for CAL mode

Definition at line 175 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1RX

LPF control register 1 for RX mode

Definition at line 74 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1RX_CLR

LPF control register 1 for RX mode

Definition at line 142 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1RX_SET

LPF control register 1 for RX mode

Definition at line 108 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1RX_TGL

LPF control register 1 for RX mode

Definition at line 176 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1TX

LPF control register 1 for TX mode

Definition at line 75 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1TX_CLR

LPF control register 1 for TX mode

Definition at line 143 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1TX_SET

LPF control register 1 for TX mode

Definition at line 109 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL1TX_TGL

LPF control register 1 for TX mode

Definition at line 177 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2RX

LPF control register 2 for RX mode

Definition at line 76 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2RX_CLR

LPF control register 2 for RX mode

Definition at line 144 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2RX_SET

LPF control register 2 for RX mode

Definition at line 110 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2RX_TGL

LPF control register 2 for RX mode

Definition at line 178 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2TX

LPF control register 2 for TX mode

Definition at line 77 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2TX_CLR

LPF control register 2 for TX mode

Definition at line 145 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2TX_SET

LPF control register 2 for TX mode

Definition at line 111 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::LPFCTRL2TX_TGL

LPF control register 2 for TX mode

Definition at line 179 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::MMDDENOMINIT

Initial Values for MMD Denom

Definition at line 71 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::MMDDENOMINIT_CLR

Initial Values for MMD Denom

Definition at line 139 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::MMDDENOMINIT_SET

Initial Values for MMD Denom

Definition at line 105 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::MMDDENOMINIT_TGL

Initial Values for MMD Denom

Definition at line 173 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED0[6U]

Reserved for future use

Definition at line 52 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED1[1U]

Reserved for future use

Definition at line 54 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED10[2U]

Reserved for future use

Definition at line 100 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED11[978U]

Reserved for future use

Definition at line 114 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED12[6U]

Reserved for future use

Definition at line 120 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED13[1U]

Reserved for future use

Definition at line 122 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED14[2U]

Reserved for future use

Definition at line 130 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED15[7U]

Reserved for future use

Definition at line 132 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED16[2U]

Reserved for future use

Definition at line 134 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED17[978U]

Reserved for future use

Definition at line 148 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED18[6U]

Reserved for future use

Definition at line 154 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED19[1U]

Reserved for future use

Definition at line 156 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED2[2U]

Reserved for future use

Definition at line 62 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED20[2U]

Reserved for future use

Definition at line 164 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED21[7U]

Reserved for future use

Definition at line 166 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED22[2U]

Reserved for future use

Definition at line 168 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED3[7U]

Reserved for future use

Definition at line 64 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED4[2U]

Reserved for future use

Definition at line 66 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED5[978U]

Reserved for future use

Definition at line 80 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED6[6U]

Reserved for future use

Definition at line 86 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED7[1U]

Reserved for future use

Definition at line 88 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED8[2U]

Reserved for future use

Definition at line 96 of file efr32bg21_synth.h.

uint32_t SYNTH_TypeDef::RESERVED9[7U]

Reserved for future use

Definition at line 98 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::STATUS

Frequency Synthesizer Status

Definition at line 49 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::STATUS_CLR

Frequency Synthesizer Status

Definition at line 117 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::STATUS_SET

Frequency Synthesizer Status

Definition at line 83 of file efr32bg21_synth.h.

__IM uint32_t SYNTH_TypeDef::STATUS_TGL

Frequency Synthesizer Status

Definition at line 151 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCDACCTRL

VCDAC Control register

Definition at line 53 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCDACCTRL_CLR

VCDAC Control register

Definition at line 121 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCDACCTRL_SET

VCDAC Control register

Definition at line 87 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCDACCTRL_TGL

VCDAC Control register

Definition at line 155 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOGAIN

Calibration values for VCO gain

Definition at line 63 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOGAIN_CLR

Calibration values for VCO gain

Definition at line 131 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOGAIN_SET

Calibration values for VCO gain

Definition at line 97 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOGAIN_TGL

Calibration values for VCO gain

Definition at line 165 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOTUNING

VCO Frequency tuning

Definition at line 61 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOTUNING_CLR

VCO Frequency tuning

Definition at line 129 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOTUNING_SET

VCO Frequency tuning

Definition at line 95 of file efr32bg21_synth.h.

__IOM uint32_t SYNTH_TypeDef::VCOTUNING_TGL

VCO Frequency tuning

Definition at line 163 of file efr32bg21_synth.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_synth.h