SYSCFG_TypeDef Struct ReferenceDevices > SYSCFG

SYSCFG Register Declaration.

Definition at line 46 of file efr32bg21_syscfg.h.

#include <efr32bg21_syscfg.h>

Data Fields

__IOM uint32_t CHIPREV
 
__IOM uint32_t CHIPREV_CLR
 
__IOM uint32_t CHIPREV_SET
 
__IOM uint32_t CHIPREV_TGL
 
__IOM uint32_t CHIPREVHW
 
__IOM uint32_t CHIPREVHW_CLR
 
__IOM uint32_t CHIPREVHW_SET
 
__IOM uint32_t CHIPREVHW_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IM uint32_t DMEM0ECCADDR
 
__IM uint32_t DMEM0ECCADDR_CLR
 
__IM uint32_t DMEM0ECCADDR_SET
 
__IM uint32_t DMEM0ECCADDR_TGL
 
__IOM uint32_t DMEM0ECCCTRL
 
__IOM uint32_t DMEM0ECCCTRL_CLR
 
__IOM uint32_t DMEM0ECCCTRL_SET
 
__IOM uint32_t DMEM0ECCCTRL_TGL
 
__IOM uint32_t DMEM0RAMCTRL
 
__IOM uint32_t DMEM0RAMCTRL_CLR
 
__IOM uint32_t DMEM0RAMCTRL_SET
 
__IOM uint32_t DMEM0RAMCTRL_TGL
 
__IOM uint32_t DMEM0RETNCTRL
 
__IOM uint32_t DMEM0RETNCTRL_CLR
 
__IOM uint32_t DMEM0RETNCTRL_SET
 
__IOM uint32_t DMEM0RETNCTRL_TGL
 
__IM uint32_t FRCRAMECCADDR
 
__IM uint32_t FRCRAMECCADDR_CLR
 
__IM uint32_t FRCRAMECCADDR_SET
 
__IM uint32_t FRCRAMECCADDR_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IOM uint32_t RADIOECCCTRL
 
__IOM uint32_t RADIOECCCTRL_CLR
 
__IOM uint32_t RADIOECCCTRL_SET
 
__IOM uint32_t RADIOECCCTRL_TGL
 
__IOM uint32_t RADIORAMCTRL
 
__IOM uint32_t RADIORAMCTRL_CLR
 
__IOM uint32_t RADIORAMCTRL_SET
 
__IOM uint32_t RADIORAMCTRL_TGL
 
__IOM uint32_t RADIORAMRETNCTRL
 
__IOM uint32_t RADIORAMRETNCTRL_CLR
 
__IOM uint32_t RADIORAMRETNCTRL_SET
 
__IOM uint32_t RADIORAMRETNCTRL_TGL
 
uint32_t RESERVED0 [2U]
 
uint32_t RESERVED1 [58U]
 
uint32_t RESERVED10 [58U]
 
uint32_t RESERVED11 [1U]
 
uint32_t RESERVED12 [63U]
 
uint32_t RESERVED13 [1U]
 
uint32_t RESERVED14 [1U]
 
uint32_t RESERVED15 [121U]
 
uint32_t RESERVED16 [1U]
 
uint32_t RESERVED17 [762U]
 
uint32_t RESERVED18 [2U]
 
uint32_t RESERVED19 [58U]
 
uint32_t RESERVED2 [1U]
 
uint32_t RESERVED20 [1U]
 
uint32_t RESERVED21 [63U]
 
uint32_t RESERVED22 [1U]
 
uint32_t RESERVED23 [1U]
 
uint32_t RESERVED24 [121U]
 
uint32_t RESERVED25 [1U]
 
uint32_t RESERVED26 [762U]
 
uint32_t RESERVED27 [2U]
 
uint32_t RESERVED28 [58U]
 
uint32_t RESERVED29 [1U]
 
uint32_t RESERVED3 [63U]
 
uint32_t RESERVED30 [63U]
 
uint32_t RESERVED31 [1U]
 
uint32_t RESERVED32 [1U]
 
uint32_t RESERVED33 [121U]
 
uint32_t RESERVED34 [1U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [1U]
 
uint32_t RESERVED6 [121U]
 
uint32_t RESERVED7 [1U]
 
uint32_t RESERVED8 [762U]
 
uint32_t RESERVED9 [2U]
 
__IM uint32_t SEQRAMECCADDR
 
__IM uint32_t SEQRAMECCADDR_CLR
 
__IM uint32_t SEQRAMECCADDR_SET
 
__IM uint32_t SEQRAMECCADDR_TGL
 

Field Documentation

__IOM uint32_t SYSCFG_TypeDef::CHIPREV

Part Family and Revision values

Definition at line 51 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREV_CLR

Part Family and Revision values

Definition at line 97 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREV_SET

Part Family and Revision values

Definition at line 74 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREV_TGL

Part Family and Revision values

Definition at line 120 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREVHW

Hardwired Chip Rev values

Definition at line 50 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREVHW_CLR

Hardwired Chip Rev values

Definition at line 96 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREVHW_SET

Hardwired Chip Rev values

Definition at line 73 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CHIPREVHW_TGL

Hardwired Chip Rev values

Definition at line 119 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CTRL

Memory System Control Register

Definition at line 55 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CTRL_CLR

Memory System Control Register

Definition at line 101 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CTRL_SET

Memory System Control Register

Definition at line 78 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::CTRL_TGL

Memory System Control Register

Definition at line 124 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::DMEM0ECCADDR

DMEM ECC Error Address Register

Definition at line 59 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::DMEM0ECCADDR_CLR

DMEM ECC Error Address Register

Definition at line 105 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::DMEM0ECCADDR_SET

DMEM ECC Error Address Register

Definition at line 82 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::DMEM0ECCADDR_TGL

DMEM ECC Error Address Register

Definition at line 128 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0ECCCTRL

DMEM ECC Control Register

Definition at line 60 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0ECCCTRL_CLR

DMEM ECC Control Register

Definition at line 106 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0ECCCTRL_SET

DMEM ECC Control Register

Definition at line 83 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0ECCCTRL_TGL

DMEM ECC Control Register

Definition at line 129 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RAMCTRL

DMEM Control enable Register

Definition at line 61 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RAMCTRL_CLR

DMEM Control enable Register

Definition at line 107 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RAMCTRL_SET

DMEM Control enable Register

Definition at line 84 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RAMCTRL_TGL

DMEM Control enable Register

Definition at line 130 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RETNCTRL

DMEM retention Control Register

Definition at line 57 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RETNCTRL_CLR

DMEM retention Control Register

Definition at line 103 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RETNCTRL_SET

DMEM retention Control Register

Definition at line 80 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::DMEM0RETNCTRL_TGL

DMEM retention Control Register

Definition at line 126 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::FRCRAMECCADDR

FRCRAM ECC Error Address Register

Definition at line 68 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::FRCRAMECCADDR_CLR

FRCRAM ECC Error Address Register

Definition at line 114 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::FRCRAMECCADDR_SET

FRCRAM ECC Error Address Register

Definition at line 91 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::FRCRAMECCADDR_TGL

FRCRAM ECC Error Address Register

Definition at line 137 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IEN

Interrupt Enable Register

Definition at line 48 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 94 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 71 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 117 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IF

Interrupt Flag Register

Definition at line 47 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 93 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 70 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 116 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIOECCCTRL

RADIO RAM ECC Control Register

Definition at line 65 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIOECCCTRL_CLR

RADIO RAM ECC Control Register

Definition at line 111 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIOECCCTRL_SET

RADIO RAM ECC Control Register

Definition at line 88 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIOECCCTRL_TGL

RADIO RAM ECC Control Register

Definition at line 134 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMCTRL

RADIO RAM Control Register

Definition at line 66 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMCTRL_CLR

RADIO RAM Control Register

Definition at line 112 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMCTRL_SET

RADIO RAM Control Register

Definition at line 89 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMCTRL_TGL

RADIO RAM Control Register

Definition at line 135 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMRETNCTRL

RADIO RAM retention Control Register

Definition at line 63 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMRETNCTRL_CLR

RADIO RAM retention Control Register

Definition at line 109 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMRETNCTRL_SET

RADIO RAM retention Control Register

Definition at line 86 of file efr32bg21_syscfg.h.

__IOM uint32_t SYSCFG_TypeDef::RADIORAMRETNCTRL_TGL

RADIO RAM retention Control Register

Definition at line 132 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED0[2U]

Reserved for future use

Definition at line 49 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED1[58U]

Reserved for future use

Definition at line 52 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED10[58U]

Reserved for future use

Definition at line 75 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED11[1U]

Reserved for future use

Definition at line 76 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED12[63U]

Reserved for future use

Definition at line 77 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED13[1U]

Reserved for future use

Definition at line 79 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED14[1U]

Reserved for future use

Definition at line 81 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED15[121U]

Reserved for future use

Definition at line 85 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED16[1U]

Reserved for future use

Definition at line 87 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED17[762U]

Reserved for future use

Definition at line 92 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED18[2U]

Reserved for future use

Definition at line 95 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED19[58U]

Reserved for future use

Definition at line 98 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED2[1U]

Reserved for future use

Definition at line 53 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED20[1U]

Reserved for future use

Definition at line 99 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED21[63U]

Reserved for future use

Definition at line 100 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED22[1U]

Reserved for future use

Definition at line 102 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED23[1U]

Reserved for future use

Definition at line 104 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED24[121U]

Reserved for future use

Definition at line 108 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED25[1U]

Reserved for future use

Definition at line 110 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED26[762U]

Reserved for future use

Definition at line 115 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED27[2U]

Reserved for future use

Definition at line 118 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED28[58U]

Reserved for future use

Definition at line 121 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED29[1U]

Reserved for future use

Definition at line 122 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED3[63U]

Reserved for future use

Definition at line 54 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED30[63U]

Reserved for future use

Definition at line 123 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED31[1U]

Reserved for future use

Definition at line 125 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED32[1U]

Reserved for future use

Definition at line 127 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED33[121U]

Reserved for future use

Definition at line 131 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED34[1U]

Reserved for future use

Definition at line 133 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 56 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED5[1U]

Reserved for future use

Definition at line 58 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED6[121U]

Reserved for future use

Definition at line 62 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED7[1U]

Reserved for future use

Definition at line 64 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED8[762U]

Reserved for future use

Definition at line 69 of file efr32bg21_syscfg.h.

uint32_t SYSCFG_TypeDef::RESERVED9[2U]

Reserved for future use

Definition at line 72 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::SEQRAMECCADDR

SEQRAM ECC Error Address Register

Definition at line 67 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::SEQRAMECCADDR_CLR

SEQRAM ECC Error Address Register

Definition at line 113 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::SEQRAMECCADDR_SET

SEQRAM ECC Error Address Register

Definition at line 90 of file efr32bg21_syscfg.h.

__IM uint32_t SYSCFG_TypeDef::SEQRAMECCADDR_TGL

SEQRAM ECC Error Address Register

Definition at line 136 of file efr32bg21_syscfg.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_syscfg.h