TIMER_CC_TypeDef Struct ReferenceDevices > TIMER

TIMER CC Register Group Declaration.

Definition at line 46 of file efr32bg21_timer.h.

#include <efr32bg21_timer.h>

Data Fields

__IOM uint32_t CFG
 
__IOM uint32_t CTRL
 
__IM uint32_t ICF
 
__IM uint32_t ICOF
 
__IOM uint32_t OC
 
__IOM uint32_t OCB
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [1U]
 

Field Documentation

__IOM uint32_t TIMER_CC_TypeDef::CFG

CC Channel Configuration Register

Definition at line 47 of file efr32bg21_timer.h.

Referenced by TIMER_CaptureBufGet(), TIMER_CaptureGet(), TIMER_InitCC(), and TIMER_Reset().

__IOM uint32_t TIMER_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 48 of file efr32bg21_timer.h.

Referenced by TIMER_InitCC(), and TIMER_Reset().

__IM uint32_t TIMER_CC_TypeDef::ICF

IC Channel Value Register

Definition at line 52 of file efr32bg21_timer.h.

Referenced by TIMER_CaptureGet().

__IM uint32_t TIMER_CC_TypeDef::ICOF

IC Channel Value Overflow Register

Definition at line 53 of file efr32bg21_timer.h.

Referenced by TIMER_CaptureBufGet().

__IOM uint32_t TIMER_CC_TypeDef::OC

OC Channel Value Register

Definition at line 49 of file efr32bg21_timer.h.

Referenced by TIMER_CaptureGet(), TIMER_CompareSet(), and TIMER_Reset().

__IOM uint32_t TIMER_CC_TypeDef::OCB

OC Channel Value Buffer Register

Definition at line 51 of file efr32bg21_timer.h.

Referenced by TIMER_CaptureBufGet(), TIMER_CompareBufSet(), and TIMER_Reset().

uint32_t TIMER_CC_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 50 of file efr32bg21_timer.h.

uint32_t TIMER_CC_TypeDef::RESERVED1[1U]

Reserved for future use

Definition at line 54 of file efr32bg21_timer.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_timer.h