USART_TypeDef Struct ReferenceDevices > USART

USART Register Declaration.

Definition at line 46 of file efr32bg21_usart.h.

#include <efr32bg21_usart.h>

Data Fields

__IOM uint32_t CLKDIV
 
__IOM uint32_t CLKDIV_CLR
 
__IOM uint32_t CLKDIV_SET
 
__IOM uint32_t CLKDIV_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t CTRLX
 
__IOM uint32_t CTRLX_CLR
 
__IOM uint32_t CTRLX_SET
 
__IOM uint32_t CTRLX_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t FRAME
 
__IOM uint32_t FRAME_CLR
 
__IOM uint32_t FRAME_SET
 
__IOM uint32_t FRAME_TGL
 
__IOM uint32_t I2SCTRL
 
__IOM uint32_t I2SCTRL_CLR
 
__IOM uint32_t I2SCTRL_SET
 
__IOM uint32_t I2SCTRL_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t IRCTRL
 
__IOM uint32_t IRCTRL_CLR
 
__IOM uint32_t IRCTRL_SET
 
__IOM uint32_t IRCTRL_TGL
 
uint32_t RESERVED0 [997U]
 
uint32_t RESERVED1 [997U]
 
uint32_t RESERVED2 [997U]
 
__IM uint32_t RXDATA
 
__IM uint32_t RXDATA_CLR
 
__IM uint32_t RXDATA_SET
 
__IM uint32_t RXDATA_TGL
 
__IM uint32_t RXDATAX
 
__IM uint32_t RXDATAX_CLR
 
__IM uint32_t RXDATAX_SET
 
__IM uint32_t RXDATAX_TGL
 
__IM uint32_t RXDATAXP
 
__IM uint32_t RXDATAXP_CLR
 
__IM uint32_t RXDATAXP_SET
 
__IM uint32_t RXDATAXP_TGL
 
__IM uint32_t RXDOUBLE
 
__IM uint32_t RXDOUBLE_CLR
 
__IM uint32_t RXDOUBLE_SET
 
__IM uint32_t RXDOUBLE_TGL
 
__IM uint32_t RXDOUBLEX
 
__IM uint32_t RXDOUBLEX_CLR
 
__IM uint32_t RXDOUBLEX_SET
 
__IM uint32_t RXDOUBLEX_TGL
 
__IM uint32_t RXDOUBLEXP
 
__IM uint32_t RXDOUBLEXP_CLR
 
__IM uint32_t RXDOUBLEXP_SET
 
__IM uint32_t RXDOUBLEXP_TGL
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t TIMECMP0
 
__IOM uint32_t TIMECMP0_CLR
 
__IOM uint32_t TIMECMP0_SET
 
__IOM uint32_t TIMECMP0_TGL
 
__IOM uint32_t TIMECMP1
 
__IOM uint32_t TIMECMP1_CLR
 
__IOM uint32_t TIMECMP1_SET
 
__IOM uint32_t TIMECMP1_TGL
 
__IOM uint32_t TIMECMP2
 
__IOM uint32_t TIMECMP2_CLR
 
__IOM uint32_t TIMECMP2_SET
 
__IOM uint32_t TIMECMP2_TGL
 
__IOM uint32_t TIMING
 
__IOM uint32_t TIMING_CLR
 
__IOM uint32_t TIMING_SET
 
__IOM uint32_t TIMING_TGL
 
__IOM uint32_t TRIGCTRL
 
__IOM uint32_t TRIGCTRL_CLR
 
__IOM uint32_t TRIGCTRL_SET
 
__IOM uint32_t TRIGCTRL_TGL
 
__IOM uint32_t TXDATA
 
__IOM uint32_t TXDATA_CLR
 
__IOM uint32_t TXDATA_SET
 
__IOM uint32_t TXDATA_TGL
 
__IOM uint32_t TXDATAX
 
__IOM uint32_t TXDATAX_CLR
 
__IOM uint32_t TXDATAX_SET
 
__IOM uint32_t TXDATAX_TGL
 
__IOM uint32_t TXDOUBLE
 
__IOM uint32_t TXDOUBLE_CLR
 
__IOM uint32_t TXDOUBLE_SET
 
__IOM uint32_t TXDOUBLE_TGL
 
__IOM uint32_t TXDOUBLEX
 
__IOM uint32_t TXDOUBLEX_CLR
 
__IOM uint32_t TXDOUBLEX_SET
 
__IOM uint32_t TXDOUBLEX_TGL
 

Field Documentation

__IOM uint32_t USART_TypeDef::CLKDIV

Clock Control Register

Definition at line 54 of file efr32bg21_usart.h.

Referenced by USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_BaudrateSyncSet(), and USART_Reset().

__IOM uint32_t USART_TypeDef::CLKDIV_CLR

Clock Control Register

Definition at line 110 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CLKDIV_SET

Clock Control Register

Definition at line 82 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CLKDIV_TGL

Clock Control Register

Definition at line 138 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CMD

Command Register

Definition at line 52 of file efr32bg21_usart.h.

Referenced by UARTDRV_InitUart(), USART_Enable(), USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::CMD_CLR

Command Register

Definition at line 108 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CMD_SET

Command Register

Definition at line 80 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CMD_TGL

Command Register

Definition at line 136 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CTRL

Control Register

Definition at line 49 of file efr32bg21_usart.h.

Referenced by SPIDRV_Init(), USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_InitAsync(), USART_InitSync(), USART_Reset(), and USARTn_InitIrDA().

__IOM uint32_t USART_TypeDef::CTRL_CLR

Control Register

Definition at line 105 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CTRL_SET

Control Register

Definition at line 77 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CTRL_TGL

Control Register

Definition at line 133 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::CTRLX

Control Register Extended

Definition at line 70 of file efr32bg21_usart.h.

Referenced by prsRxInput(), UARTDRV_InitUart(), and USART_Reset().

__IOM uint32_t USART_TypeDef::CTRLX_CLR

Control Register Extended

Definition at line 126 of file efr32bg21_usart.h.

Referenced by USART_InitAsync().

__IOM uint32_t USART_TypeDef::CTRLX_SET

Control Register Extended

Definition at line 98 of file efr32bg21_usart.h.

Referenced by UARTDRV_InitUart(), and USART_InitAsync().

__IOM uint32_t USART_TypeDef::CTRLX_TGL

Control Register Extended

Definition at line 154 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::EN

USART Enable

Definition at line 48 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::EN_CLR

USART Enable

Definition at line 104 of file efr32bg21_usart.h.

Referenced by USART_Enable(), and USART_Reset().

__IOM uint32_t USART_TypeDef::EN_SET

USART Enable

Definition at line 76 of file efr32bg21_usart.h.

Referenced by USART_Enable(), USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::EN_TGL

USART Enable

Definition at line 132 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::FRAME

USART Frame Format Register

Definition at line 50 of file efr32bg21_usart.h.

Referenced by USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::FRAME_CLR

USART Frame Format Register

Definition at line 106 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::FRAME_SET

USART Frame Format Register

Definition at line 78 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::FRAME_TGL

USART Frame Format Register

Definition at line 134 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::I2SCTRL

I2S Control Register

Definition at line 68 of file efr32bg21_usart.h.

Referenced by USART_InitI2s(), and USART_Reset().

__IOM uint32_t USART_TypeDef::I2SCTRL_CLR

I2S Control Register

Definition at line 124 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::I2SCTRL_SET

I2S Control Register

Definition at line 96 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::I2SCTRL_TGL

I2S Control Register

Definition at line 152 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IEN

Interrupt Enable Register

Definition at line 66 of file efr32bg21_usart.h.

Referenced by USART_IntDisable(), USART_IntEnable(), USART_IntGetEnabled(), and USART_Reset().

__IOM uint32_t USART_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 122 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 94 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 150 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IF

Interrupt Flag Register

Definition at line 65 of file efr32bg21_usart.h.

Referenced by USART_IntGet(), and USART_IntGetEnabled().

__IOM uint32_t USART_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 121 of file efr32bg21_usart.h.

Referenced by USART_IntClear(), and USART_Reset().

__IOM uint32_t USART_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 93 of file efr32bg21_usart.h.

Referenced by USART_IntSet().

__IOM uint32_t USART_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 149 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::IPVERSION

IPVERSION

Definition at line 47 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::IPVERSION_CLR

IPVERSION

Definition at line 103 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::IPVERSION_SET

IPVERSION

Definition at line 75 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::IPVERSION_TGL

IPVERSION

Definition at line 131 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IRCTRL

IrDA Control Register

Definition at line 67 of file efr32bg21_usart.h.

Referenced by prsIrInput(), USART_Reset(), and USARTn_InitIrDA().

__IOM uint32_t USART_TypeDef::IRCTRL_CLR

IrDA Control Register

Definition at line 123 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IRCTRL_SET

IrDA Control Register

Definition at line 95 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::IRCTRL_TGL

IrDA Control Register

Definition at line 151 of file efr32bg21_usart.h.

uint32_t USART_TypeDef::RESERVED0[997U]

Reserved for future use

Definition at line 74 of file efr32bg21_usart.h.

uint32_t USART_TypeDef::RESERVED1[997U]

Reserved for future use

Definition at line 102 of file efr32bg21_usart.h.

uint32_t USART_TypeDef::RESERVED2[997U]

Reserved for future use

Definition at line 130 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATA

RX Buffer Data Register

Definition at line 56 of file efr32bg21_usart.h.

Referenced by USART_Rx(), USART_RxDataGet(), and USART_SpiTransfer().

__IM uint32_t USART_TypeDef::RXDATA_CLR

RX Buffer Data Register

Definition at line 112 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATA_SET

RX Buffer Data Register

Definition at line 84 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATA_TGL

RX Buffer Data Register

Definition at line 140 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAX

RX Buffer Data Extended Register

Definition at line 55 of file efr32bg21_usart.h.

Referenced by USART_RxDataXGet(), and USART_RxExt().

__IM uint32_t USART_TypeDef::RXDATAX_CLR

RX Buffer Data Extended Register

Definition at line 111 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAX_SET

RX Buffer Data Extended Register

Definition at line 83 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAX_TGL

RX Buffer Data Extended Register

Definition at line 139 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAXP

RX Buffer Data Extended Peek Register

Definition at line 59 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAXP_CLR

RX Buffer Data Extended Peek Register

Definition at line 115 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAXP_SET

RX Buffer Data Extended Peek Register

Definition at line 87 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDATAXP_TGL

RX Buffer Data Extended Peek Register

Definition at line 143 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLE

RX FIFO Double Data Register

Definition at line 58 of file efr32bg21_usart.h.

Referenced by USART_RxDouble(), and USART_RxDoubleGet().

__IM uint32_t USART_TypeDef::RXDOUBLE_CLR

RX FIFO Double Data Register

Definition at line 114 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLE_SET

RX FIFO Double Data Register

Definition at line 86 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLE_TGL

RX FIFO Double Data Register

Definition at line 142 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEX

RX Buffer Double Data Extended Register

Definition at line 57 of file efr32bg21_usart.h.

Referenced by USART_RxDoubleExt(), and USART_RxDoubleXGet().

__IM uint32_t USART_TypeDef::RXDOUBLEX_CLR

RX Buffer Double Data Extended Register

Definition at line 113 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEX_SET

RX Buffer Double Data Extended Register

Definition at line 85 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEX_TGL

RX Buffer Double Data Extended Register

Definition at line 141 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEXP

RX Buffer Double Data Extended Peek R...

Definition at line 60 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEXP_CLR

RX Buffer Double Data Extended Peek R...

Definition at line 116 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEXP_SET

RX Buffer Double Data Extended Peek R...

Definition at line 88 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLEXP_TGL

RX Buffer Double Data Extended Peek R...

Definition at line 144 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::STATUS

USART Status Register

Definition at line 53 of file efr32bg21_usart.h.

Referenced by USART_Rx(), USART_RxDouble(), USART_RxDoubleExt(), USART_RxExt(), USART_SpiTransfer(), USART_StatusGet(), USART_Tx(), USART_TxDouble(), USART_TxDoubleExt(), and USART_TxExt().

__IM uint32_t USART_TypeDef::STATUS_CLR

USART Status Register

Definition at line 109 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::STATUS_SET

USART Status Register

Definition at line 81 of file efr32bg21_usart.h.

__IM uint32_t USART_TypeDef::STATUS_TGL

USART Status Register

Definition at line 137 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP0

Used to generate interrupts and vario...

Definition at line 71 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP0_CLR

Used to generate interrupts and vario...

Definition at line 127 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP0_SET

Used to generate interrupts and vario...

Definition at line 99 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP0_TGL

Used to generate interrupts and vario...

Definition at line 155 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP1

Used to generate interrupts and vario...

Definition at line 72 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP1_CLR

Used to generate interrupts and vario...

Definition at line 128 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP1_SET

Used to generate interrupts and vario...

Definition at line 100 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP1_TGL

Used to generate interrupts and vario...

Definition at line 156 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP2

Used to generate interrupts and vario...

Definition at line 73 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP2_CLR

Used to generate interrupts and vario...

Definition at line 129 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP2_SET

Used to generate interrupts and vario...

Definition at line 101 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP2_TGL

Used to generate interrupts and vario...

Definition at line 157 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMING

Timing Register

Definition at line 69 of file efr32bg21_usart.h.

Referenced by USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::TIMING_CLR

Timing Register

Definition at line 125 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMING_SET

Timing Register

Definition at line 97 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TIMING_TGL

Timing Register

Definition at line 153 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TRIGCTRL

USART Trigger Control register

Definition at line 51 of file efr32bg21_usart.h.

Referenced by prsTriggerInput(), USART_InitPrsTrigger(), and USART_Reset().

__IOM uint32_t USART_TypeDef::TRIGCTRL_CLR

USART Trigger Control register

Definition at line 107 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TRIGCTRL_SET

USART Trigger Control register

Definition at line 79 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TRIGCTRL_TGL

USART Trigger Control register

Definition at line 135 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDATA

TX Buffer Data Register

Definition at line 62 of file efr32bg21_usart.h.

Referenced by USART_SpiTransfer(), and USART_Tx().

__IOM uint32_t USART_TypeDef::TXDATA_CLR

TX Buffer Data Register

Definition at line 118 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDATA_SET

TX Buffer Data Register

Definition at line 90 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDATA_TGL

TX Buffer Data Register

Definition at line 146 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDATAX

TX Buffer Data Extended Register

Definition at line 61 of file efr32bg21_usart.h.

Referenced by USART_TxExt().

__IOM uint32_t USART_TypeDef::TXDATAX_CLR

TX Buffer Data Extended Register

Definition at line 117 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDATAX_SET

TX Buffer Data Extended Register

Definition at line 89 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDATAX_TGL

TX Buffer Data Extended Register

Definition at line 145 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDOUBLE

TX Buffer Double Data Register

Definition at line 64 of file efr32bg21_usart.h.

Referenced by USART_TxDouble().

__IOM uint32_t USART_TypeDef::TXDOUBLE_CLR

TX Buffer Double Data Register

Definition at line 120 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDOUBLE_SET

TX Buffer Double Data Register

Definition at line 92 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDOUBLE_TGL

TX Buffer Double Data Register

Definition at line 148 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDOUBLEX

TX Buffer Double Data Extended Register

Definition at line 63 of file efr32bg21_usart.h.

Referenced by USART_TxDoubleExt().

__IOM uint32_t USART_TypeDef::TXDOUBLEX_CLR

TX Buffer Double Data Extended Register

Definition at line 119 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDOUBLEX_SET

TX Buffer Double Data Extended Register

Definition at line 91 of file efr32bg21_usart.h.

__IOM uint32_t USART_TypeDef::TXDOUBLEX_TGL

TX Buffer Double Data Extended Register

Definition at line 147 of file efr32bg21_usart.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_usart.h