WDOG_TypeDef Struct ReferenceDevices > WDOG

WDOG Register Declaration.

Definition at line 46 of file efr32bg21_wdog.h.

#include <efr32bg21_wdog.h>

Data Fields

__IOM uint32_t CFG
 
__IOM uint32_t CFG_CLR
 
__IOM uint32_t CFG_SET
 
__IOM uint32_t CFG_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [1014U]
 
uint32_t RESERVED2 [1U]
 
uint32_t RESERVED3 [1014U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [1014U]
 
uint32_t RESERVED6 [1U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IM uint32_t SYNCBUSY
 
__IM uint32_t SYNCBUSY_CLR
 
__IM uint32_t SYNCBUSY_SET
 
__IM uint32_t SYNCBUSY_TGL
 

Field Documentation

__IOM uint32_t WDOG_TypeDef::CFG

Configuration Register

Definition at line 49 of file efr32bg21_wdog.h.

Referenced by WDOGn_Init().

__IOM uint32_t WDOG_TypeDef::CFG_CLR

Configuration Register

Definition at line 71 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::CFG_SET

Configuration Register

Definition at line 60 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::CFG_TGL

Configuration Register

Definition at line 82 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::CMD

Command Register

Definition at line 50 of file efr32bg21_wdog.h.

Referenced by WDOGn_Feed().

__IOM uint32_t WDOG_TypeDef::CMD_CLR

Command Register

Definition at line 72 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::CMD_SET

Command Register

Definition at line 61 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::CMD_TGL

Command Register

Definition at line 83 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::EN

Enable Register

Definition at line 48 of file efr32bg21_wdog.h.

Referenced by WDOGn_Feed(), WDOGn_Init(), WDOGn_IsEnabled(), and WDOGn_SyncWait().

__IOM uint32_t WDOG_TypeDef::EN_CLR

Enable Register

Definition at line 70 of file efr32bg21_wdog.h.

Referenced by WDOGn_Enable(), and WDOGn_Init().

__IOM uint32_t WDOG_TypeDef::EN_SET

Enable Register

Definition at line 59 of file efr32bg21_wdog.h.

Referenced by WDOGn_Enable().

__IOM uint32_t WDOG_TypeDef::EN_TGL

Enable Register

Definition at line 81 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::IEN

Interrupt Enable Register

Definition at line 54 of file efr32bg21_wdog.h.

Referenced by WDOGn_IntDisable(), WDOGn_IntEnable(), and WDOGn_IntGetEnabled().

__IOM uint32_t WDOG_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 76 of file efr32bg21_wdog.h.

Referenced by WDOGn_IntDisable().

__IOM uint32_t WDOG_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 65 of file efr32bg21_wdog.h.

Referenced by WDOGn_IntEnable().

__IOM uint32_t WDOG_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 87 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efr32bg21_wdog.h.

Referenced by WDOGn_IntGet(), and WDOGn_IntGetEnabled().

__IOM uint32_t WDOG_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 75 of file efr32bg21_wdog.h.

Referenced by WDOGn_IntClear().

__IOM uint32_t WDOG_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 64 of file efr32bg21_wdog.h.

Referenced by WDOGn_IntSet().

__IOM uint32_t WDOG_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 86 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::IPVERSION

IP Version Register

Definition at line 47 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::IPVERSION_CLR

IP Version Register

Definition at line 69 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::IPVERSION_SET

IP Version Register

Definition at line 58 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::IPVERSION_TGL

IP Version Register

Definition at line 80 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::LOCK

Lock Register

Definition at line 55 of file efr32bg21_wdog.h.

Referenced by WDOGn_Lock(), and WDOGn_Unlock().

__IOM uint32_t WDOG_TypeDef::LOCK_CLR

Lock Register

Definition at line 77 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::LOCK_SET

Lock Register

Definition at line 66 of file efr32bg21_wdog.h.

__IOM uint32_t WDOG_TypeDef::LOCK_TGL

Lock Register

Definition at line 88 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 51 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED1[1014U]

Reserved for future use

Definition at line 57 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED2[1U]

Reserved for future use

Definition at line 62 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED3[1014U]

Reserved for future use

Definition at line 68 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 73 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED5[1014U]

Reserved for future use

Definition at line 79 of file efr32bg21_wdog.h.

uint32_t WDOG_TypeDef::RESERVED6[1U]

Reserved for future use

Definition at line 84 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::STATUS

Status Register

Definition at line 52 of file efr32bg21_wdog.h.

Referenced by WDOGn_Enable(), and WDOGn_IsLocked().

__IM uint32_t WDOG_TypeDef::STATUS_CLR

Status Register

Definition at line 74 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::STATUS_SET

Status Register

Definition at line 63 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::STATUS_TGL

Status Register

Definition at line 85 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 56 of file efr32bg21_wdog.h.

Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), WDOGn_Lock(), and WDOGn_SyncWait().

__IM uint32_t WDOG_TypeDef::SYNCBUSY_CLR

Synchronization Busy Register

Definition at line 78 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::SYNCBUSY_SET

Synchronization Busy Register

Definition at line 67 of file efr32bg21_wdog.h.

__IM uint32_t WDOG_TypeDef::SYNCBUSY_TGL

Synchronization Busy Register

Definition at line 89 of file efr32bg21_wdog.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_wdog.h