LETIMER_TypeDef Struct ReferenceDevices > LETIMER

LETIMER Register Declaration

Definition at line 48 of file efr32fg14p_letimer.h.

#include <efr32fg14p_letimer.h>

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CNT
 
__IOM uint32_t COMP0
 
__IOM uint32_t COMP1
 
__IOM uint32_t CTRL
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t PRSSEL
 
__IOM uint32_t REP0
 
__IOM uint32_t REP1
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [2U]
 
uint32_t RESERVED2 [2U]
 
__IOM uint32_t ROUTELOC0
 
__IOM uint32_t ROUTEPEN
 
__IM uint32_t STATUS
 
__IM uint32_t SYNCBUSY
 

Field Documentation

__IOM uint32_t LETIMER_TypeDef::CMD

Command Register

Definition at line 50 of file efr32fg14p_letimer.h.

Referenced by LETIMER_Enable(), LETIMER_Init(), and LETIMER_Reset().

__IOM uint32_t LETIMER_TypeDef::CNT

Counter Value Register

Definition at line 52 of file efr32fg14p_letimer.h.

Referenced by LETIMER_CounterGet(), and LETIMER_CounterSet().

__IOM uint32_t LETIMER_TypeDef::COMP0

Compare Value Register 0

Definition at line 53 of file efr32fg14p_letimer.h.

Referenced by LETIMER_CompareGet(), LETIMER_CompareSet(), LETIMER_Init(), LETIMER_Reset(), and LETIMER_TopGet().

__IOM uint32_t LETIMER_TypeDef::COMP1

Compare Value Register 1

Definition at line 54 of file efr32fg14p_letimer.h.

Referenced by LETIMER_CompareGet(), LETIMER_CompareSet(), and LETIMER_Reset().

__IOM uint32_t LETIMER_TypeDef::CTRL

Control Register

Definition at line 49 of file efr32fg14p_letimer.h.

Referenced by LETIMER_Init(), LETIMER_Reset(), and LETIMER_TopSet().

__IOM uint32_t LETIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 60 of file efr32fg14p_letimer.h.

Referenced by LETIMER_IntDisable(), LETIMER_IntEnable(), LETIMER_IntGetEnabled(), and LETIMER_Reset().

__IM uint32_t LETIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 57 of file efr32fg14p_letimer.h.

Referenced by LETIMER_IntGet(), and LETIMER_IntGetEnabled().

__IOM uint32_t LETIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 59 of file efr32fg14p_letimer.h.

Referenced by LETIMER_IntClear().

__IOM uint32_t LETIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 58 of file efr32fg14p_letimer.h.

Referenced by LETIMER_IntSet().

__IOM uint32_t LETIMER_TypeDef::PRSSEL

PRS Input Select Register

Definition at line 70 of file efr32fg14p_letimer.h.

__IOM uint32_t LETIMER_TypeDef::REP0

Repeat Counter Register 0

Definition at line 55 of file efr32fg14p_letimer.h.

Referenced by LETIMER_RepeatGet(), LETIMER_RepeatSet(), and LETIMER_Reset().

__IOM uint32_t LETIMER_TypeDef::REP1

Repeat Counter Register 1

Definition at line 56 of file efr32fg14p_letimer.h.

Referenced by LETIMER_RepeatGet(), LETIMER_RepeatSet(), and LETIMER_Reset().

uint32_t LETIMER_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 62 of file efr32fg14p_letimer.h.

uint32_t LETIMER_TypeDef::RESERVED1[2U]

Reserved for future use

Definition at line 65 of file efr32fg14p_letimer.h.

uint32_t LETIMER_TypeDef::RESERVED2[2U]

Reserved for future use

Definition at line 69 of file efr32fg14p_letimer.h.

__IOM uint32_t LETIMER_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 67 of file efr32fg14p_letimer.h.

__IOM uint32_t LETIMER_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 66 of file efr32fg14p_letimer.h.

__IM uint32_t LETIMER_TypeDef::STATUS

Status Register

Definition at line 51 of file efr32fg14p_letimer.h.

Referenced by LETIMER_Init().

__IM uint32_t LETIMER_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 63 of file efr32fg14p_letimer.h.

Referenced by LETIMER_SyncWait().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG14P/Include/efr32fg14p_letimer.h