Description Version API. Macros specifying the EMLIB and CMSIS version. ... #define _EMLIB_VERSION_PATCH 0 #define _CMSIS_VERSION 5.3.0 Version number of targeted CMSIS package.
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... The storage location can either be application memory or inside the SE, for more details, see sl_se_storage_method_t. Depending on the use-case, the ...
You should avoid using it in production. ... sl_iostream_rtt_handle sl_iostream_instance_info_t sl_iostream_instance_rtt_info ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollersResource TypeSoftware API documentation
Configuration Options The API Flow Control Support Example ... // Set to 1 to enable hardware flow control. ... uartdrvAbortTransmit = 1, uartdrvAbortReceive = 2, uartdrvAbortAll = 3
ProductMicrocontrollersResource TypeSoftware API documentation
Training ... Github ... // Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... http://man7.org/linux/man-pages/man3/strftime.3.html
Results 1-6 of 6 for mcu/5.8/structLESENSE-TimeCtrlDesc-TypeDef