Capsense initialization structure.
       Definition at line
       
        605
       
       of file
       
        em_acmp.h
       
       .
      
      
       #include <
       
     
        em_acmp.h
       
       >
      
| Data Fields | |
| uint32_t | biasProg | 
| bool | enable | 
| bool | fullBias | 
| bool | halfBias | 
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel | 
| bool | lowPowerReferenceEnabled | 
| ACMP_CapsenseResistor_TypeDef | resistor | 
| uint32_t | vddLevel | 
| ACMP_WarmTime_TypeDef | warmTime | 
Field Documentation
| uint32_t ACMP_CapsenseInit_TypeDef::biasProg | 
Bias current. See the ACMP chapter about bias and response time in the reference manual for details.
        Definition at line
        
         620
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| bool ACMP_CapsenseInit_TypeDef::enable | 
If true, ACMP is enabled after configuration.
        Definition at line
        
         679
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| bool ACMP_CapsenseInit_TypeDef::fullBias | 
Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
        Definition at line
        
         609
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() , and CAPLESENSE_setupACMP() .
| bool ACMP_CapsenseInit_TypeDef::halfBias | 
Half-bias current. See the ACMP chapter about bias and response time in the reference manual for details.
        Definition at line
        
         615
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel | 
| bool ACMP_CapsenseInit_TypeDef::lowPowerReferenceEnabled | 
Low-power reference enabled. This setting, if enabled, reduces the power used by VDD and bandgap references.
        Definition at line
        
         647
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor | 
A resistor used in the capacative sensing circuit. For values see the device data sheet.
        Definition at line
        
         642
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| uint32_t ACMP_CapsenseInit_TypeDef::vddLevel | 
VDD reference value. VDD_SCALED = (VDD * VDDLEVEL) / 63. Valid values are in the 0-63 range.
        Definition at line
        
         657
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
| ACMP_WarmTime_TypeDef ACMP_CapsenseInit_TypeDef::warmTime | 
Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.
        Definition at line
        
         625
        
        of file
        
         em_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_acmp.h