// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... sl_bt_cmd_system_set_identity_address_id 0x13010020 ... Bluetooth identity address in little endian format
// Bluetooth LE//Version 6.0.0 //Bluetooth API Reference Guide //System ... sl_bt_cmd_system_set_identity_address_id 0x13010020 ... Bluetooth identity address in little endian format
enum | sl_bt_gatt_server_client_configuration_t { sl_bt_gatt_server_disable = 0x0, sl_bt_gatt_server_notification = 0x1, sl_bt_ ... Set the maximum size of ATT Message Transfer Units (MTU).
sl_bt_cmd_connection_read_remote_used_features_id 0x0d060020 ... Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.
// Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... sl_bt_cmd_advertiser_clear_random_address_id 0x11040020 ... Time range: 10 ms to 655.35 s Default : 0 uint8_t