UART uart_update UDP ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... [Disassociated] SILABS-WGM160P-4.0.0, Gecko_OS-STANDARD-4.0.12-1198, WGM160P
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... bus.mode uart.baud uart.data uart.flow uart.parity uart.stop Factory Reset Command
ProductWirelessResource TypeSoftware API documentation
uartu --- restart UART with new baud rate and flow control settings ... os pins can only use the strong drive strength. ... Use the dfu parameter to reboot in the UART-DFU bootloader mode.
ProductWirelessResource TypeSoftware API documentation