Description Version API. Macros specifying the EMLIB and CMSIS version. ... #define _EMLIB_VERSION_PATCH 0 #define _CMSIS_VERSION 5.3.0 Version number of targeted CMSIS package.
ProductMicrocontrollersResource TypeSoftware API documentation
A receiver should set RTS high when it is no longer capable of receiving data. ... UART software flow control uses in-band signaling, meaning the receiver sends special flow control characters ...
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... A pointer to this function is passed to sl_sleeptimer_start_timer().
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered ... Functions sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-6 of 6 for mcu/5.9/group-platform-common