// Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... example the device will erase OTP and become inoperable if 4 glitch signals is seen in a 1 minute time period.
Home ... // Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... All API functions can be called from within interrupt handlers. ... Expected value: 1-31. uint8_t N/A
... to the UARTDRV_InitLeuart() function for LEUART peripherals. The API This section contains brief descriptions of the functions in the API. ... LEUART driver instance initialization structure.
ProductMicrocontrollersResource TypeSoftware API documentation
Description Version API. Macros specifying the EMLIB and CMSIS version. ... Version number of targeted CMSIS package. ... A new version system for EMLIB will be provided in a later release.
ProductMicrocontrollersResource TypeSoftware API documentation