Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.cmd.buffered system.cmd.echo system.cmd.header_enabled system.cmd.prompt_enabled
ProductWirelessResource TypeSoftware API documentation
Modules Types Command data types. Functions gos_result_t gos_cmd_issue (const char *fmt,.) Issue Gecko OS Command. More. ... Issue Gecko OS command, store string result in buffer. ... Note
ProductWirelessResource TypeSoftware API documentation
1 - an update is available, the contains the new bundle version string ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... ipd 1 Input, high-impedance
BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... > gge 5 1 gges
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for mcu/5.9/structQSPI-StigCmd-TypeDef