ADC_TypeDef Struct ReferenceDevices > EFM32G_ADC

Definition at line 48 of file efm32g_adc.h.

Data Fields

__IOM uint32_t BIASPROG
 
__IOM uint32_t CAL
 
__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t SCANCTRL
 
__IM uint32_t SCANDATA
 
__IM uint32_t SCANDATAP
 
__IOM uint32_t SINGLECTRL
 
__IM uint32_t SINGLEDATA
 
__IM uint32_t SINGLEDATAP
 
__IM uint32_t STATUS
 

Field Documentation

__IOM uint32_t ADC_TypeDef::BIASPROG

Bias Programming Register

Definition at line 64 of file efm32g_adc.h.

Referenced by ADC_InitSingle(), and ADC_Reset().

__IOM uint32_t ADC_TypeDef::CAL

Calibration Register

Definition at line 62 of file efm32g_adc.h.

__IOM uint32_t ADC_TypeDef::CMD

Command Register

Definition at line 50 of file efm32g_adc.h.

Referenced by ADC_Init(), ADC_InitScan(), ADC_InitSingle(), ADC_Reset(), and ADC_Start().

__IOM uint32_t ADC_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32g_adc.h.

Referenced by ADC_Init(), ADC_InitScan(), ADC_InitSingle(), and ADC_Reset().

__IOM uint32_t ADC_TypeDef::IEN

Interrupt Enable Register

Definition at line 54 of file efm32g_adc.h.

Referenced by ADC_IntDisable(), ADC_IntEnable(), ADC_IntGetEnabled(), and ADC_Reset().

__IM uint32_t ADC_TypeDef::IF

Interrupt Flag Register

Definition at line 55 of file efm32g_adc.h.

Referenced by ADC_IntGet(), and ADC_IntGetEnabled().

__IOM uint32_t ADC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 57 of file efm32g_adc.h.

Referenced by ADC_IntClear(), and ADC_Reset().

__IOM uint32_t ADC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 56 of file efm32g_adc.h.

Referenced by ADC_IntSet().

uint32_t ADC_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 63 of file efm32g_adc.h.

__IOM uint32_t ADC_TypeDef::SCANCTRL

Scan Control Register

Definition at line 53 of file efm32g_adc.h.

Referenced by ADC_InitScan(), and ADC_Reset().

__IM uint32_t ADC_TypeDef::SCANDATA

Scan Conversion Result Data

Definition at line 59 of file efm32g_adc.h.

Referenced by ADC_DataScanGet().

__IM uint32_t ADC_TypeDef::SCANDATAP

Scan Sequence Result Data Peek Register

Definition at line 61 of file efm32g_adc.h.

Referenced by ADC_DataScanPeek().

__IOM uint32_t ADC_TypeDef::SINGLECTRL

Single Sample Control Register

Definition at line 52 of file efm32g_adc.h.

Referenced by ADC_InitSingle(), and ADC_Reset().

__IM uint32_t ADC_TypeDef::SINGLEDATA

Single Conversion Result Data

Definition at line 58 of file efm32g_adc.h.

Referenced by ADC_DataSingleGet().

__IM uint32_t ADC_TypeDef::SINGLEDATAP

Single Conversion Result Data Peek Register

Definition at line 60 of file efm32g_adc.h.

Referenced by ADC_DataSinglePeek().

__IM uint32_t ADC_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32g_adc.h.

Referenced by ADC_InitScan(), and ADC_InitSingle().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32G/Include/efm32g_adc.h