RTCC_CC_TypeDef Struct ReferenceDevicesDevices > | RTCC

RTCC_CC RTCC CC Register

.

Definition at line 46 of file efm32gg11b_rtcc_cc.h.

#include <efm32gg11b_rtcc_cc.h>

Data Fields

__IOM uint32_t CCV
 
__IOM uint32_t CTRL
 
__IOM uint32_t DATE
 
__IOM uint32_t TIME
 

Field Documentation

__IOM uint32_t RTCC_CC_TypeDef::CCV

Capture/Compare Value Register

Definition at line 48 of file efm32gg11b_rtcc_cc.h.

__IOM uint32_t RTCC_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 47 of file efm32gg11b_rtcc_cc.h.

__IOM uint32_t RTCC_CC_TypeDef::DATE

Capture/Compare Date Register

Definition at line 50 of file efm32gg11b_rtcc_cc.h.

__IOM uint32_t RTCC_CC_TypeDef::TIME

Capture/Compare Time Register

Definition at line 49 of file efm32gg11b_rtcc_cc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/efm32gg11b_rtcc_cc.h