PRS_TypeDef Struct ReferenceDevices > EFM32HG_PRS

Definition at line 48 of file efm32hg_prs.h.

Data Fields

PRS_CH_TypeDef CH [6U]
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [6U]
 
__IOM uint32_t ROUTE
 
__IOM uint32_t SWLEVEL
 
__IOM uint32_t SWPULSE
 
__IOM uint32_t TRACECTRL
 

Field Documentation

PRS_CH_TypeDef PRS_TypeDef::CH[6U]

Channel registers

Definition at line 54 of file efm32hg_prs.h.

uint32_t PRS_TypeDef::RESERVED0[1U]

Reserved registers

Definition at line 53 of file efm32hg_prs.h.

uint32_t PRS_TypeDef::RESERVED1[6U]

Reserved for future use

Definition at line 56 of file efm32hg_prs.h.

__IOM uint32_t PRS_TypeDef::ROUTE

I/O Routing Register

Definition at line 51 of file efm32hg_prs.h.

__IOM uint32_t PRS_TypeDef::SWLEVEL

Software Level Register

Definition at line 50 of file efm32hg_prs.h.

__IOM uint32_t PRS_TypeDef::SWPULSE

Software Pulse Register

Definition at line 49 of file efm32hg_prs.h.

__IOM uint32_t PRS_TypeDef::TRACECTRL

MTB Trace Control Register

Definition at line 57 of file efm32hg_prs.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/efm32hg_prs.h