WDOG_TypeDef Struct ReferenceDevices > WDOG

WDOG Register Declaration

Definition at line 49 of file efm32pg1b_wdog.h.

#include <efm32pg1b_wdog.h>

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
WDOG_PCH_TypeDef PCH [2U]
 
uint32_t RESERVED0 [2U]
 
__IM uint32_t SYNCBUSY
 

Field Documentation

__IOM uint32_t WDOG_TypeDef::CMD

Command Register

Definition at line 51 of file efm32pg1b_wdog.h.

Referenced by WDOGn_Feed().

__IOM uint32_t WDOG_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32pg1b_wdog.h.

Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), WDOGn_IsEnabled(), WDOGn_IsLocked(), and WDOGn_Lock().

__IOM uint32_t WDOG_TypeDef::IEN

Interrupt Enable Register

Definition at line 61 of file efm32pg1b_wdog.h.

Referenced by WDOGn_IntDisable(), WDOGn_IntEnable(), and WDOGn_IntGetEnabled().

__IM uint32_t WDOG_TypeDef::IF

Watchdog Interrupt Flags

Definition at line 58 of file efm32pg1b_wdog.h.

Referenced by WDOGn_IntGet(), and WDOGn_IntGetEnabled().

__IOM uint32_t WDOG_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 60 of file efm32pg1b_wdog.h.

Referenced by WDOGn_IntClear().

__IOM uint32_t WDOG_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 59 of file efm32pg1b_wdog.h.

Referenced by WDOGn_IntSet().

WDOG_PCH_TypeDef WDOG_TypeDef::PCH[2U]

PCH

Definition at line 55 of file efm32pg1b_wdog.h.

uint32_t WDOG_TypeDef::RESERVED0[2U]

Reserved for future use

Definition at line 57 of file efm32pg1b_wdog.h.

__IM uint32_t WDOG_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 53 of file efm32pg1b_wdog.h.

Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), and WDOGn_Lock().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32PG1B/Include/efm32pg1b_wdog.h