Deprecated List

globalScope> Global _SILICON_LABS_32B_PLATFORM_2_GEN
Platform 2, generation 1
globalScope> Global _SILICON_LABS_32B_PLATFORM_2_GEN_1
Platform 2, generation 1
globalScope> Global AES_CBC128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
This function preserves backwards compatibility. Use CRYPTO_AES_CBC128 instead.
globalScope> Global AES_CBC256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
This function preserves backwards compatibility. Use CRYPTO_AES_CBC256 instead.
globalScope> Global AES_CFB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
This function preserves backwards compatibility. Use CRYPTO_AES_CFB128 instead.
globalScope> Global AES_CFB256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt)
This function preserves backwards compatibility. Use CRYPTO_AES_CFB256 instead.
globalScope> Global AES_CTR128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, uint8_t *ctr, CRYPTO_AES_CtrFuncPtr_TypeDef ctrFunc)
This function preserves backwards compatibility. Use CRYPTO_AES_CTR128 instead.
globalScope> Global AES_CTR256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, uint8_t *ctr, CRYPTO_AES_CtrFuncPtr_TypeDef ctrFunc)
This function preserves backwards compatibility. Use CRYPTO_AES_CTR256 instead.
globalScope> Global AES_CTRUpdate32Bit (uint8_t *ctr)
This function preserves backwards compatibility. Use CRYPTO_AES_CTRUpdate32Bit instead.
globalScope> Global AES_DecryptKey128 (uint8_t *out, const uint8_t *in)
This function preserves backwards compatibility. Use CRYPTO_AES_DecryptKey128 instead.
globalScope> Global AES_DecryptKey256 (uint8_t *out, const uint8_t *in)
This function preserves backwards compatibility. Use CRYPTO_AES_DecryptKey256 instead.
globalScope> Global AES_ECB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, bool encrypt)
This function preserves backwards compatibility. Use CRYPTO_AES_ECB128 instead.
globalScope> Global AES_ECB256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, bool encrypt)
This function preserves backwards compatibility. Use CRYPTO_AES_ECB256 instead.
globalScope> Global AES_OFB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv)
This function preserves backwards compatibility. Use CRYPTO_AES_OFB128 instead.
globalScope> Global AES_OFB256 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv)
This function preserves backwards compatibility. Use CRYPTO_AES_OFB256 instead.
globalScope> Global CMU_AUXHFRCOFreqGet (void)
A deprecated function. New code should use CMU_AUXHFRCOBandGet().
globalScope> Global CMU_AUXHFRCOFreqSet (CMU_AUXHFRCOFreq_TypeDef setFreq)
A deprecated function. New code should use CMU_AUXHFRCOBandSet().
globalScope> Global CMU_HFRCOFreqGet (void)
A deprecated function. New code should use CMU_HFRCOBandGet().
globalScope> Global CMU_HFRCOFreqSet (CMU_HFRCOFreq_TypeDef setFreq)
A deprecated function. New code should use CMU_HFRCOBandSet().
globalScope> Global CMU_Log2ToDiv (uint32_t log2)
Deprecated and marked for removal in a later release. It will be replaced by SL_Log2ToDiv.
Parameters
[in]log2Logarithm of 2, as used by fixed prescalers.
globalScope> Global EMU_MemPwrDown (uint32_t blocks)
This function is deprecated, use EMU_RamPowerDown() instead which maps a user provided memory range into RAM blocks to power down.
globalScope> Global EMU_UpdateOscConfig (void)
Oscillator status is saved in EMU_EnterEM2() and EMU_EnterEM3().
globalScope> Global GPIO_IntConfig (GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable)
Deprecated function. New code should use GPIO_ExtIntConfig().
Module INT
These functions are deprecated and marked for removal in a later release. Use the CORE module instead. See Porting from em_int for information on how to convert existing code bases to use CORE.
globalScope> Global INT_Disable (void)
Deprecated and marked for removal in a later release. Use new CORE module instead.
globalScope> Global INT_Enable (void)
Deprecated and marked for removal in a later release. Use the new CORE module instead.
Module MPU
These functions are deprecated and marked for removal in a later release. Use ARM's ARM_MPU_xxx API instead. See file platform/CMSIS/Include/mpu_armv7.h or mpu_armv8.h
globalScope> Global MPU_ConfigureRegion (const MPU_RegionInit_TypeDef *init)
Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_SetRegion(), ARM_MPU_SetRegionEx(), ARM_MPU_Load() or similar instead.
globalScope> Global MPU_Disable (void)

Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_Disable() instead.

globalScope> Global MPU_Enable (uint32_t flags)

Deprecated and marked for removal in a later release. Use ARM's ARM_MPU_Enable() instead.

Module NVM
This driver is deprecated and marked for removal in a later release. New code should use NVM3.
globalScope> Global setupSWOForPrint
Use RETARGET_SwoInit instead
globalScope> Global SLEEP_Init (SLEEP_CbFuncPtr_t pSleepCb, SLEEP_CbFuncPtr_t pWakeUpCb)
New code should use the SLEEP_InitEx function for initializing the sleep module.
globalScope> Global UARTDRV_Init (UARTDRV_Handle_t handle, UARTDRV_InitUart_t *initData)
Deprecated; Use UARTDRV_InitUart() instead.
globalScope> Global USART_InitIrDA (const USART_InitIrDA_TypeDef *init)
Deprecated function. New code should use USARTn_InitIrDA(). This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
globalScope> Global WDOG_Enable (bool enable)
Deprecated function. New code should use WDOGn_Enable(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_Feed (void)
Deprecated function. New code should use WDOGn_Feed(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_Init (const WDOG_Init_TypeDef *init)
Deprecated function. New code should use WDOGn_Init(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_IsEnabled (void)
Deprecated function. New code should use WDOGn_IsEnabled(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_IsLocked (void)
Deprecated function. New code should use WDOGn_IsLocked(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_Lock (void)
Deprecated function. New code should use WDOGn_Lock(). This function uses DEFAULT_WDOG.