CMUEMLIB

Detailed Description

Clock management unit (CMU) Peripheral API.

This module contains functions for the CMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The CMU module controls oscillators, clocks gates, clock multiplexers, pre-scalers, calibration modules and wait-states.

Data Structures

struct  CMU_DPLLInit_TypeDef
 
struct  CMU_HFXOInit_TypeDef
 
struct  CMU_LFXOInit_TypeDef
 

Macros

#define CMU_AUXHFRCO_MAX   cmuAUXHFRCOFreq_48M0Hz
 
#define CMU_AUXHFRCO_MIN   cmuAUXHFRCOFreq_1M0Hz
 
#define CMU_DPLL_LFXO_TO_40MHZ
 
#define CMU_HFRCO_MAX   cmuHFRCOFreq_48M0Hz
 
#define CMU_HFRCO_MIN   cmuHFRCOFreq_1M0Hz
 
#define CMU_HFXOINIT_DEFAULT
 
#define CMU_HFXOINIT_EXTERNAL_CLOCK
 
#define CMU_LFXOINIT_DEFAULT
 
#define CMU_LFXOINIT_EXTERNAL_CLOCK
 
#define cmuClkDiv_1   1
 
#define cmuClkDiv_1024   1024
 
#define cmuClkDiv_128   128
 
#define cmuClkDiv_16   16
 
#define cmuClkDiv_16384   16384
 
#define cmuClkDiv_2   2
 
#define cmuClkDiv_2048   2048
 
#define cmuClkDiv_256   256
 
#define cmuClkDiv_32   32
 
#define cmuClkDiv_32768   32768
 
#define cmuClkDiv_4   4
 
#define cmuClkDiv_4096   4096
 
#define cmuClkDiv_512   512
 
#define cmuClkDiv_64   64
 
#define cmuClkDiv_8   8
 
#define cmuClkDiv_8192   8192
 

Typedefs

typedef uint32_t CMU_ClkDiv_TypeDef
 
typedef uint32_t CMU_ClkPresc_TypeDef
 

Enumerations

enum  CMU_AUXHFRCOFreq_TypeDef {
  cmuAUXHFRCOFreq_1M0Hz = 1000000U,
  cmuAUXHFRCOFreq_2M0Hz = 2000000U,
  cmuAUXHFRCOFreq_4M0Hz = 4000000U,
  cmuAUXHFRCOFreq_7M0Hz = 7000000U,
  cmuAUXHFRCOFreq_13M0Hz = 13000000U,
  cmuAUXHFRCOFreq_16M0Hz = 16000000U,
  cmuAUXHFRCOFreq_19M0Hz = 19000000U,
  cmuAUXHFRCOFreq_26M0Hz = 26000000U,
  cmuAUXHFRCOFreq_32M0Hz = 32000000U,
  cmuAUXHFRCOFreq_38M0Hz = 38000000U,
  cmuAUXHFRCOFreq_48M0Hz = 48000000U,
  cmuAUXHFRCOFreq_UserDefined = 0
}
 
enum  CMU_Clock_TypeDef {
  cmuClock_HF,
  cmuClock_DBG,
  cmuClock_AUX,
  cmuClock_EXPORT,
  cmuClock_BUS,
  cmuClock_CRYPTO0,
  cmuClock_LDMA,
  cmuClock_GPCRC,
  cmuClock_GPIO,
  cmuClock_HFLE,
  cmuClock_PRS,
  cmuClock_HFPER,
  cmuClock_HFPERB,
  cmuClock_HFPERC,
  cmuClock_USART0,
  cmuClock_USART1,
  cmuClock_USART2,
  cmuClock_USART3,
  cmuClock_UART0,
  cmuClock_TIMER0,
  cmuClock_TIMER1,
  cmuClock_WTIMER0,
  cmuClock_WTIMER1,
  cmuClock_CRYOTIMER,
  cmuClock_ACMP0,
  cmuClock_ACMP1,
  cmuClock_VDAC0,
  cmuClock_ADC0,
  cmuClock_I2C0,
  cmuClock_I2C1,
  cmuClock_CSEN_HF,
  cmuClock_TRNG0,
  cmuClock_CAN0,
  cmuClock_CORE,
  cmuClock_LFA,
  cmuClock_LETIMER0,
  cmuClock_LCDpre,
  cmuClock_LCD,
  cmuClock_PCNT0,
  cmuClock_LESENSE,
  cmuClock_LFB,
  cmuClock_LEUART0,
  cmuClock_CSEN_LF,
  cmuClock_SYSTICK,
  cmuClock_LFE,
  cmuClock_RTCC,
  cmuClock_ADC0ASYNC
}
 
enum  CMU_DPLLClkSel_TypeDef {
  cmuDPLLClkSel_Hfxo = _CMU_DPLLCTRL_REFSEL_HFXO,
  cmuDPLLClkSel_Lfxo = _CMU_DPLLCTRL_REFSEL_LFXO,
  cmuDPLLClkSel_Clkin0 = _CMU_DPLLCTRL_REFSEL_CLKIN0
}
 
enum  CMU_DPLLEdgeSel_TypeDef {
  cmuDPLLEdgeSel_Fall = _CMU_DPLLCTRL_EDGESEL_FALL,
  cmuDPLLEdgeSel_Rise = _CMU_DPLLCTRL_EDGESEL_RISE
}
 
enum  CMU_DPLLLockMode_TypeDef {
  cmuDPLLLockMode_Freq = _CMU_DPLLCTRL_MODE_FREQLL,
  cmuDPLLLockMode_Phase = _CMU_DPLLCTRL_MODE_PHASELL
}
 
enum  CMU_HFRCOFreq_TypeDef {
  cmuHFRCOFreq_1M0Hz = 1000000U,
  cmuHFRCOFreq_2M0Hz = 2000000U,
  cmuHFRCOFreq_4M0Hz = 4000000U,
  cmuHFRCOFreq_7M0Hz = 7000000U,
  cmuHFRCOFreq_13M0Hz = 13000000U,
  cmuHFRCOFreq_16M0Hz = 16000000U,
  cmuHFRCOFreq_19M0Hz = 19000000U,
  cmuHFRCOFreq_26M0Hz = 26000000U,
  cmuHFRCOFreq_32M0Hz = 32000000U,
  cmuHFRCOFreq_38M0Hz = 38000000U,
  cmuHFRCOFreq_48M0Hz = 48000000U,
  cmuHFRCOFreq_UserDefined = 0
}
 
enum  CMU_HFXOTuningMode_TypeDef {
  cmuHFXOTuningMode_Auto = 0,
  cmuHFXOTuningMode_PeakDetectCommand = CMU_CMD_HFXOPEAKDETSTART
}
 
enum  CMU_Osc_TypeDef {
  cmuOsc_LFXO,
  cmuOsc_LFRCO,
  cmuOsc_HFXO,
  cmuOsc_HFRCO,
  cmuOsc_AUXHFRCO,
  cmuOsc_ULFRCO,
  cmuOsc_CLKIN0
}
 
enum  CMU_OscMode_TypeDef {
  cmuOscMode_Crystal,
  cmuOscMode_AcCoupled,
  cmuOscMode_External
}
 
enum  CMU_Select_TypeDef {
  cmuSelect_Error,
  cmuSelect_Disabled,
  cmuSelect_LFXO,
  cmuSelect_LFRCO,
  cmuSelect_HFXO,
  cmuSelect_HFRCO,
  cmuSelect_HFCLKLE,
  cmuSelect_AUXHFRCO,
  cmuSelect_HFSRCCLK,
  cmuSelect_HFCLK,
  cmuSelect_ULFRCO,
  cmuSelect_HFRCODIV2,
  cmuSelect_CLKIN0
}
 

Functions

CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOBandGet (void)
 Get the current AUXHFRCO frequency.
 
void CMU_AUXHFRCOBandSet (CMU_AUXHFRCOFreq_TypeDef setFreq)
 Set AUXHFRCO calibration for the selected target frequency.
 
static uint32_t CMU_AUXHFRCODevinfoGet (CMU_AUXHFRCOFreq_TypeDef freq)
 Get the AUXHFRCO frequency calibration word in DEVINFO.
 
__STATIC_INLINE CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOFreqGet (void)
 Get the current AUXHFRCO frequency.
 
__STATIC_INLINE void CMU_AUXHFRCOFreqSet (CMU_AUXHFRCOFreq_TypeDef setFreq)
 Set AUXHFRCO calibration for the selected target frequency.
 
uint32_t CMU_Calibrate (uint32_t HFCycles, CMU_Osc_TypeDef reference)
 Calibrate the clock.
 
void CMU_CalibrateConfig (uint32_t downCycles, CMU_Osc_TypeDef downSel, CMU_Osc_TypeDef upSel)
 Configure the clock calibration.
 
__STATIC_INLINE void CMU_CalibrateCont (bool enable)
 Configure continuous calibration mode.
 
uint32_t CMU_CalibrateCountGet (void)
 Get the calibration count register.
 
__STATIC_INLINE void CMU_CalibrateStart (void)
 Start calibration.
 
__STATIC_INLINE void CMU_CalibrateStop (void)
 Stop the calibration counters.
 
CMU_ClkDiv_TypeDef CMU_ClockDivGet (CMU_Clock_TypeDef clock)
 Get the clock divisor/prescaler.
 
void CMU_ClockDivSet (CMU_Clock_TypeDef clock, CMU_ClkDiv_TypeDef div)
 Set the clock divisor/prescaler.
 
void CMU_ClockEnable (CMU_Clock_TypeDef clock, bool enable)
 Enable/disable a clock.
 
uint32_t CMU_ClockFreqGet (CMU_Clock_TypeDef clock)
 Get the clock frequency for a clock point.
 
uint32_t CMU_ClockPrescGet (CMU_Clock_TypeDef clock)
 Get the clock prescaler.
 
void CMU_ClockPrescSet (CMU_Clock_TypeDef clock, CMU_ClkPresc_TypeDef presc)
 Set the clock prescaler.
 
CMU_Select_TypeDef CMU_ClockSelectGet (CMU_Clock_TypeDef clock)
 Get the currently selected reference clock used for a clock branch.
 
void CMU_ClockSelectSet (CMU_Clock_TypeDef clock, CMU_Select_TypeDef ref)
 Select the reference clock/oscillator used for a clock branch.
 
__STATIC_INLINE uint32_t CMU_DivToLog2 (CMU_ClkDiv_TypeDef div)
 Convert dividend to logarithmic value. It only works for even numbers equal to 2^n.
 
bool CMU_DPLLLock (const CMU_DPLLInit_TypeDef *init)
 Lock the DPLL to a given frequency.
 
__STATIC_INLINE void CMU_DPLLUnlock (void)
 Unlock DPLL.
 
void CMU_FreezeEnable (bool enable)
 CMU low frequency register synchronization freeze control.
 
CMU_HFRCOFreq_TypeDef CMU_HFRCOBandGet (void)
 Get the current HFRCO frequency.
 
void CMU_HFRCOBandSet (CMU_HFRCOFreq_TypeDef setFreq)
 Set the HFRCO calibration for the selected target frequency.
 
static uint32_t CMU_HFRCODevinfoGet (CMU_HFRCOFreq_TypeDef freq)
 Get the HFRCO frequency calibration word in DEVINFO.
 
__STATIC_INLINE CMU_HFRCOFreq_TypeDef CMU_HFRCOFreqGet (void)
 Get the current HFRCO frequency.
 
__STATIC_INLINE void CMU_HFRCOFreqSet (CMU_HFRCOFreq_TypeDef setFreq)
 Set HFRCO calibration for the selected target frequency.
 
void CMU_HFXOAutostartEnable (uint32_t userSel, bool enEM0EM1Start, bool enEM0EM1StartSel)
 Enable or disable HFXO autostart.
 
void CMU_HFXOInit (const CMU_HFXOInit_TypeDef *hfxoInit)
 Set HFXO control registers.
 
__STATIC_INLINE void CMU_IntClear (uint32_t flags)
 Clear one or more pending CMU interrupts.
 
__STATIC_INLINE void CMU_IntDisable (uint32_t flags)
 Disable one or more CMU interrupts.
 
__STATIC_INLINE void CMU_IntEnable (uint32_t flags)
 Enable one or more CMU interrupts.
 
__STATIC_INLINE uint32_t CMU_IntGet (void)
 Get pending CMU interrupts.
 
__STATIC_INLINE uint32_t CMU_IntGetEnabled (void)
 Get enabled and pending CMU interrupt flags.
 
__STATIC_INLINE void CMU_IntSet (uint32_t flags)
 Set one or more pending CMU interrupts.
 
uint32_t CMU_LCDClkFDIVGet (void)
 Get the LCD framerate divisor (FDIV) setting.
 
void CMU_LCDClkFDIVSet (uint32_t div)
 Set the LCD framerate divisor (FDIV) setting.
 
void CMU_LFXOInit (const CMU_LFXOInit_TypeDef *lfxoInit)
 Set LFXO control registers.
 
__STATIC_INLINE void CMU_Lock (void)
 Lock the CMU to protect some of its registers against unintended modification.
 
__STATIC_INLINE uint32_t CMU_Log2ToDiv (uint32_t log2)
 Convert logarithm of 2 prescaler to division factor.
 
void CMU_OscillatorEnable (CMU_Osc_TypeDef osc, bool enable, bool wait)
 Enable/disable oscillator.
 
uint32_t CMU_OscillatorTuningGet (CMU_Osc_TypeDef osc)
 Get the oscillator frequency tuning setting.
 
bool CMU_OscillatorTuningOptimize (CMU_Osc_TypeDef osc, CMU_HFXOTuningMode_TypeDef mode, bool wait)
 Start and optionally wait for the oscillator tuning optimization.
 
void CMU_OscillatorTuningSet (CMU_Osc_TypeDef osc, uint32_t val)
 Set the oscillator frequency tuning control.
 
bool CMU_OscillatorTuningWait (CMU_Osc_TypeDef osc, CMU_HFXOTuningMode_TypeDef mode)
 Wait for the oscillator tuning optimization.
 
bool CMU_PCNTClockExternalGet (unsigned int instance)
 Determine if the currently selected PCNTn clock used is external or LFBCLK.
 
void CMU_PCNTClockExternalSet (unsigned int instance, bool external)
 Select the PCNTn clock.
 
__STATIC_INLINE uint32_t CMU_PrescToLog2 (uint32_t presc)
 Convert prescaler dividend to a logarithmic value. It only works for even numbers equal to 2^n.
 
__STATIC_INLINE void CMU_Unlock (void)
 Unlock the CMU so that writing to locked registers again is possible.
 
void CMU_UpdateWaitStates (uint32_t freq, int vscale)
 

Macro Definition Documentation

#define CMU_DPLL_LFXO_TO_40MHZ
Value:
{ \
39998805, /* Target frequency. */ \
3661, /* Factor N. */ \
2, /* Factor M. */ \
0, /* No spread spectrum clocking. */ \
0, /* No spread spectrum clocking. */ \
cmuDPLLClkSel_Lfxo, /* Select LFXO as reference clock. */ \
cmuDPLLEdgeSel_Fall, /* Select falling edge of ref clock. */ \
cmuDPLLLockMode_Freq, /* Use frequency lock mode. */ \
true /* Enable automatic lock recovery. */ \
}

DPLL initialization values for 39,998,805 Hz using LFXO as reference clock, M=2 and N=3661.

Definition at line 2552 of file em_cmu.h.

Referenced by BSP_initClocks().

#define CMU_HFXOINIT_DEFAULT
Value:
{ \
_CMU_HFXOSTARTUPCTRL_CTUNE_DEFAULT, \
_CMU_HFXOSTEADYSTATECTRL_CTUNE_DEFAULT, \
_CMU_HFXOSTARTUPCTRL_IBTRIMXOCORE_DEFAULT, \
_CMU_HFXOSTEADYSTATECTRL_IBTRIMXOCORE_DEFAULT, \
_CMU_HFXOTIMEOUTCTRL_PEAKDETTIMEOUT_DEFAULT, \
_CMU_HFXOTIMEOUTCTRL_STEADYTIMEOUT_DEFAULT, \
_CMU_HFXOTIMEOUTCTRL_STARTUPTIMEOUT_DEFAULT, \
cmuOscMode_Crystal, \
}

Definition at line 2430 of file em_cmu.h.

#define CMU_HFXOINIT_EXTERNAL_CLOCK
Value:
{ \
_CMU_HFXOSTARTUPCTRL_CTUNE_DEFAULT, \
_CMU_HFXOSTEADYSTATECTRL_CTUNE_DEFAULT, \
_CMU_HFXOSTARTUPCTRL_IBTRIMXOCORE_DEFAULT, \
_CMU_HFXOSTEADYSTATECTRL_IBTRIMXOCORE_DEFAULT, \
_CMU_HFXOTIMEOUTCTRL_PEAKDETTIMEOUT_DEFAULT, \
_CMU_HFXOTIMEOUTCTRL_STEADYTIMEOUT_DEFAULT, \
_CMU_HFXOTIMEOUTCTRL_STARTUPTIMEOUT_DEFAULT, \
cmuOscMode_External, \
}

Definition at line 2441 of file em_cmu.h.

#define CMU_LFXOINIT_DEFAULT
Value:
{ \
_CMU_LFXOCTRL_TUNING_DEFAULT, /* Default CTUNE value, 0 */ \
_CMU_LFXOCTRL_GAIN_DEFAULT, /* Default gain, 2 */ \
_CMU_LFXOCTRL_TIMEOUT_DEFAULT, /* Default start-up delay, 32 K cycles */ \
cmuOscMode_Crystal, /* Crystal oscillator */ \
}

Default LFXO initialization values for platform 2 devices, which contain a separate LFXOCTRL register.

Definition at line 2365 of file em_cmu.h.

#define CMU_LFXOINIT_EXTERNAL_CLOCK
Value:
{ \
0, /* No CTUNE value needed */ \
0, /* No LFXO startup gain */ \
_CMU_LFXOCTRL_TIMEOUT_2CYCLES, /* Minimal lfxo start-up delay, 2 cycles */ \
cmuOscMode_External, /* External digital clock */ \
}

Definition at line 2372 of file em_cmu.h.

#define cmuClkDiv_1   1

Clock divisors. These values are valid for prescalers. Divide clock by 1.

Definition at line 1086 of file em_cmu.h.

Referenced by CAPLESENSE_setupCMU(), CMU_ClockDivGet(), CMU_ClockDivSet(), and RETARGET_SerialInit().

#define cmuClkDiv_1024   1024

Divide clock by 1024.

Definition at line 1096 of file em_cmu.h.

#define cmuClkDiv_128   128

Divide clock by 128.

Definition at line 1093 of file em_cmu.h.

Referenced by CMU_ClockDivSet(), and CMU_LCDClkFDIVSet().

#define cmuClkDiv_16   16

Divide clock by 16.

Definition at line 1090 of file em_cmu.h.

Referenced by CMU_ClockDivGet(), CMU_ClockDivSet(), and CMU_ClockFreqGet().

#define cmuClkDiv_16384   16384

Divide clock by 16384.

Definition at line 1100 of file em_cmu.h.

#define cmuClkDiv_2   2

Divide clock by 2.

Definition at line 1087 of file em_cmu.h.

#define cmuClkDiv_2048   2048

Divide clock by 2048.

Definition at line 1097 of file em_cmu.h.

#define cmuClkDiv_256   256

Divide clock by 256.

Definition at line 1094 of file em_cmu.h.

Referenced by UDELAY_Calibrate().

#define cmuClkDiv_32   32

Divide clock by 32.

Definition at line 1091 of file em_cmu.h.

#define cmuClkDiv_32768   32768

Divide clock by 32768.

Definition at line 1101 of file em_cmu.h.

Referenced by CMU_ClockDivSet().

#define cmuClkDiv_4   4

Divide clock by 4.

Definition at line 1088 of file em_cmu.h.

#define cmuClkDiv_4096   4096

Divide clock by 4096.

Definition at line 1098 of file em_cmu.h.

#define cmuClkDiv_512   512

Divide clock by 512.

Definition at line 1095 of file em_cmu.h.

Referenced by CMU_ClockDivSet().

#define cmuClkDiv_64   64

Divide clock by 64.

Definition at line 1092 of file em_cmu.h.

#define cmuClkDiv_8   8

Divide clock by 8.

Definition at line 1089 of file em_cmu.h.

Referenced by CMU_ClockDivSet().

#define cmuClkDiv_8192   8192

Divide clock by 8192.

Definition at line 1099 of file em_cmu.h.

Typedef Documentation

typedef uint32_t CMU_ClkDiv_TypeDef

Clock divider configuration

Definition at line 1104 of file em_cmu.h.

typedef uint32_t CMU_ClkPresc_TypeDef

Clockprescaler configuration

Definition at line 1108 of file em_cmu.h.

Enumeration Type Documentation

AUX high-frequency RCO bands

Enumerator
cmuAUXHFRCOFreq_1M0Hz 

1 MHz RC band

cmuAUXHFRCOFreq_2M0Hz 

2 MHz RC band

cmuAUXHFRCOFreq_4M0Hz 

4 MHz RC band

cmuAUXHFRCOFreq_7M0Hz 

7 MHz RC band

cmuAUXHFRCOFreq_13M0Hz 

13 MHz RC band

cmuAUXHFRCOFreq_16M0Hz 

16 MHz RC band

cmuAUXHFRCOFreq_19M0Hz 

19 MHz RC band

cmuAUXHFRCOFreq_26M0Hz 

26 MHz RC band

cmuAUXHFRCOFreq_32M0Hz 

32 MHz RC band

cmuAUXHFRCOFreq_38M0Hz 

38 MHz RC band

cmuAUXHFRCOFreq_48M0Hz 

48 MHz RC band

Definition at line 1205 of file em_cmu.h.

Clock points in CMU. See CMU overview in the reference manual.

Enumerator
cmuClock_HF 

High-frequency clock

cmuClock_DBG 

Debug clock

cmuClock_AUX 

AUX clock

cmuClock_EXPORT 

Export clock

cmuClock_BUS 

High-frequency bus clock

cmuClock_CRYPTO0 

Cryptography accelerator 0 clock

cmuClock_LDMA 

Direct-memory access controller clock

cmuClock_GPCRC 

General-purpose cyclic redundancy checksum clock

cmuClock_GPIO 

General-purpose input/output clock

cmuClock_HFLE 

Low-energy clock divided down from HFBUSCLK

cmuClock_PRS 

Peripheral reflex system clock

cmuClock_HFPER 

High-frequency peripheral clock

cmuClock_HFPERB 

Branch B figh-frequency peripheral clock

cmuClock_HFPERC 

Branch C figh-frequency peripheral clock

cmuClock_USART0 

Universal sync/async receiver/transmitter 0 clock

cmuClock_USART1 

Universal sync/async receiver/transmitter 1 clock

cmuClock_USART2 

Universal sync/async receiver/transmitter 2 clock

cmuClock_USART3 

Universal sync/async receiver/transmitter 3 clock

cmuClock_UART0 

Universal async receiver/transmitter 0 clock

cmuClock_TIMER0 

Timer 0 clock

cmuClock_TIMER1 

Timer 1 clock

cmuClock_WTIMER0 

Wide-timer 0 clock

cmuClock_WTIMER1 

Wide-timer 1 clock

cmuClock_CRYOTIMER 

CRYOtimer clock

cmuClock_ACMP0 

Analog comparator 0 clock

cmuClock_ACMP1 

Analog comparator 1 clock

cmuClock_VDAC0 

Voltage digital-to-analog converter 0 clock

cmuClock_ADC0 

Analog-to-digital converter 0 clock

cmuClock_I2C0 

I2C 0 clock

cmuClock_I2C1 

I2C 1 clock

cmuClock_CSEN_HF 

Capacitive Sense HF clock

cmuClock_TRNG0 

True random number generator clock

cmuClock_CAN0 

Controller Area Network 0 clock

cmuClock_CORE 

Core clock

cmuClock_LFA 

Low-frequency A clock

cmuClock_LETIMER0 

Low-energy timer 0 clock

cmuClock_LCDpre 

Liquid crystal display, pre FDIV clock

cmuClock_LCD 

Liquid crystal display clock. Note that FDIV prescaler must be set by special API.

cmuClock_PCNT0 

Pulse counter 0 clock

cmuClock_LESENSE 

LESENSE clock

cmuClock_LFB 

Low-frequency B clock

cmuClock_LEUART0 

Low-energy universal asynchronous receiver/transmitter 0 clock

cmuClock_CSEN_LF 

Capacitive Sense LF clock

cmuClock_SYSTICK 

Cortex SYSTICK LF clock

cmuClock_LFE 

Low-frequency E clock

cmuClock_RTCC 

Real-time counter and calendar clock

cmuClock_ADC0ASYNC 

ADC0 asynchronous clock

Definition at line 1235 of file em_cmu.h.

DPLL reference clock selector.

Enumerator
cmuDPLLClkSel_Hfxo 

HFXO is DPLL reference clock.

cmuDPLLClkSel_Lfxo 

LFXO is DPLL reference clock.

cmuDPLLClkSel_Clkin0 

CLKIN0 is DPLL reference clock.

Definition at line 2326 of file em_cmu.h.

DPLL reference clock edge detect selector.

Enumerator
cmuDPLLEdgeSel_Fall 

Detect falling edge of reference clock.

cmuDPLLEdgeSel_Rise 

Detect rising edge of reference clock.

Definition at line 2333 of file em_cmu.h.

DPLL lock mode selector.

Enumerator
cmuDPLLLockMode_Freq 

Frequency lock mode.

cmuDPLLLockMode_Phase 

Phase lock mode.

Definition at line 2339 of file em_cmu.h.

High-frequency system RCO bands

Enumerator
cmuHFRCOFreq_1M0Hz 

1 MHz RC band

cmuHFRCOFreq_2M0Hz 

2 MHz RC band

cmuHFRCOFreq_4M0Hz 

4 MHz RC band

cmuHFRCOFreq_7M0Hz 

7 MHz RC band

cmuHFRCOFreq_13M0Hz 

13 MHz RC band

cmuHFRCOFreq_16M0Hz 

16 MHz RC band

cmuHFRCOFreq_19M0Hz 

19 MHz RC band

cmuHFRCOFreq_26M0Hz 

26 MHz RC band

cmuHFRCOFreq_32M0Hz 

32 MHz RC band

cmuHFRCOFreq_38M0Hz 

38 MHz RC band

cmuHFRCOFreq_48M0Hz 

48 MHz RC band

Definition at line 1164 of file em_cmu.h.

HFXO tuning modes

Enumerator
cmuHFXOTuningMode_PeakDetectCommand 

Run peak detect optimization only.

Definition at line 2301 of file em_cmu.h.

Oscillator types.

Enumerator
cmuOsc_LFXO 

Low-frequency crystal oscillator.

cmuOsc_LFRCO 

Low-frequency RC oscillator.

cmuOsc_HFXO 

High-frequency crystal oscillator.

cmuOsc_HFRCO 

High-frequency RC oscillator.

cmuOsc_AUXHFRCO 

Auxiliary high-frequency RC oscillator.

cmuOsc_ULFRCO 

Ultra low-frequency RC oscillator.

cmuOsc_CLKIN0 

External oscillator.

Definition at line 2229 of file em_cmu.h.

Oscillator modes.

Enumerator
cmuOscMode_Crystal 

Crystal oscillator.

cmuOscMode_AcCoupled 

AC-coupled buffer.

cmuOscMode_External 

External digital clock.

Definition at line 2250 of file em_cmu.h.

Selectable clock sources.

Enumerator
cmuSelect_Error 

Usage error.

cmuSelect_Disabled 

Clock selector disabled.

cmuSelect_LFXO 

Low-frequency crystal oscillator.

cmuSelect_LFRCO 

Low-frequency RC oscillator.

cmuSelect_HFXO 

High-frequency crystal oscillator.

cmuSelect_HFRCO 

High-frequency RC oscillator.

cmuSelect_HFCLKLE 

High-frequency LE clock divided by 2 or 4.

cmuSelect_AUXHFRCO 

Auxilliary clock source can be used for debug clock.

cmuSelect_HFSRCCLK 

High-frequency source clock.

cmuSelect_HFCLK 

Divided HFCLK on Giant for debug clock, undivided on Tiny Gecko and for USBC (not used on Gecko).

cmuSelect_ULFRCO 

Ultra low-frequency RC oscillator.

cmuSelect_HFRCODIV2 

High-frequency RC oscillator divided by 2.

cmuSelect_CLKIN0 

External clock input.

Definition at line 2257 of file em_cmu.h.

Function Documentation

CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOBandGet ( void  )

Get the current AUXHFRCO frequency.

Returns
AUXHFRCO frequency.

Definition at line 4275 of file em_cmu.c.

Referenced by CMU_AUXHFRCOFreqGet().

void CMU_AUXHFRCOBandSet ( CMU_AUXHFRCOFreq_TypeDef  setFreq)

Set AUXHFRCO calibration for the selected target frequency.

Parameters
[in]setFreqAUXHFRCO frequency to set

Definition at line 4289 of file em_cmu.c.

References _CMU_AUXHFRCOCTRL_CLKDIV_MASK, _CMU_SYNCBUSY_AUXHFRCOBSY_SHIFT, BUS_RegBitRead(), CMU, CMU_AUXHFRCOCTRL_CLKDIV_DIV1, CMU_AUXHFRCOCTRL_CLKDIV_DIV2, CMU_AUXHFRCOCTRL_CLKDIV_DIV4, CMU_AUXHFRCODevinfoGet(), cmuAUXHFRCOFreq_1M0Hz, cmuAUXHFRCOFreq_2M0Hz, and cmuAUXHFRCOFreq_4M0Hz.

Referenced by CMU_AUXHFRCOFreqSet().

static uint32_t CMU_AUXHFRCODevinfoGet ( CMU_AUXHFRCOFreq_TypeDef  freq)
static

Get the AUXHFRCO frequency calibration word in DEVINFO.

Parameters
[in]freqFrequency in Hz.
Returns
AUXHFRCO calibration word for a given frequency.

Definition at line 4222 of file em_cmu.c.

References cmuAUXHFRCOFreq_13M0Hz, cmuAUXHFRCOFreq_16M0Hz, cmuAUXHFRCOFreq_19M0Hz, cmuAUXHFRCOFreq_1M0Hz, cmuAUXHFRCOFreq_26M0Hz, cmuAUXHFRCOFreq_2M0Hz, cmuAUXHFRCOFreq_32M0Hz, cmuAUXHFRCOFreq_38M0Hz, cmuAUXHFRCOFreq_48M0Hz, cmuAUXHFRCOFreq_4M0Hz, cmuAUXHFRCOFreq_7M0Hz, and DEVINFO.

Referenced by CMU_AUXHFRCOBandSet().

__STATIC_INLINE CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOFreqGet ( void  )

Get the current AUXHFRCO frequency.

Deprecated:
A deprecated function. New code should use CMU_AUXHFRCOBandGet().
Returns
AUXHFRCO frequency.

Definition at line 2910 of file em_cmu.h.

References CMU_AUXHFRCOBandGet().

__STATIC_INLINE void CMU_AUXHFRCOFreqSet ( CMU_AUXHFRCOFreq_TypeDef  setFreq)

Set AUXHFRCO calibration for the selected target frequency.

Deprecated:
A deprecated function. New code should use CMU_AUXHFRCOBandSet().
Parameters
[in]setFreqAUXHFRCO frequency to set.

Definition at line 2925 of file em_cmu.h.

References CMU_AUXHFRCOBandSet().

uint32_t CMU_Calibrate ( uint32_t  HFCycles,
CMU_Osc_TypeDef  reference 
)

Calibrate the clock.

Run a calibration for HFCLK against a selectable reference clock. See the reference manual, CMU chapter, for more details.

Note
This function will not return until the calibration measurement is completed.
Parameters
[in]HFCyclesThe number of HFCLK cycles to run the calibration. Increasing this number increases precision but the calibration will take more time.
[in]refThe reference clock used to compare HFCLK.
Returns
The number of ticks the reference clock after HFCycles ticks on the HF clock.

Definition at line 4350 of file em_cmu.c.

References _CMU_CALCNT_CALCNT_MASK, _CMU_CALCNT_CALCNT_SHIFT, _CMU_STATUS_CALRDY_SHIFT, BUS_RegBitRead(), CMU, CMU_CALCTRL_UPSEL_AUXHFRCO, CMU_CALCTRL_UPSEL_HFRCO, CMU_CALCTRL_UPSEL_HFXO, CMU_CALCTRL_UPSEL_LFRCO, CMU_CALCTRL_UPSEL_LFXO, CMU_CMD_CALSTART, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.

void CMU_CalibrateConfig ( uint32_t  downCycles,
CMU_Osc_TypeDef  downSel,
CMU_Osc_TypeDef  upSel 
)

Configure the clock calibration.

Configure a calibration for a selectable clock source against another selectable reference clock. See the reference manual, CMU chapter, for more details.

Note
After configuration, a call to CMU_CalibrateStart() is required and the resulting calibration value can be read out with the CMU_CalibrateCountGet() function call.
Parameters
[in]downCyclesThe number of downSel clock cycles to run the calibration. Increasing this number increases precision but the calibration will take more time.
[in]downSelThe clock, which will be counted down downCycles.
[in]upSelThe reference clock; the number of cycles generated by this clock will be counted and added up and the result can be given with the CMU_CalibrateCountGet() function call.

Definition at line 4439 of file em_cmu.c.

References _CMU_CALCNT_CALCNT_MASK, _CMU_CALCNT_CALCNT_SHIFT, _CMU_CALCTRL_DOWNSEL_MASK, _CMU_CALCTRL_UPSEL_MASK, CMU, CMU_CALCTRL_DOWNSEL_AUXHFRCO, CMU_CALCTRL_DOWNSEL_HFRCO, CMU_CALCTRL_DOWNSEL_HFXO, CMU_CALCTRL_DOWNSEL_LFRCO, CMU_CALCTRL_DOWNSEL_LFXO, CMU_CALCTRL_UPSEL_AUXHFRCO, CMU_CALCTRL_UPSEL_HFRCO, CMU_CALCTRL_UPSEL_HFXO, CMU_CALCTRL_UPSEL_LFRCO, CMU_CALCTRL_UPSEL_LFXO, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.

__STATIC_INLINE void CMU_CalibrateCont ( bool  enable)

Configure continuous calibration mode.

Parameters
[in]enableIf true, enables continuous calibration, if false disables continuous calibration.

Definition at line 2668 of file em_cmu.h.

References _CMU_CALCTRL_CONT_SHIFT, BUS_RegBitWrite(), and CMU.

uint32_t CMU_CalibrateCountGet ( void  )

Get the calibration count register.

Note
If continuous calibration mode is active, calibration busy will almost always be off and only the value needs to be read. In a normal case, this function call is triggered by the CALRDY interrupt flag.
Returns
The calibration count, the number of UPSEL clocks (see CMU_CalibrateConfig()) in the period of DOWNSEL oscillator clock cycles configured by a previous write operation to CMU->CALCNT.

Definition at line 4547 of file em_cmu.c.

References _CMU_CALCTRL_CONT_SHIFT, _CMU_STATUS_CALRDY_SHIFT, BUS_RegBitRead(), and CMU.

__STATIC_INLINE void CMU_CalibrateStart ( void  )

Start calibration.

Note
This call is usually invoked after CMU_CalibrateConfig() and possibly CMU_CalibrateCont().

Definition at line 2681 of file em_cmu.h.

References CMU, and CMU_CMD_CALSTART.

CMU_ClkDiv_TypeDef CMU_ClockDivGet ( CMU_Clock_TypeDef  clock)

Get the clock divisor/prescaler.

Parameters
[in]clockA clock point to get the divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual.
Returns
The current clock point divisor/prescaler. 1 is returned if clock specifies a clock point without a divisor/prescaler.

Definition at line 4582 of file em_cmu.c.

References _CMU_LFAPRESC0_LCD_MASK, _CMU_LFAPRESC0_LCD_SHIFT, _CMU_LFAPRESC0_LESENSE_MASK, _CMU_LFAPRESC0_LESENSE_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, CMU, CMU_ClockPrescGet(), CMU_DivToLog2(), cmuClkDiv_1, cmuClkDiv_16, cmuClock_LCDpre, cmuClock_LESENSE, cmuClock_LETIMER0, cmuClock_LEUART0, and SL_Log2ToDiv().

Referenced by UDELAY_Calibrate().

void CMU_ClockDivSet ( CMU_Clock_TypeDef  clock,
CMU_ClkDiv_TypeDef  div 
)

Set the clock divisor/prescaler.

Note
If setting an LF clock prescaler, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.

HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.

Parameters
[in]clockClock point to set divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual.
[in]divThe clock divisor to use (<= cmuClkDiv_512).

Definition at line 4713 of file em_cmu.c.

References _CMU_LFAPRESC0_LCD_MASK, _CMU_LFAPRESC0_LCD_SHIFT, _CMU_LFAPRESC0_LESENSE_MASK, _CMU_LFAPRESC0_LESENSE_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, CMU, CMU_ClockPrescSet(), CMU_DivToLog2(), CMU_SYNCBUSY_LFAPRESC0, CMU_SYNCBUSY_LFBPRESC0, cmuClkDiv_1, cmuClkDiv_128, cmuClkDiv_16, cmuClkDiv_32768, cmuClkDiv_512, cmuClkDiv_8, cmuClock_LCDpre, cmuClock_LESENSE, cmuClock_LETIMER0, cmuClock_LEUART0, SystemCoreClockGet(), and SystemHFClockGet().

Referenced by CAPLESENSE_setupCMU(), RETARGET_SerialInit(), RTCDRV_Init(), SegmentLCD_Init(), UARTDRV_InitLeuart(), and UDELAY_Calibrate().

void CMU_ClockEnable ( CMU_Clock_TypeDef  clock,
bool  enable 
)

Enable/disable a clock.

In general, module clocking is disabled after a reset. If a module clock is disabled, the registers of that module are not accessible and reading from such registers may return undefined values. Writing to registers of clock-disabled modules has no effect. Avoid accessing module registers of a module with a disabled clock.

Note
If enabling/disabling an LF clock, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.

HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.

Parameters
[in]clockThe clock to enable/disable. Notice that not all defined clock points have separate enable/disable control. See the CMU overview in the reference manual.
[in]enable
  • true - enable specified clock.
  • false - disable specified clock.

Definition at line 4921 of file em_cmu.c.

References BUS_RegBitWrite(), CMU, CMU_ClockFreqGet(), CMU_SYNCBUSY_LFACLKEN0, CMU_SYNCBUSY_LFBCLKEN0, CMU_SYNCBUSY_LFECLKEN0, and cmuClock_HFLE.

Referenced by adcInit(), BOARD_init(), BSP_BccDeInit(), BSP_BccInit(), BSP_BusControlModeSet(), BSP_EbiInit(), BSP_initBoard(), BSP_McuBoard_Init(), CAPLESENSE_setupCMU(), CAPSENSE_Init(), DMADRV_DeInit(), ezradio_hal_GpioInit(), gpioInit(), I2CSPM_Init(), ICM20648_spiInit(), initEbiCommon(), initGpio(), LDMA_DeInit(), LDMA_Init(), MIC_init(), MICROSD_Init(), MICROSD_PowerOff(), MICROSD_PowerOn(), MSDD_Init(), RETARGET_SerialInit(), RTCDRV_DeInit(), RTCDRV_Init(), SegmentLCD_Disable(), SegmentLCD_Init(), SPI_TFT_Init(), SPIDRV_DeInit(), SPIDRV_Init(), TOUCH_Init(), UARTDRV_DeInit(), UARTDRV_InitLeuart(), UARTDRV_InitUart(), UDELAY_Calibrate(), USTIMER_DeInit(), USTIMER_Init(), VDDCHECK_Disable(), and VDDCHECK_Init().

uint32_t CMU_ClockFreqGet ( CMU_Clock_TypeDef  clock)

Get the clock frequency for a clock point.

Parameters
[in]clockA clock point to fetch the frequency for.
Returns
The current frequency in Hz.

Definition at line 5045 of file em_cmu.c.

References _CMU_ADCCTRL_ADC0CLKDIV_MASK, _CMU_ADCCTRL_ADC0CLKDIV_SHIFT, _CMU_HFBUSPRESC_MASK, _CMU_HFBUSPRESC_PRESC_SHIFT, _CMU_HFCOREPRESC_PRESC_MASK, _CMU_HFCOREPRESC_PRESC_SHIFT, _CMU_HFEXPPRESC_PRESC_MASK, _CMU_HFEXPPRESC_PRESC_SHIFT, _CMU_HFPERPRESC_PRESC_MASK, _CMU_HFPERPRESC_PRESC_SHIFT, _CMU_HFPERPRESCB_PRESC_MASK, _CMU_HFPERPRESCB_PRESC_SHIFT, _CMU_HFPERPRESCC_PRESC_MASK, _CMU_HFPERPRESCC_PRESC_SHIFT, _CMU_LFAPRESC0_LCD_MASK, _CMU_LFAPRESC0_LCD_SHIFT, _CMU_LFAPRESC0_LESENSE_MASK, _CMU_LFAPRESC0_LESENSE_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_CSEN_MASK, _CMU_LFBPRESC0_CSEN_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, _CMU_LFEPRESC0_RTCC_MASK, _CMU_LFEPRESC0_RTCC_SHIFT, CMU, CMU_DivToLog2(), cmuClkDiv_16, cmuClock_LFA, cmuClock_LFB, cmuClock_LFE, SL_Log2ToDiv(), SystemCoreClockGet(), and SystemHFClockGet().

Referenced by ADC_Init(), ADC_PrescaleCalc(), ADC_TimebaseCalc(), CAN_GetClockFrequency(), CMU_ClockEnable(), CMU_ClockPrescSet(), CMU_ClockSelectSet(), CMU_DPLLLock(), CMU_HFRCOBandSet(), I2C_BusFreqGet(), I2C_BusFreqSet(), LESENSE_ScanFreqSet(), LEUART_BaudrateGet(), LEUART_BaudrateSet(), MIC_init(), MSC_Init(), UARTDRV_InitLeuart(), USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_BaudrateSyncSet(), USTIMER_Init(), UTIL_init(), and VDAC_PrescaleCalc().

void CMU_ClockPrescSet ( CMU_Clock_TypeDef  clock,
CMU_ClkPresc_TypeDef  presc 
)

Set the clock prescaler.

Note
If setting an LF clock prescaler, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.

HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.

Parameters
[in]clockA clock point to set the prescaler for. Notice that not all clock points have a prescaler. See the CMU overview in the reference manual.
[in]prescThe clock prescaler.

Definition at line 5546 of file em_cmu.c.

References _CMU_ADCCTRL_ADC0CLKDIV_MASK, _CMU_ADCCTRL_ADC0CLKDIV_SHIFT, _CMU_HFBUSPRESC_MASK, _CMU_HFBUSPRESC_PRESC_SHIFT, _CMU_HFCOREPRESC_PRESC_MASK, _CMU_HFCOREPRESC_PRESC_SHIFT, _CMU_HFEXPPRESC_PRESC_MASK, _CMU_HFEXPPRESC_PRESC_SHIFT, _CMU_HFPERPRESC_PRESC_MASK, _CMU_HFPERPRESC_PRESC_SHIFT, _CMU_HFPERPRESCB_PRESC_MASK, _CMU_HFPERPRESCB_PRESC_SHIFT, _CMU_HFPERPRESCC_PRESC_MASK, _CMU_HFPERPRESCC_PRESC_SHIFT, _CMU_HFPRESC_PRESC_MASK, _CMU_HFPRESC_PRESC_SHIFT, _CMU_LFAPRESC0_LCD_MASK, _CMU_LFAPRESC0_LCD_SHIFT, _CMU_LFAPRESC0_LESENSE_MASK, _CMU_LFAPRESC0_LESENSE_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_CSEN_MASK, _CMU_LFBPRESC0_CSEN_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, _CMU_LFEPRESC0_RTCC_DIV2, _CMU_LFEPRESC0_RTCC_DIV4, _CMU_LFEPRESC0_RTCC_MASK, _CMU_LFEPRESC0_RTCC_SHIFT, CMU, CMU_ClockFreqGet(), CMU_PrescToLog2(), CMU_SYNCBUSY_LFAPRESC0, CMU_SYNCBUSY_LFBPRESC0, CMU_SYNCBUSY_LFEPRESC0, cmuClock_ADC0ASYNC, cmuClock_CSEN_LF, cmuClock_HFLE, cmuClock_LCD, cmuClock_LCDpre, cmuClock_LESENSE, cmuClock_LETIMER0, cmuClock_LEUART0, cmuClock_RTCC, and SystemCoreClockGet().

Referenced by CMU_ClockDivSet().

CMU_Select_TypeDef CMU_ClockSelectGet ( CMU_Clock_TypeDef  clock)
void CMU_ClockSelectSet ( CMU_Clock_TypeDef  clock,
CMU_Select_TypeDef  ref 
)

Select the reference clock/oscillator used for a clock branch.

Notice that if a selected reference is not enabled prior to selecting its use, it will be enabled and this function will wait for the selected oscillator to be stable. It will however NOT be disabled if another reference clock is selected later.

This feature is particularly important if selecting a new reference clock for the clock branch clocking the core. Otherwise, the system may halt.

Note
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
Parameters
[in]clockA clock branch to select reference clock for. One of:
[in]refA reference selected for clocking. See the reference manual for details about references available for a specific clock branch.

Definition at line 6443 of file em_cmu.c.

References _CMU_ADCCTRL_ADC0CLKSEL_AUXHFRCO, _CMU_ADCCTRL_ADC0CLKSEL_DISABLED, _CMU_ADCCTRL_ADC0CLKSEL_HFSRCCLK, _CMU_ADCCTRL_ADC0CLKSEL_HFXO, _CMU_ADCCTRL_ADC0CLKSEL_MASK, _CMU_ADCCTRL_ADC0CLKSEL_SHIFT, _CMU_HFBUSCLKEN0_LE_SHIFT, _CMU_LFACLKSEL_LFA_DISABLED, _CMU_LFACLKSEL_LFA_LFRCO, _CMU_LFACLKSEL_LFA_LFXO, _CMU_LFACLKSEL_LFA_ULFRCO, _CMU_LFBCLKSEL_LFB_HFCLKLE, BUS_RegBitWrite(), CMU, CMU_ClockFreqGet(), CMU_DBGCLKSEL_DBG_AUXHFRCO, CMU_DBGCLKSEL_DBG_HFCLK, CMU_HFCLKSEL_HF_CLKIN0, CMU_HFCLKSEL_HF_HFRCO, CMU_HFCLKSEL_HF_HFRCODIV2, CMU_HFCLKSEL_HF_HFXO, CMU_HFCLKSEL_HF_LFRCO, CMU_HFCLKSEL_HF_LFXO, CMU_HFRCOBandGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuClock_HFLE, cmuOsc_AUXHFRCO, cmuOsc_CLKIN0, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, cmuOsc_LFXO, cmuSelect_AUXHFRCO, cmuSelect_CLKIN0, cmuSelect_Disabled, cmuSelect_HFCLK, cmuSelect_HFCLKLE, cmuSelect_HFRCO, cmuSelect_HFRCODIV2, cmuSelect_HFSRCCLK, cmuSelect_HFXO, cmuSelect_LFRCO, cmuSelect_LFXO, cmuSelect_ULFRCO, EMU_VScaleEM01ByClock(), EMU_VScaleWait(), SL_FALLTHROUGH, SystemCoreClockGet(), and SystemHFXOClockGet().

Referenced by BSP_BccInit(), BSP_initClocks(), CAPLESENSE_setupCMU(), MIC_init(), RETARGET_SerialInit(), RTCDRV_Init(), SegmentLCD_Init(), UARTDRV_InitLeuart(), and UDELAY_Calibrate().

__STATIC_INLINE uint32_t CMU_DivToLog2 ( CMU_ClkDiv_TypeDef  div)

Convert dividend to logarithmic value. It only works for even numbers equal to 2^n.

Parameters
[in]divAn unscaled dividend.
Returns
Logarithm of 2, as used by fixed prescalers.

Definition at line 2708 of file em_cmu.h.

Referenced by CMU_ClockDivGet(), CMU_ClockDivSet(), CMU_ClockFreqGet(), and RTCDRV_Init().

bool CMU_DPLLLock ( const CMU_DPLLInit_TypeDef init)

Lock the DPLL to a given frequency.

The frequency is given by: Fout = Fref * (N+1) / (M+1).

Note
This function does not check if the given N & M values will actually produce the desired target frequency.
N & M limitations:
300 < N <= 4095
0 <= M <= 4095
Any peripheral running off HFRCO should be switched to HFRCODIV2 prior to calling this function to avoid over-clocking.

HFCLKLE prescaler is automatically modified before updating HFRCO based on the maximum HFLE frequency allowed.

Parameters
[in]initDPLL setup parameters.
Returns
Returns false on invalid target frequency or DPLL locking error.

Definition at line 7175 of file em_cmu.c.

References _CMU_DPLLCTRL1_M_MASK, _CMU_DPLLCTRL1_M_SHIFT, _CMU_DPLLCTRL1_N_MASK, _CMU_DPLLCTRL1_N_SHIFT, _CMU_DPLLCTRL_AUTORECOVER_SHIFT, _CMU_DPLLCTRL_EDGESEL_SHIFT, _CMU_DPLLCTRL_MODE_SHIFT, _CMU_DPLLCTRL_REFSEL_SHIFT, _CMU_HFRCOCTRL_TUNING_MASK, _CMU_HFRCOCTRL_TUNING_SHIFT, _CMU_HFRCOSS_SSAMP_MASK, _CMU_HFRCOSS_SSAMP_SHIFT, _CMU_HFRCOSS_SSINV_MASK, _CMU_HFRCOSS_SSINV_SHIFT, CMU_DPLLInit_TypeDef::autoRecover, CMU, CMU_ClockFreqGet(), CMU_ClockSelectGet(), CMU_HFCLKSEL_HF_HFRCO, CMU_HFCLKSEL_HF_HFRCODIV2, CMU_HFRCODevinfoGet(), CMU_IF_DPLLLOCKFAILHIGH, CMU_IF_DPLLLOCKFAILLOW, CMU_IF_DPLLRDY, CMU_IFC_DPLLLOCKFAILHIGH, CMU_IFC_DPLLLOCKFAILLOW, CMU_IFC_DPLLRDY, CMU_OSCENCMD_DPLLDIS, CMU_OSCENCMD_DPLLEN, CMU_STATUS_DPLLENS, CMU_STATUS_DPLLRDY, cmuClock_HF, cmuClock_HFLE, cmuSelect_HFRCO, cmuSelect_HFRCODIV2, CMU_DPLLInit_TypeDef::edgeSel, EMU_VScaleEM01ByClock(), EMU_VScaleGet(), emuVScaleEM01_LowPower, CMU_DPLLInit_TypeDef::frequency, CMU_DPLLInit_TypeDef::lockMode, CMU_DPLLInit_TypeDef::m, CMU_DPLLInit_TypeDef::n, CMU_DPLLInit_TypeDef::refClk, CMU_DPLLInit_TypeDef::ssAmplitude, CMU_DPLLInit_TypeDef::ssInterval, SystemCoreClockGet(), and SystemHfrcoFreq.

Referenced by BSP_initClocks().

__STATIC_INLINE void CMU_DPLLUnlock ( void  )

Unlock DPLL.

Note
HFRCO is not turned off.

Definition at line 2728 of file em_cmu.h.

References CMU, and CMU_OSCENCMD_DPLLDIS.

void CMU_FreezeEnable ( bool  enable)

CMU low frequency register synchronization freeze control.

Some CMU registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).

Another use case for this feature is using an API (such as the CMU API) for modifying several bit fields consecutively in the same register. If freeze mode is enabled during this sequence, stalling can be avoided.

Note
When enabling freeze mode, this function will wait for all current ongoing CMU synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
Parameters
[in]enable
  • true - enable freeze, modified registers are not propagated to the LF domain
  • false - disable freeze, modified registers are propagated to the LF domain

Definition at line 7331 of file em_cmu.c.

References CMU, and CMU_FREEZE_REGFREEZE.

CMU_HFRCOFreq_TypeDef CMU_HFRCOBandGet ( void  )

Get the current HFRCO frequency.

Returns
HFRCO frequency.

Definition at line 7523 of file em_cmu.c.

References SystemHfrcoFreq.

Referenced by CMU_ClockSelectSet(), and CMU_HFRCOFreqGet().

void CMU_HFRCOBandSet ( CMU_HFRCOFreq_TypeDef  setFreq)

Set the HFRCO calibration for the selected target frequency.

Note
HFCLKLE prescaler is automatically modified based on the maximum HFLE frequency allowed.
Parameters
[in]setFreqHFRCO frequency to set.

Definition at line 7539 of file em_cmu.c.

References _CMU_HFRCOCTRL_CLKDIV_MASK, _CMU_SYNCBUSY_HFRCOBSY_SHIFT, BUS_RegBitRead(), CMU, CMU_ClockFreqGet(), CMU_ClockSelectGet(), CMU_HFRCOCTRL_CLKDIV_DIV1, CMU_HFRCOCTRL_CLKDIV_DIV2, CMU_HFRCOCTRL_CLKDIV_DIV4, CMU_HFRCODevinfoGet(), cmuClock_HF, cmuClock_HFLE, cmuHFRCOFreq_1M0Hz, cmuHFRCOFreq_2M0Hz, cmuHFRCOFreq_4M0Hz, cmuSelect_HFRCO, EMU_VScaleEM01ByClock(), SystemCoreClockGet(), and SystemHfrcoFreq.

Referenced by CMU_HFRCOFreqSet().

static uint32_t CMU_HFRCODevinfoGet ( CMU_HFRCOFreq_TypeDef  freq)
static

Get the HFRCO frequency calibration word in DEVINFO.

Parameters
[in]freqFrequency in Hz.
Returns
HFRCO calibration word for a given frequency.

Definition at line 7461 of file em_cmu.c.

References cmuHFRCOFreq_13M0Hz, cmuHFRCOFreq_16M0Hz, cmuHFRCOFreq_19M0Hz, cmuHFRCOFreq_1M0Hz, cmuHFRCOFreq_26M0Hz, cmuHFRCOFreq_2M0Hz, cmuHFRCOFreq_32M0Hz, cmuHFRCOFreq_38M0Hz, cmuHFRCOFreq_48M0Hz, cmuHFRCOFreq_4M0Hz, cmuHFRCOFreq_7M0Hz, and DEVINFO.

Referenced by CMU_DPLLLock(), and CMU_HFRCOBandSet().

__STATIC_INLINE CMU_HFRCOFreq_TypeDef CMU_HFRCOFreqGet ( void  )

Get the current HFRCO frequency.

Deprecated:
A deprecated function. New code should use CMU_HFRCOBandGet().
Returns
HFRCO frequency.

Definition at line 2878 of file em_cmu.h.

References CMU_HFRCOBandGet().

__STATIC_INLINE void CMU_HFRCOFreqSet ( CMU_HFRCOFreq_TypeDef  setFreq)

Set HFRCO calibration for the selected target frequency.

Deprecated:
A deprecated function. New code should use CMU_HFRCOBandSet().
Parameters
[in]setFreqHFRCO frequency to set.

Definition at line 2893 of file em_cmu.h.

References CMU_HFRCOBandSet().

void CMU_HFXOAutostartEnable ( uint32_t  userSel,
bool  enEM0EM1Start,
bool  enEM0EM1StartSel 
)

Enable or disable HFXO autostart.

Parameters
[in]userSelAdditional user specified enable bit.
[in]enEM0EM1StartIf true, HFXO is automatically started upon entering EM0/EM1 entry from EM2/EM3. HFXO selection has to be handled by the user. If false, HFXO is not started automatically when entering EM0/EM1.
[in]enEM0EM1StartSelIf true, HFXO is automatically started and immediately selected upon entering EM0/EM1 entry from EM2/EM3. Note that this option stalls the use of HFSRCCLK until HFXO becomes ready. HFCLKLE prescaler is also automatically modified if userSel is specified. If false, HFXO is not started or selected automatically when entering EM0/EM1.

Definition at line 7767 of file em_cmu.c.

References _CMU_HFXOCTRL_AUTOSTARTEM0EM1_MASK, _CMU_HFXOCTRL_AUTOSTARTSELEM0EM1_MASK, _EMU_CTRL_EM23VSCALE_MASK, CMU, CMU_HFXOCTRL_AUTOSTARTEM0EM1, CMU_HFXOCTRL_AUTOSTARTSELEM0EM1, CMU_OscillatorEnable(), cmuOsc_HFXO, EMU, EMU_CTRL_EM23VSCALE_VSCALE2, EMU_VScaleEM01ByClock(), and SystemHFXOClockGet().

Referenced by BSP_initClocks().

__STATIC_INLINE void CMU_IntClear ( uint32_t  flags)

Clear one or more pending CMU interrupts.

Parameters
[in]flagsCMU interrupt sources to clear.

Definition at line 2741 of file em_cmu.h.

References CMU.

__STATIC_INLINE void CMU_IntDisable ( uint32_t  flags)

Disable one or more CMU interrupts.

Parameters
[in]flagsCMU interrupt sources to disable.

Definition at line 2753 of file em_cmu.h.

References CMU.

__STATIC_INLINE void CMU_IntEnable ( uint32_t  flags)

Enable one or more CMU interrupts.

Note
Depending on use case, a pending interrupt may already be set prior to enabling the interrupt. Consider using CMU_IntClear() prior to enabling if the pending interrupt should be ignored.
Parameters
[in]flagsCMU interrupt sources to enable.

Definition at line 2770 of file em_cmu.h.

References CMU.

__STATIC_INLINE uint32_t CMU_IntGet ( void  )

Get pending CMU interrupts.

Returns
CMU interrupt sources pending.

Definition at line 2782 of file em_cmu.h.

References CMU.

__STATIC_INLINE uint32_t CMU_IntGetEnabled ( void  )

Get enabled and pending CMU interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
This function does not clear event bits.
Returns
Pending and enabled CMU interrupt sources. The return value is the bitwise AND of
  • the enabled interrupt sources in CMU_IEN and
  • the pending interrupt flags CMU_IF

Definition at line 2803 of file em_cmu.h.

References CMU.

__STATIC_INLINE void CMU_IntSet ( uint32_t  flags)

Set one or more pending CMU interrupts.

Parameters
[in]flagsCMU interrupt sources to set to pending.

Definition at line 2818 of file em_cmu.h.

References CMU.

uint32_t CMU_LCDClkFDIVGet ( void  )

Get the LCD framerate divisor (FDIV) setting.

Returns
The LCD framerate divisor.

Definition at line 7968 of file em_cmu.c.

References CMU.

void CMU_LCDClkFDIVSet ( uint32_t  div)

Set the LCD framerate divisor (FDIV) setting.

Note
The FDIV field (CMU LCDCTRL register) should only be modified while the LCD module is clock disabled (CMU LFACLKEN0.LCD bit is 0). This function will NOT modify FDIV if the LCD module clock is enabled. See CMU_ClockEnable() for disabling/enabling LCD clock.
Parameters
[in]divThe FDIV setting to use.

Definition at line 7990 of file em_cmu.c.

References CMU, CMU_LFACLKEN0_LCD, and cmuClkDiv_128.

Referenced by SegmentLCD_Init().

void CMU_LFXOInit ( const CMU_LFXOInit_TypeDef lfxoInit)

Set LFXO control registers.

Note
LFXO configuration should be obtained from a configuration tool, app note, or xtal data sheet. This function disables the LFXO when necessary to ensure a valid state before update.
Parameters
[in]lfxoInitLFXO setup parameters.

Definition at line 8020 of file em_cmu.c.

References _CMU_LFXOCTRL_GAIN_MASK, _CMU_LFXOCTRL_GAIN_SHIFT, _CMU_LFXOCTRL_MODE_MASK, _CMU_LFXOCTRL_MODE_SHIFT, _CMU_LFXOCTRL_TIMEOUT_MASK, _CMU_LFXOCTRL_TIMEOUT_SHIFT, _CMU_LFXOCTRL_TUNING_MASK, _CMU_LFXOCTRL_TUNING_SHIFT, BUS_RegBitWrite(), BUS_RegMaskedWrite(), CMU, CMU_ClockSelectGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuOsc_LFXO, cmuSelect_LFXO, CMU_LFXOInit_TypeDef::ctune, EMU, CMU_LFXOInit_TypeDef::gain, CMU_LFXOInit_TypeDef::mode, and CMU_LFXOInit_TypeDef::timeout.

Referenced by BSP_initClocks().

__STATIC_INLINE void CMU_Lock ( void  )

Lock the CMU to protect some of its registers against unintended modification.

See the reference manual for CMU registers that will be locked.

Note
If locking the CMU registers, they must be unlocked prior to using any CMU API functions modifying CMU registers protected by the lock.

Definition at line 2836 of file em_cmu.h.

References CMU, and CMU_LOCK_LOCKKEY_LOCK.

Referenced by EMU_EnterEM3().

__STATIC_INLINE uint32_t CMU_Log2ToDiv ( uint32_t  log2)

Convert logarithm of 2 prescaler to division factor.

Deprecated:
Deprecated and marked for removal in a later release. It will be replaced by SL_Log2ToDiv.
Parameters
[in]log2Logarithm of 2, as used by fixed prescalers.
Returns
Dividend.

Definition at line 2853 of file em_cmu.h.

References SL_Log2ToDiv().

void CMU_OscillatorEnable ( CMU_Osc_TypeDef  osc,
bool  enable,
bool  wait 
)

Enable/disable oscillator.

Note
WARNING: When this function is called to disable either cmuOsc_LFXO or cmuOsc_HFXO, the LFXOMODE or HFXOMODE fields of the CMU_CTRL register are reset to the reset value. In other words, if external clock sources are selected in either LFXOMODE or HFXOMODE fields, the configuration will be cleared and needs to be reconfigured if needed later.
Parameters
[in]oscThe oscillator to enable/disable.
[in]enable
  • true - enable specified oscillator.
  • false - disable specified oscillator.
[in]waitOnly used if enable is true.
  • true - wait for oscillator start-up time to timeout before returning.
  • false - do not wait for oscillator start-up time to timeout before returning.

Definition at line 8087 of file em_cmu.c.

References _CMU_HFXOCTRL_MODE_MASK, _CMU_STATUS_AUXHFRCOENS_SHIFT, _CMU_STATUS_AUXHFRCORDY_SHIFT, _CMU_STATUS_HFRCOENS_SHIFT, _CMU_STATUS_HFRCORDY_SHIFT, _CMU_STATUS_HFXOENS_SHIFT, _CMU_STATUS_HFXORDY_SHIFT, _CMU_STATUS_LFRCOENS_SHIFT, _CMU_STATUS_LFRCORDY_SHIFT, _CMU_STATUS_LFXOENS_SHIFT, _CMU_STATUS_LFXORDY_SHIFT, BUS_RegBitRead(), CMU, CMU_HFXOCTRL_MODE_DIGEXTCLK, CMU_OSCENCMD_AUXHFRCODIS, CMU_OSCENCMD_AUXHFRCOEN, CMU_OSCENCMD_HFRCODIS, CMU_OSCENCMD_HFRCOEN, CMU_OSCENCMD_HFXODIS, CMU_OSCENCMD_HFXOEN, CMU_OSCENCMD_LFRCODIS, CMU_OSCENCMD_LFRCOEN, CMU_OSCENCMD_LFXODIS, CMU_OSCENCMD_LFXOEN, CMU_OscillatorTuningGet(), CMU_OscillatorTuningOptimize(), CMU_OscillatorTuningSet(), CMU_OscillatorTuningWait(), cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, cmuOsc_LFXO, EMU, and EMU_PWRCTRL_REGPWRSEL_DVDD.

Referenced by BSP_initClocks(), CMU_ClockSelectSet(), CMU_HFXOAutostartEnable(), CMU_HFXOInit(), CMU_LFXOInit(), and UDELAY_Calibrate().

uint32_t CMU_OscillatorTuningGet ( CMU_Osc_TypeDef  osc)

Get the oscillator frequency tuning setting.

Parameters
[in]oscAn oscillator to get tuning value for, one of the following:
Returns
The oscillator frequency tuning setting in use.

Definition at line 8276 of file em_cmu.c.

References _CMU_AUXHFRCOCTRL_TUNING_MASK, _CMU_AUXHFRCOCTRL_TUNING_SHIFT, _CMU_HFRCOCTRL_TUNING_MASK, _CMU_HFRCOCTRL_TUNING_SHIFT, _CMU_HFXOTRIMSTATUS_IBTRIMXOCORE_MASK, _CMU_LFRCOCTRL_TUNING_MASK, _CMU_LFRCOCTRL_TUNING_SHIFT, CMU, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, and cmuOsc_LFRCO.

Referenced by CMU_OscillatorEnable().

bool CMU_OscillatorTuningOptimize ( CMU_Osc_TypeDef  osc,
CMU_HFXOTuningMode_TypeDef  mode,
bool  wait 
)

Start and optionally wait for the oscillator tuning optimization.

Parameters
[in]oscAn oscillator to set tuning value for, one of the following:
[in]modeTuning optimization mode.
[in]waitWait for tuning optimization to complete. true - wait for tuning optimization to complete. false - return without waiting.
Returns
Returns false on invalid parameters or oscillator error status.

Definition at line 8520 of file em_cmu.c.

References CMU, CMU_OscillatorTuningWait(), and cmuOsc_HFXO.

Referenced by CMU_OscillatorEnable().

void CMU_OscillatorTuningSet ( CMU_Osc_TypeDef  osc,
uint32_t  val 
)

Set the oscillator frequency tuning control.

Note
Oscillator tuning is done during production and the tuning value is automatically loaded after reset. Changing the tuning value from the calibrated value is for more advanced use. Certain oscillators also have build-in tuning optimization.
Parameters
[in]oscAn oscillator to set tuning value for, one of the following:
[in]valThe oscillator frequency tuning setting to use.

Definition at line 8344 of file em_cmu.c.

References _CMU_AUXHFRCOCTRL_TUNING_MASK, _CMU_AUXHFRCOCTRL_TUNING_SHIFT, _CMU_HFRCOCTRL_TUNING_MASK, _CMU_HFRCOCTRL_TUNING_SHIFT, _CMU_HFXOSTEADYSTATECTRL_IBTRIMXOCORE_MASK, _CMU_LFRCOCTRL_TUNING_MASK, _CMU_LFRCOCTRL_TUNING_SHIFT, _CMU_SYNCBUSY_AUXHFRCOBSY_SHIFT, _CMU_SYNCBUSY_HFRCOBSY_SHIFT, _CMU_SYNCBUSY_LFRCOBSY_SHIFT, BUS_RegBitRead(), CMU, CMU_STATUS_HFXOENS, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, and cmuOsc_LFRCO.

Referenced by CMU_OscillatorEnable().

bool CMU_OscillatorTuningWait ( CMU_Osc_TypeDef  osc,
CMU_HFXOTuningMode_TypeDef  mode 
)

Wait for the oscillator tuning optimization.

Parameters
[in]oscAn oscillator to set tuning value for, one of the following:
[in]modeTuning optimization mode.
Returns
Returns false on invalid parameters or oscillator error status.

Definition at line 8454 of file em_cmu.c.

References _CMU_STATUS_MASK, CMU, CMU_STATUS_HFXOPEAKDETRDY, and cmuOsc_HFXO.

Referenced by CMU_OscillatorEnable(), and CMU_OscillatorTuningOptimize().

bool CMU_PCNTClockExternalGet ( unsigned int  instance)

Determine if the currently selected PCNTn clock used is external or LFBCLK.

Parameters
[in]instancePCNT instance number to get currently selected clock source for.
Returns
  • true - selected clock is external clock.
  • false - selected clock is LFBCLK.

Definition at line 8557 of file em_cmu.c.

References CMU, and CMU_PCNTCTRL_PCNT0CLKSEL_PCNT0S0.

void CMU_PCNTClockExternalSet ( unsigned int  instance,
bool  external 
)

Select the PCNTn clock.

Parameters
[in]instancePCNT instance number to set selected clock source for.
[in]externalSet to true to select the external clock, false to select LFBCLK.

Definition at line 8597 of file em_cmu.c.

References BUS_RegBitWrite(), CMU, and PCNT_COUNT.

Referenced by PCNT_Init(), and PCNT_Reset().

__STATIC_INLINE uint32_t CMU_PrescToLog2 ( uint32_t  presc)

Convert prescaler dividend to a logarithmic value. It only works for even numbers equal to 2^n.

Parameters
[in]prescAn unscaled dividend (dividend = presc + 1).
Returns
Logarithm of 2, as used by fixed 2^n prescalers.

Definition at line 2945 of file em_cmu.h.

References SL_Log2ToDiv().

Referenced by CMU_ClockPrescSet().