SMU_PrivilegedAccess_TypeDef Struct ReferenceEMLIB > SMU

SMU peripheral privileged access enablers.

Definition at line 485 of file em_smu.h.

#include <em_smu.h>

Data Fields

bool privilegedACMP0: 1
 
bool privilegedACMP1: 1
 
bool privilegedADC0: 1
 
bool privilegedCAN0: 1
 
bool privilegedCMU: 1
 
bool privilegedCRYOTIMER: 1
 
bool privilegedCRYPTO0: 1
 
bool privilegedCSEN: 1
 
bool privilegedEMU: 1
 
bool privilegedGPCRC: 1
 
bool privilegedGPIO: 1
 
bool privilegedI2C0: 1
 
bool privilegedI2C1: 1
 
bool privilegedLCD: 1
 
bool privilegedLDMA: 1
 
bool privilegedLESENSE: 1
 
bool privilegedLETIMER0: 1
 
bool privilegedLEUART0: 1
 
bool privilegedMSC: 1
 
bool privilegedPCNT0: 1
 
bool privilegedPRS: 1
 
bool privilegedRMU: 1
 
bool privilegedRTCC: 1
 
bool privilegedSMU: 1
 
bool privilegedTIMER0: 1
 
bool privilegedTIMER1: 1
 
bool privilegedTRNG0: 1
 
bool privilegedUART0: 1
 
bool privilegedUSART0: 1
 
bool privilegedUSART1: 1
 
bool privilegedUSART2: 1
 
bool privilegedUSART3: 1
 
bool privilegedVDAC0: 1
 
bool privilegedWDOG0: 1
 
bool privilegedWTIMER0: 1
 
bool privilegedWTIMER1: 1
 

Field Documentation

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP0

Privileged access enabler for ACMP0.

Definition at line 694 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP1

Privileged access enabler for ACMP1.

Definition at line 695 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedADC0

Privileged access enabler for ADC0.

Definition at line 696 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCAN0

Privileged access enabler for CAN0.

Definition at line 697 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCMU

Privileged access enabler for CMU.

Definition at line 698 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYOTIMER

Privileged access enabler for CRYOTIMER.

Definition at line 699 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO0

Privileged access enabler for CRYPTO0.

Definition at line 700 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCSEN

Privileged access enabler for CSEN.

Definition at line 701 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedEMU

Privileged access enabler for EMU.

Definition at line 704 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPCRC

Privileged access enabler for GPCRC.

Definition at line 705 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPIO

Privileged access enabler for GPIO.

Definition at line 706 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C0

Privileged access enabler for I2C0.

Definition at line 707 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C1

Privileged access enabler for I2C1.

Definition at line 708 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLCD

Privileged access enabler for LCD.

Definition at line 710 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMA

Privileged access enabler for LDMA.

Definition at line 711 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLESENSE

Privileged access enabler for LESENSE.

Definition at line 712 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLETIMER0

Privileged access enabler for LETIMER0.

Definition at line 713 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLEUART0

Privileged access enabler for LEUART0.

Definition at line 714 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedMSC

Privileged access enabler for MAC.

Definition at line 709 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT0

Privileged access enabler for PCNT0.

Definition at line 715 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPRS

Privileged access enabler for PRS.

Definition at line 703 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRMU

Privileged access enabler for RMU.

Definition at line 716 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRTCC

Privileged access enabler for RTCC.

Definition at line 717 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedSMU

Privileged access enabler for SMU.

Definition at line 718 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER0

Privileged access enabler for TIMER0.

Definition at line 719 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER1

Privileged access enabler for TIMER1.

Definition at line 720 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTRNG0

Privileged access enabler for TRNG0.

Definition at line 721 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUART0

Privileged access enabler for UART0.

Definition at line 722 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART0

Privileged access enabler for USART0.

Definition at line 723 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART1

Privileged access enabler for USART1.

Definition at line 724 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART2

Privileged access enabler for USART2.

Definition at line 725 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART3

Privileged access enabler for USART3.

Definition at line 726 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedVDAC0

Privileged access enabler for VDAC0.

Definition at line 702 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG0

Privileged access enabler for WDOG0.

Definition at line 727 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER0

Privileged access enabler for WTIMER0.

Definition at line 728 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER1

Privileged access enabler for WTIMER1.

Definition at line 729 of file em_smu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/em_smu.h