LESENSE_CH_TypeDef Struct ReferenceDevices

LESENSE_CH EFM32WG LESENSE CH.

Definition at line 46 of file efm32wg_lesense_ch.h.

#include <efm32wg_lesense_ch.h>

Data Fields

__IOM uint32_t EVAL
 
__IOM uint32_t INTERACT
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t TIMING
 

Field Documentation

__IOM uint32_t LESENSE_CH_TypeDef::EVAL

Scan configuration

Definition at line 49 of file efm32wg_lesense_ch.h.

__IOM uint32_t LESENSE_CH_TypeDef::INTERACT

Scan configuration

Definition at line 48 of file efm32wg_lesense_ch.h.

uint32_t LESENSE_CH_TypeDef::RESERVED0[1U]

Reserved future

Definition at line 50 of file efm32wg_lesense_ch.h.

__IOM uint32_t LESENSE_CH_TypeDef::TIMING

Scan configuration

Definition at line 47 of file efm32wg_lesense_ch.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/efm32wg_lesense_ch.h