PRS_TypeDef Struct ReferenceDevices > EFM32WG_PRS

Definition at line 48 of file efm32wg_prs.h.

Data Fields

PRS_CH_TypeDef CH [12U]
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTE
 
__IOM uint32_t SWLEVEL
 
__IOM uint32_t SWPULSE
 

Field Documentation

PRS_CH_TypeDef PRS_TypeDef::CH[12U]

Channel registers

Definition at line 54 of file efm32wg_prs.h.

uint32_t PRS_TypeDef::RESERVED0[1U]

Reserved registers

Definition at line 53 of file efm32wg_prs.h.

__IOM uint32_t PRS_TypeDef::ROUTE

I/O Routing Register

Definition at line 51 of file efm32wg_prs.h.

__IOM uint32_t PRS_TypeDef::SWLEVEL

Software Level Register

Definition at line 50 of file efm32wg_prs.h.

__IOM uint32_t PRS_TypeDef::SWPULSE

Software Pulse Register

Definition at line 49 of file efm32wg_prs.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/efm32wg_prs.h