USART_TypeDef Struct ReferenceDevices > USART

USART Register Declaration

Definition at line 48 of file efr32mg12p_usart.h.

#include <efr32mg12p_usart.h>

Data Fields

__IOM uint32_t CLKDIV
 
__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRLX
 
__IOM uint32_t FRAME
 
__IOM uint32_t I2SCTRL
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t INPUT
 
__IOM uint32_t IRCTRL
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTELOC0
 
__IOM uint32_t ROUTELOC1
 
__IOM uint32_t ROUTEPEN
 
__IM uint32_t RXDATA
 
__IM uint32_t RXDATAX
 
__IM uint32_t RXDATAXP
 
__IM uint32_t RXDOUBLE
 
__IM uint32_t RXDOUBLEX
 
__IM uint32_t RXDOUBLEXP
 
__IM uint32_t STATUS
 
__IOM uint32_t TIMECMP0
 
__IOM uint32_t TIMECMP1
 
__IOM uint32_t TIMECMP2
 
__IOM uint32_t TIMING
 
__IOM uint32_t TRIGCTRL
 
__IOM uint32_t TXDATA
 
__IOM uint32_t TXDATAX
 
__IOM uint32_t TXDOUBLE
 
__IOM uint32_t TXDOUBLEX
 

Field Documentation

__IOM uint32_t USART_TypeDef::CLKDIV

Clock Control Register

Definition at line 54 of file efr32mg12p_usart.h.

Referenced by USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_BaudrateSyncSet(), and USART_Reset().

__IOM uint32_t USART_TypeDef::CMD

Command Register

Definition at line 52 of file efr32mg12p_usart.h.

Referenced by UARTDRV_InitUart(), USART_Enable(), USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::CTRL

Control Register

Definition at line 49 of file efr32mg12p_usart.h.

Referenced by SPIDRV_Init(), USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_InitAsync(), USART_InitSync(), USART_Reset(), and USARTn_InitIrDA().

__IOM uint32_t USART_TypeDef::CTRLX

Control Register Extended

Definition at line 74 of file efr32mg12p_usart.h.

Referenced by prsRxInput(), UARTDRV_InitUart(), and USART_Reset().

__IOM uint32_t USART_TypeDef::FRAME

USART Frame Format Register

Definition at line 50 of file efr32mg12p_usart.h.

Referenced by USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::I2SCTRL

I2S Control Register

Definition at line 72 of file efr32mg12p_usart.h.

Referenced by USART_InitI2s(), and USART_Reset().

__IOM uint32_t USART_TypeDef::IEN

Interrupt Enable Register

Definition at line 68 of file efr32mg12p_usart.h.

Referenced by USART_IntDisable(), USART_IntEnable(), USART_IntGetEnabled(), and USART_Reset().

__IM uint32_t USART_TypeDef::IF

Interrupt Flag Register

Definition at line 65 of file efr32mg12p_usart.h.

Referenced by USART_IntGet(), and USART_IntGetEnabled().

__IOM uint32_t USART_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 67 of file efr32mg12p_usart.h.

Referenced by USART_IntClear(), and USART_Reset().

__IOM uint32_t USART_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 66 of file efr32mg12p_usart.h.

Referenced by USART_IntSet().

__IOM uint32_t USART_TypeDef::INPUT

USART Input Register

Definition at line 71 of file efr32mg12p_usart.h.

Referenced by prsRxInput(), and USART_Reset().

__IOM uint32_t USART_TypeDef::IRCTRL

IrDA Control Register

Definition at line 69 of file efr32mg12p_usart.h.

Referenced by prsIrInput(), USART_Reset(), and USARTn_InitIrDA().

uint32_t USART_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 70 of file efr32mg12p_usart.h.

__IOM uint32_t USART_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 79 of file efr32mg12p_usart.h.

Referenced by ICM20648_spiInit(), RETARGET_SerialInit(), SPIDRV_Init(), UARTDRV_InitUart(), and USART_Reset().

__IOM uint32_t USART_TypeDef::ROUTELOC1

I/O Routing Location Register

Definition at line 80 of file efr32mg12p_usart.h.

Referenced by UARTDRV_InitUart(), and USART_Reset().

__IOM uint32_t USART_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 78 of file efr32mg12p_usart.h.

Referenced by ICM20648_spiInit(), RETARGET_SerialInit(), SPIDRV_Init(), UARTDRV_InitUart(), USART_InitAsync(), and USART_Reset().

__IM uint32_t USART_TypeDef::RXDATA

RX Buffer Data Register

Definition at line 56 of file efr32mg12p_usart.h.

Referenced by USART_Rx(), USART_RxDataGet(), and USART_SpiTransfer().

__IM uint32_t USART_TypeDef::RXDATAX

RX Buffer Data Extended Register

Definition at line 55 of file efr32mg12p_usart.h.

Referenced by USART_RxDataXGet(), and USART_RxExt().

__IM uint32_t USART_TypeDef::RXDATAXP

RX Buffer Data Extended Peek Register

Definition at line 59 of file efr32mg12p_usart.h.

__IM uint32_t USART_TypeDef::RXDOUBLE

RX FIFO Double Data Register

Definition at line 58 of file efr32mg12p_usart.h.

Referenced by USART_RxDouble(), and USART_RxDoubleGet().

__IM uint32_t USART_TypeDef::RXDOUBLEX

RX Buffer Double Data Extended Register

Definition at line 57 of file efr32mg12p_usart.h.

Referenced by USART_RxDoubleExt(), and USART_RxDoubleXGet().

__IM uint32_t USART_TypeDef::RXDOUBLEXP

RX Buffer Double Data Extended Peek Register

Definition at line 60 of file efr32mg12p_usart.h.

__IM uint32_t USART_TypeDef::STATUS

USART Status Register

Definition at line 53 of file efr32mg12p_usart.h.

Referenced by USART_Rx(), USART_RxDouble(), USART_RxDoubleExt(), USART_RxExt(), USART_SpiTransfer(), USART_StatusGet(), USART_Tx(), USART_TxDouble(), USART_TxDoubleExt(), and USART_TxExt().

__IOM uint32_t USART_TypeDef::TIMECMP0

Used to Generate Interrupts and Various Delays

Definition at line 75 of file efr32mg12p_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP1

Used to Generate Interrupts and Various Delays

Definition at line 76 of file efr32mg12p_usart.h.

__IOM uint32_t USART_TypeDef::TIMECMP2

Used to Generate Interrupts and Various Delays

Definition at line 77 of file efr32mg12p_usart.h.

__IOM uint32_t USART_TypeDef::TIMING

Timing Register

Definition at line 73 of file efr32mg12p_usart.h.

Referenced by USART_InitAsync(), USART_InitSync(), and USART_Reset().

__IOM uint32_t USART_TypeDef::TRIGCTRL

USART Trigger Control Register

Definition at line 51 of file efr32mg12p_usart.h.

Referenced by prsTriggerInput(), USART_InitPrsTrigger(), and USART_Reset().

__IOM uint32_t USART_TypeDef::TXDATA

TX Buffer Data Register

Definition at line 62 of file efr32mg12p_usart.h.

Referenced by USART_SpiTransfer(), and USART_Tx().

__IOM uint32_t USART_TypeDef::TXDATAX

TX Buffer Data Extended Register

Definition at line 61 of file efr32mg12p_usart.h.

Referenced by USART_TxExt().

__IOM uint32_t USART_TypeDef::TXDOUBLE

TX Buffer Double Data Register

Definition at line 64 of file efr32mg12p_usart.h.

Referenced by USART_TxDouble().

__IOM uint32_t USART_TypeDef::TXDOUBLEX

TX Buffer Double Data Extended Register

Definition at line 63 of file efr32mg12p_usart.h.

Referenced by USART_TxDoubleExt().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/efr32mg12p_usart.h