7.1.1 Security Manager# Security Manager. The commands in this class manage Bluetooth ... 0: Prefer just works pairing when both options are possible based on the settings.
// Bluetooth LE//Version 5.0 //API Reference ... To use these new events, the application needs to include the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component.
For legacy devices (BLExxx) <=1.5.0 4.0 ... Bluetooth 4.2 specifies the PHY bitrate to be exactly 1 Mbps. Bluetooth 5 (introduced in Bluetooth SDK v2.3) specifies PHY bitrates as follows:
0 dBm is enough to cover about 10 to 15 m range, based on tests made with iBeacon example and Android ... events app_assert_status(sc); // Start general advertising and enable connections.
Results 1-6 of 6 for mcu/latest/structIADC-AllConfigs-t/