Class List
Here are the classes, structs, unions and interfaces with brief descriptions:
CotActiveScanResult | This structure represents a received IEEE 802.15.4 Beacon |
CotBackboneRouterConfig | This structure represents Backbone Router configuration |
CotBackboneRouterMulticastListenerInfo | This structure represents a Backbone Router Multicast Listener info |
CotBackboneRouterNdProxyInfo | Represents the Backbone Router ND Proxy info |
CotBorderRouterConfig | This structure represents a Border Router configuration |
CotBufferInfo | This structure represents the message buffer information for different queues used by OpenThread stack |
CotCacheEntryInfo | This structure represents an EID cache entry |
CotCacheEntryIterator | This type represents an iterator used for iterating through the EID cache table entries |
CotChildInfo | This structure holds diagnostic information for a Thread Child |
CotCliCommand | This structure represents a CLI command |
CotCoapBlockwiseResource | This structure represents a CoAP resource with block-wise transfer |
CotCoapOption | This structure represents a CoAP option |
CotCoapOptionIterator | This structure acts as an iterator for CoAP options |
CotCoapResource | This structure represents a CoAP resource |
CotCoapTxParameters | This structure represents the CoAP transmission parameters |
CotCommissioningDataset | This structure represents a Commissioning Dataset |
CotCryptoContext | This structure stores the context object for platform APIs |
CotCryptoKey | This structure represents the Key Material required for Crypto operations |
CotCryptoSha256Hash | This structure represents a SHA-256 hash |
CotDnsQueryConfig | This structure represents a DNS query configuration |
CotDnssdCounters | This structure contains the counters of DNS-SD server |
CotDnssdHostInfo | This structure represents information of a discovered host for a DNS-SD query |
CotDnssdServiceInstanceInfo | This structure represents information of a discovered service instance for a DNS-SD query |
CotDnsServiceInfo | This structure provides info for a DNS service instance |
CotDnsTxtEntry | This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3) |
CotDnsTxtEntryIterator | This structure represents an iterator for TXT record entires (key/value pairs) |
CotEnergyScanResult | This structure represents an energy scan result |
CotExtAddress | This structure represents the IEEE 802.15.4 Extended Address |
CotExtendedPanId | This structure represents an Extended PAN ID |
CotExternalRouteConfig | This structure represents an External Route configuration |
CotHistoryTrackerExternalRouteInfo | This structure represent a Network Data extern route info |
CotHistoryTrackerIterator | This type represents an iterator to iterate through a history list |
CotHistoryTrackerMessageInfo | This structure represents a RX/TX IPv6 message info |
CotHistoryTrackerMulticastAddressInfo | This structure represent an IPv6 multicast address info |
CotHistoryTrackerNeighborInfo | This structure represents a neighbor info |
CotHistoryTrackerNetworkInfo | This structure represents Thread network info |
CotHistoryTrackerOnMeshPrefixInfo | This structure represent a Network Data on mesh prefix info |
CotHistoryTrackerUnicastAddressInfo | This structure represent a unicast IPv6 address info |
CotIcmp6Handler | This structure implements ICMPv6 message handler |
►CotIcmp6Header | This structure represents an ICMPv6 header |
►CotIp6Address | This structure represents an IPv6 address |
CotIp6AddressComponents | This structure represents the components of an IPv6 address |
CotIp6AddressInfo | This structure represents IPv6 address information |
►CotIp6InterfaceIdentifier | This structure represents the Interface Identifier of an IPv6 address |
CotIp6NetworkPrefix | This structure represents the Network Prefix of an IPv6 address (most significant 64 bits of the address) |
CotIp6Prefix | This structure represents an IPv6 prefix |
CotIpCounters | This structure represents the IP level counters |
CotJoinerDiscerner | This structure represents a Joiner Discerner |
CotJoinerInfo | This structure represents a Joiner Info |
CotJoinerPskd | This structure represents a Joiner PSKd |
CotLeaderData | This structure represents the Thread Leader Data |
CotLinkedBuffer | A linked buffer structure for use with TCP |
CotLinkMetrics | This structure represents what metrics are specified to query |
CotLinkMetricsSeriesFlags | This structure represents which frames are accounted in a Forward Tracking Series |
CotLinkMetricsValues | This structure represents the result (value) for a Link Metrics query |
CotLinkModeConfig | This structure represents an MLE Link Mode configuration |
CotMacCounters | This structure represents the MAC layer counters |
CotMacFilterEntry | This structure represents a Mac Filter entry |
CotMacKey | This structure represents a MAC Key |
CotMacKeyMaterial | This structure represents a MAC Key |
CotMessageBuffer | This struct represents an OpenThread message buffer |
CotMessageInfo | This structure represents the local and peer IPv6 socket addresses |
CotMessageQueue | This structure represents an OpenThread message queue |
CotMessageQueueInfo | This structure represents information about a message queue |
CotMessageSettings | This structure represents a message settings |
CotMleCounters | This structure represents the Thread MLE counters |
CotMultiRadioNeighborInfo | This type represents multi radio link information associated with a neighbor |
CotNcpLegacyHandlers | Defines a struct containing all the legacy handlers (function pointers) |
CotNeighborInfo | This structure holds diagnostic information for a neighboring Thread node |
CotNeighborTableEntryInfo | This type represent a neighbor table entry info (child or router) and is used as a parameter in the neighbor table callback otNeighborTableCallback |
CotNetifAddress | This structure represents an IPv6 network interface unicast address |
CotNetifMulticastAddress | This structure represents an IPv6 network interface multicast address |
CotNetworkDiagChildEntry | This structure represents a Network Diagnostic Child Table Entry |
CotNetworkDiagConnectivity | This structure represents a Network Diagnostic Connectivity value |
CotNetworkDiagMacCounters | This structure represents a Network Diagnostic Mac Counters value |
CotNetworkDiagRoute | This structure represents a Network Diagnostic Route TLV value |
CotNetworkDiagRouteData | This structure represents a Network Diagnostic Route data |
CotNetworkDiagTlv | This structure represents a Network Diagnostic TLV |
CotNetworkKey | This structure represents a Thread Network Key |
CotNetworkName | This structure represents a Network Name |
CotOperationalDataset | This structure represents an Active or Pending Operational Dataset |
CotOperationalDatasetComponents | This structure represents presence of different components in Active or Pending Operational Dataset |
CotOperationalDatasetTlvs | This structure represents an Active or Pending Operational Dataset |
CotPingSenderConfig | This structure represents a ping request configuration |
CotPingSenderReply | This structure represents a ping reply |
CotPingSenderStatistics | This structure represents statistics of a ping request |
CotPlatTrelPeerInfo | This structure represents a TREL peer info discovered using DNS-SD browse on the service name "_trel._udp" |
CotPskc | This structure represents PSKc |
CotRadioCoexMetrics | The following are valid radio state transitions: |
CotRadioFrame | This structure represents an IEEE 802.15.4 radio frame |
CotRadioIeInfo | This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame |
CotRadioLinkInfo | This type represents information associated with a radio link |
CotRouterInfo | This structure holds diagnostic information for a Thread Router |
CotSecurityPolicy | This structure represent Security Policy |
CotServerConfig | This structure represents a Server configuration |
CotServiceConfig | This structure represents a Service configuration |
CotSntpQuery | This structure implements SNTP Query parameters |
CotSockAddr | This structure represents an IPv6 socket address |
CotSrpClientBuffersServiceEntry | This struct represents a SRP client service pool entry |
CotSrpClientHostInfo | This structure represents an SRP client host info |
CotSrpClientService | This structure represents an SRP client service |
CotSrpServerLeaseConfig | This structure includes SRP server LEASE and KEY-LEASE configurations |
CotSrpServerLeaseInfo | This structure includes SRP server lease information of a host/service |
CotSrpServerResponseCounters | This structure includes the statistics of SRP server responses |
CotSrpServerTtlConfig | This structure includes SRP server TTL configurations |
CotSteeringData | This structure represents the steering data |
CotTcpCircularSendBuffer | This structure represents a circular send buffer for use with a TCP endpoint |
CotTcpEndpoint | This structure represents a TCP endpoint |
CotTcpEndpointInitializeArgs | This structure contains arguments to the otTcpEndpointInitialize() function |
CotTcpListener | This structure represents a TCP listener |
CotTcpListenerInitializeArgs | This structure contains arguments to the otTcpListenerInitialize() function |
CotThreadDiscoveryRequestInfo | This structure represents the Thread Discovery Request data |
CotThreadLinkInfo | This structure represents link-specific information for messages received from the Thread radio |
CotThreadParentResponseInfo | This structure represents the MLE Parent Response data |
CotTrelPeer | This struct represents a TREL peer |
CotUdpReceiver | This structure represents a UDP receiver |
CotUdpSocket | This structure represents a UDP socket |