RAIL SDK - Power Manager Sleep Component.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
Functions#
Initializes RAIL and Power Manager to work together in SYNC mode.
Function Documentation#
sl_rail_sdk_sleep_init#
RAIL_Status_t sl_rail_sdk_sleep_init (void )
Initializes RAIL and Power Manager to work together in SYNC mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function sets up the necessary configurations and prepares the RAIL SDK sleep module for operation. It should be called before using any other functions in the sleep module.
Returns
RAIL_Status_t
RAIL_STATUS_NO_ERROR if initialization was successful.
An appropriate error code otherwise.