This file contains the type definitions for EFR32xG2x chip-specific aspects of RAIL.
License#
Copyright 2020 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
Modules#
Macros#
SLI_LIBRARY_BUILD.
Time it takes to take care of protocol switching.
Indicates the number of 2.4 GHz RF Paths suppported.
Indicates the number of Sub-GHz RF Paths supported.
Indicates the number of RF Paths supported.
Indicates this version of RAIL supports IR calibration on multiple RF paths Needed for backwards compatibility.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_HP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_HP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_MP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_MP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_LP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_LP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_LLP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_2P4GIG_LLP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when using a Sub-GHz PA mode.
The minimum valid value for the RAIL_TxPowerLevel_t when using a Sub-GHz PA mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_HP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_HP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_MP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_MP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_LP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_LP mode.
The maximum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_LLP mode.
The minimum valid value for the RAIL_TxPowerLevel_t when in RAIL_TX_POWER_MODE_SUBGIG_LLP mode.
Backwards compatability define.
Backwards compatability define.
Backwards compatability define.
Backwards compatability define.
Backwards compatability define.
Backwards compatability define.
Backwards compatability define.
Backwards compatability define.
The number of PA's on this chip (including Virtual PAs).
Convenience macro for any mapping table mode.
Convenience macro to check if the power mode supports raw setting.
The static amount of memory needed per channel for channel hopping, measured in 32 bit words, regardless of the size of radio configuration structures.
Default PRS channel to use when configuring sleep.
Default RTCC channel to use when configuring sleep.
The minimum value for a consistent RAIL transition.
The maximum value for a consistent RAIL transition.