Wireless M-Bus Button Pulse Counter (Wireless M-Bus Meter Only)
License#
Copyright 2024 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
Functions#
Wireless M-Bus Pulse counter initialization function.
Wireless M-Bus Pulse counter deinitialization function.
Wireless M-Bus Pulse counter measure function.
Retrieves the sensor data for the Wireless M-Bus pulse counter sensor.
Wireless M-Bus Pulse counter 7 segment LCD print function.
Wireless M-Bus Pulse counter button pressed function.
Function Documentation#
sl_rail_sdk_wmbus_sensor_pulse_counter_init#
sl_status_t sl_rail_sdk_wmbus_sensor_pulse_counter_init (void )
Wireless M-Bus Pulse counter initialization function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sl_status_t: SL_STATUS_OK if init was successful SL_STATUS_FAIL if init failed
sl_rail_sdk_wmbus_sensor_pulse_counter_deinit#
sl_status_t sl_rail_sdk_wmbus_sensor_pulse_counter_deinit (void )
Wireless M-Bus Pulse counter deinitialization function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sl_status_t: SL_STATUS_OK if init was successful SL_STATUS_FAIL if init failed
sl_rail_sdk_wmbus_sensor_pulse_counter_measure#
sl_status_t sl_rail_sdk_wmbus_sensor_pulse_counter_measure (void )
Wireless M-Bus Pulse counter measure function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sl_status_t: SL_STATUS_OK if measure was successful SL_STATUS_FAIL if measure failed
sl_rail_sdk_wmbus_sensor_pulse_counter_get_data#
sl_rail_sdk_wmbus_sensor_data_t * sl_rail_sdk_wmbus_sensor_pulse_counter_get_data (void )
Retrieves the sensor data for the Wireless M-Bus pulse counter sensor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns a pointer to the sl_rail_sdk_wmbus_sensor_data_t structure that contains the sensor data for the Wireless M-Bus pulse counter sensor.
Returns
Pointer to a sl_rail_sdk_wmbus_sensor_data_t, the sensor data for the Wireless M-Bus pulse counter sensor
sl_rail_sdk_wmbus_sensor_pulse_counter_print#
sl_status_t sl_rail_sdk_wmbus_sensor_pulse_counter_print (void )
Wireless M-Bus Pulse counter 7 segment LCD print function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sl_status_t: SL_STATUS_OK if 7 segment LCD print was successfully SL_STATUS_FAIL if 7 segment LCD print failed
sl_rail_sdk_wmbus_sensor_pulse_counter_button_pressed
sl_status_t sl_rail_sdk_wmbus_sensor_pulse_counter_button_pressed (void )
Wireless M-Bus Pulse counter button pressed function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function handles the button press event for the Wireless M-Bus pulse counter, in this case, it increments the counter value.
Returns
sl_status_t: SL_STATUS_OK if button press was successfully SL_STATUS_FAIL if button press failed