RAIL Library Version 2.19.3 (February 18, 2026) - Release Notes#

Simplicity SDK Version 2025.6.3

Silicon Labs RAIL (Radio Abstraction Interface Layer) provides an intuitive and easily-customizable radio interface that is designed to support proprietary or standards-based wireless protocols.

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 2.19.3#

None.

Added in 2.19.2#

  • Added support for Concurrent listening feature on the SiXG301 part.

  • Added support for IEEE 802.15.4 High Data Rate (1 Mbps and 2 Mbps custom 802.15.4 SUN PHYs) on the SiXG301 part.

Added in 2.19.1#

None.

Added in 2.19.0#

  • Added support for Concurrent Listening in combination with IEEE 802.15.4 High Data Rate (1 Mbps and 2 Mbps custom 802.15.4 SUN PHYs) on the EFR32xG26 part.

  • Added support for the EFR32xG27 SiP Module.

  • Added support for storing Antenna calibrations like RSSI offset, PA mode, PA curves/tables in NVM3 on EFR32xG24 and EFR32xG26 parts.

API Changes#

Changed in 2.19.3#

None.

Changed in 2.19.2#

None.

Changed in 2.19.1#

None.

Changed in 2.19.0#

Added new APIs to store Antenna Calibrations in persistent NVM3 on EFR32xG24 and EFR32xG26 parts.

Bug Fixes#

Fixed in 2.19.3#

Minor Improvements.

Fixed in 2.19.2#

Minor Improvements.

Fixed in 2.19.1#

Minor Improvements.

Fixed in 2.19.0#

Minor Improvements.

Chip Enablement#

Added in 2.19.3#

None.

Added in 2.19.2#

Added support for new SiXG301 part.

Added in 2.19.1#

None.

Added in 2.19.0#

  • Added support for EFR32xG29 part.

  • Added support for EFR32xG22L part.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 2.19.3#

None.

Added in 2.19.2#

None.

Added in 2.19.1#

None.

Added in 2.19.0#

  • The rail_util_rssi component can now store and retrieve the chip RSSI offset from NVM3 persistent storage.

  • Added new component "RAIL Utility, NVM storage of PA configs and mode" component providing ability to store PA mode and/or PA curves/tables configs in persistent NVM3 on EFR32xG24 and EFR32xG26, overriding their compile-time configurations.

  • Added RAIL support for the MGM270SC32SNA2 module.

Enhancements#

None.

Removed Features#

None.

Deprecated Features#

Deprecated in 2.19.3#

None.

Deprecated in 2.19.2#

None.

Deprecated in 2.19.1#

None.

Deprecated in 2.19.0#

  • The RAIL 2.x API is planned for deprecation in the 2025.12.0 release (December 2025). At that time, the new RAIL 3.0 API will be released for all supported chips along with a RAIL 2.x compatibility layer and migration guide.

    • The goal of this new API is to get rid of some unused features, add better support for concurrent listening use cases, and to simplify channel and PA configurations.

    • The migration is intended to be straight forward and simple for the majority of customers. However, in some cases manual help might be required to ease this transition.

  • Note: RAIL 3.0 API is in evaluation in sl_rail_*.h files, though subject to change, and the RAIL library has RAIL 3.0 symbols alongside RAIL 2.x, with some stacks and RAIL apps having started to use it in 2025.6.0.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 2.19.3#

None.

Added in 2.19.2#

None.

Added in 2.19.1#

None.

Added in 2.19.0#

New API Signature

Deprecated API replaced by this (if any)

sl_status_t sl_rail_util_pa_nvm_read_config(sl_rail_nvm_pa_config_t *p_pa_config)

None.

RAIL_TxPowerMode_t sl_rail_util_pa_nvm_read_mode(void)

None.

sl_status_t sl_rail_util_pa_nvm_write_config(const sl_rail_nvm_pa_config_t *p_pa_config)

None.

sl_status_t sl_rail_util_pa_nvm_write_mode(RAIL_TxPowerMode_t pa_mode)

None.

Modified APIs#

Added in 2.19.3#

None.

Added in 2.19.2#

None.

Added in 2.19.1#

None.

Added in 2.19.0#

Old API

Modified

RAIL_Status_t RAIL_ZWAVE_ConfigBeamRx(RAIL_Handle_t railHandle, RAIL_ZWAVE_BeamRxConfig_t *config)

RAIL_Status_t RAIL_ZWAVE_ConfigBeamRx(RAIL_Handle_t railHandle, const RAIL_ZWAVE_BeamRxConfig_t *config)

RAIL_Status_t RAIL_ZWAVE_SetTxLowPowerDbm(RAIL_Handle_t railHandle, RAIL_TxPower_t powerLevel)

RAIL_Status_t RAIL_ZWAVE_SetTxLowPowerDbm(RAIL_Handle_t railHandle, RAIL_TxPower_t power)

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 2.19.3#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1499282 Fixed an issue where RAIL could hang in its idle code path when switching from the IEEE 802.15.4 High Data Rate (HDR) PHY to the normal 802.15.4 PHY.
    None.
    All chips
1524998 Fixed an issue with Concurrent RX Channel Switching on EFR32xG2x platforms which could cause transmit to lock up and never complete.
    00333649
    All EFR32xG2x parts
1530983 Fixed an issue with BLE on EFR32xG27 and EFR32xG29 where RX overflow could render the protocol deaf.
    None.
  • EFR32xG27
  • EFR32xG29
1565641 Eliminated a race condition on the SixG301 part where Fast Channel Switching could impact CSMA transmits.
    00335449
    SixG301
1569271 Fixed an issue on the SixG301 part where RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND was not generated for the IEEE 802.15.4 stack when Fast Channel Switching is enabled.
    00335936
    SixG301

Fixed in 2.19.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1473541 Fixed an issue with RAIL_BLE_PhySimulscan that could break BLE 1 Mbps transmit on EFR32xG24 and EFR32xG26 parts.
    None.
  • EFR32xG24
  • EFR32xG26
1503811 Fixed an issue introduced in 2.19.1 which caused applications using the Coexistence directional priority feature to fail to compile on EFR32xGxx parts. This feature is not yet supported on the SiXG301 part.
    None.
    All chips
1509674 Fixed an assert issue on the MGM260PB22VNA module when running BLE applications.
    00332448
    MGM260PB22VNA

Fixed in 2.19.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1455258 Fixed a BLE scan response timing issue that could affect BLE-related applications on the 20dBm EFR32xG21 devices interacting with non Silabs devices.
  • 00327420
  • 00330083
    EFR32xG21
1473957 Updated the quality of the RAIL Utility, IEEE802.15.4 Fast Channel Switching Configuration component to Production. None.
    EFR32xG26
1476867 Fixed an issue where BGM260PB32VNA module failed to build due to incorrect signatures. None.
  • EFR32xG26
  • BGM260PB32VNA

Fixed in 2.19.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1274214 Fixed an issue on EFR32xG23, EFR32xG25, EFR32xG26 and EFR32xG28 where radio was blocked in RAIL_RF_STATE_RX_ACTIVE. None.
  • EFR32xG23
  • EFR32xG25
  • EFR32xG26
  • EFR32xG28
1355305 Fixed an issue where the events RAIL_EVENT_RX_PREAMBLE_DETECT, RAIL_EVENT_RX_PREAMBLE_LOST and RAIL_EVENT_RX_SYNC1_DETECT were not generated for WiSUN OQPSK PHYs on the EFR32xG25 part. None.
    EFR32xG25
1357024 Fixed a false CCA busy issue on the EFR32xG28 part. None.
    EFR32xG28
1426472 Fixed an issue were PTI was only partially disabled when configured with RAIL_PTI_MODE_DISABLED (which is RAIL's default), and accordingly clarified RAIL_ConfigPti() and RAIL_EnablePti() documentation. None.
    All chips
1435514 Fixed an issue on the EFR32xG24, where enabling channel sounding under certain conditions can potentially result in hanging the system in the default handler. None.
    EFR32xG24
1437972 Fixed an issue on the EFR32xG24, where the RSSI reported on certain channel sounding SYNC packets could be lower than expected. None.
    EFR32xG24
1439816 Fixed an issue with Wi-SUN mode switch where idling the radio after RAIL_EVENT_IEEE802154_MODESWITCH_START can prevent reception of future mode switch headers. None.
    Unknown
1445964 Fixed an issue in RAIL_GetRxPacketDetails() where the duration of the packet would be incorrect when packet size is larger than 534 bytes on the EFR32xG25 part. None.
    EFR32xG25
1450906 Fixed an issue on the EFR32xG24, where CS antenna switching would not work when configured for GPIOs on PortC or PortD. None.
    EFR32xG24

Chip Enablement#

Added in 2.19.3#

None.

Added in 2.19.2#

Chip Family OPNs / Boards / OPN Combinations Supported Software Variants (if applicable) Supported Modes Supported Host Interfaces
SiXG301 Not Applicable Not Applicable Not Applicable Not Applicable

Added in 2.19.1#

None.

Added in 2.19.0#

Chip Family OPNs / Boards / OPN Combinations Supported Software Variants (if applicable) Supported Modes Supported Host Interfaces
EFR32xG29 Not Applicable Not Applicable Not Applicable Not Applicable
EFR32xG22L Not Applicable Not Applicable Not Applicable Not Applicable
EFR32xG27 MGM270SC32SNA2 Not Applicable Not Applicable Not Applicable

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1465156 Excessively long Rx2Tx turnaround time reported on EFR32xG25 after hours of network stack test. Issue has been seen after CCA. Turnaround time increases by jump over time and has been observed at 10x its nominal value. None. None. EFR32xG25
1458845 When running Channel Sounding RTT with a non-BG24 CS device, RTT has an error of +/- 12.5 ns depending on CS role. Precision is not affected. BG24 to BG24 RTT is not affected. None. None.
  • non-BG24 CS devices
  • Channel Sounding RTT
641705 Infinite receive operations where the frame's fixed length is set to 0 are not working correctly on the EFR32xG23 series chips. Not Applicable Not Applicable EFR32xG23 series chips
732659 Wi-SUN FSK mode 1a exhibits a PER floor with frequency offsets around ± 8 to 10 KHz Wi-SUN FSK mode 1b exhibits a PER floor with frequency offsets around ± 18 to 20 KHz. Not Applicable Not Applicable EFR32xG23 series chips

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Migration Guide#

None.

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

RAIL Library packages and plugins.

Compatible Software#

None.

Installation and Use#

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

Help and Feedback#

Unsupported Features#

None.

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.