RAILtest User Guide#

Note: This section replaces UG409: RAILtest User Guide. Further updates to this user guide note will be provided here.

The RAILtest application (RAILtest) provides you with a simple tool for testing the radio and the functionality of the RAIL library. For more advanced usage, developers must write software against the RAIL library and create a custom radio configuration.

Proprietary is supported on all EFR32FG devices. For others, check the device's data sheet under Ordering Information > Protocol Stack to see if Proprietary is supported. In Proprietary SDK version 2.7.n, Connect is not supported on EFR32xG22.

Key Points#

  • Command Line Interface description

  • Application features

  • Protocol-specific features

  • Testing modes