Edit

Debugging#

EFR32 Wireless Geckos, like any modern MCU, supports on-chip debugging. However, when debugging radio problems, on-chip debugging is often inadequate. Generally, the problem is that some bugs originate from the real time nature of the radio. When stopping the radio at a breakpoint, you change the behavior of the target. Also, you might need information from multiple targets at the same time. In this article, we recommend RAIL/EFR32 debug techniques for these problems as well as other RAIL-specific debug features.

RAILtest#

While the original goal for RAILtest was to test the RAIL library, it can be a useful tool for software development as well. In most cases, you probably want to concentrate on either receiving or transmitting, and need something to play the role of the other side. RAILtest can be simply used for that. Just set up the desired config, and it will immediately start in receive mode, printing the received messages with timestamps (useful for checking synchronized transmits). It doesn't just print; it has a command line interface to change almost anything in RAIL. Some of the most useful commands for testing:

  • rx 0 turns off the radio, while rx 1 reenables it in receive mode

  • tx <N> sends N message or if N=0, it will send messages until you call tx 0 again

  • settxdelay <N> changes the delay between transmitted packets

  • setchannel <N> changes the channel to N

  • setconfigindex <N> will change the radio config to the given number in a multi-PHY setup

  • status prints a statistics (e.g., number of received packets) since the device booted

  • resetcounters zeroes out the statistics for the status command

  • setrxoption 3 can be used to disable CRC check while setrxoptions 0 reenables it

  • setfixedlength <N> sets the configured packet length to N, for both Tx and Rx, even if the radio config is variable length

  • settxpayload can change the packet RAILtest transmits. The first parameter is the offset and all following parameters will be written continuously

  • settxlength <N> changes how many bytes will be written into the Tx FIFO before transmission (note that it does not actually change the transmitted length)

  • settxtransitions and setrxtransitions can be used to configure automatic state transitions. Do disable going back to Rx, call it both with the argument i i (i as idle)

  • settxtone 1 transmits an unmodulated carrier on the channel until settxtone 0 is called

  • getrssi prints out the current RSSI measured on the antenna

  • startavgrssi <N> measures RSSI for N µs

  • settxstream can be used to transmit various periodic modulated signal, including PN9 pseudorandom and '01' pattern

  • setgpiooutpin can be used to drive a pin low or high, e.g., to drive an external PA. For example, setgpiooutpin C 3 0 will drive portC3 down

  • setdebugsignal outputs an internal debug signal to GPIO, this is discussed in detail below

  • reset resets the part

For further details, refer to RAILtest User's Guide.

Debugging with SWD#

EFR32 provides SWD as the debug interface. You can use breakpoints and read register values when the MCU is halted, just like any other EFM32. However, you should be careful when using this tool for debugging the radio.

Keep in mind that the radio is fast; if you put a breakpoint to the RAIL event handler, you can stop the MCU while it's receiving/transmitting a packet, which could result in bugs that normally wouldn't happen, e.g., the timestamps could be completely wrong, or you can run into buffer overflow/buffer underflow events.

You could also see some strange phenomena when debugging the radio; that is, you might see that the values stored in the memory have changed, even though the MCU is halted. That is caused by the radio co-processor of EFR32 (sometimes called sequencer), which is used to help with time-critical event handling of the radio, and shares some memory with the main MCU.

Generally, we would recommend not putting breakpoints into the RAIL event handler (of course, it is fine to do it if you don't care about execution after the breakpoint); set temporary flags instead and stop the application in the main loop when it's safe to check the values. Another good technique is to put past events into a queue:

volatile sl_rail_events_t event_queue[5];

void sl_rail_util_on_event(sl_rail_handle_t rail_handle, sl_rail_events_t events)
{
  // Handle events
  for(int i=1;i<5;i++){
    event_queue[i-1] = event_queue[i];
  }
  event_queue[4] = events;
}

This helps a lot to figure out the flow that resulted in the problem you're debugging.

Assertion#

RAIL provides an assertion mechanism. For example, if you try to set a channel on a frequency that is not available from the radio configuration, you'll get a SL_RAIL_ASSERT_FAILED_SYNTH_VCO_FREQUENCY assert. If RAIL Utility, Callbacks component is installed, these assert will be printed to stdout by default. You can catch these asserts by overriding sl_rail_util_on_assert_failed weak function.

It's a good idea to stop normal operation on assert - in a production application, you probably want to reset from it. If you put a breakpoint in sl_rail_util_on_assert_failed, you can also see the callstack of the assert, where you might not understand all levels (as part of it is probably in the closed source library), but at least you can see the original source of the assert.

Note that if nothing implements sl_rail_util_on_assert_failed, it defaults to the rail-lib implementation, which is an infinite loop. Unless you have a watchdog, this can be harmful in production.

Debugging with GPIOs and PRS Channels#

You probably already used this technique to debug time-critical problems: toggle a GPIO when something happens, and use a logic analyzer or an oscilloscope to analyze it. EFR32 can help further with radio specific PRS (Peripheral Reflex System) channels that are wired to GPIOs. If a GPIO is configured for a given PRS signal, it will go high when the signal is active; i.e., if you configure PRS_RAC_TX to a GPIO, the signal will be high during transmission. You can find a list of the available radio PRS signals below.

PRS signals can be extremely useful when working on multiple devices:

Logic Analyzer Snapshot of
PRSLogic Analyzer Snapshot of
PRS

In the logic analyzer capture above (of a PRS-modified duty cycle example), you can see that device 2 starts transmitting, and how device 1 locks on that signal.

PRS signals also can be used to measure state transition times, which is often important in time-critical applications. Note, however, that even though the RXSTATE signal is driven high, the radio and RAIL could still need some time to complete the state transition, so it might be possible that you can't detect a signal at the beginning of the Rx window, or you're already leaving Rx mode when an event is triggered, making it useless. The magnitude of this error however is small only a few µs.

Setting up PRS Signals with PRS Debug Signal Support Component#

Simplicity Studio 6's PRS Debug Signal Support (in earlier SDKs, Flex - RAIL PRS Support) component offers an easy way to set up the radio PRS signals. After installing the component, you can create multiple component instances. Each instance corresponds to a PRS signal where you can select the PRS signal source and the output pin. In the picture below, we created an instance named dout and we set Modem data out to pin PC09. (Before configuring the pin, check the pin tool, datasheet, and schematic to ensure it does not conflict with other assigned functions.)

RAIL PRS Support component
instanceRAIL PRS Support component
instance

Note that while this article is intended for proprietary developers, the above component and the radio PRS debug signal system is available with any stack. The only possible caveat is that some PRS channels might be used with certain stacks. E.g., PRS channel 7 is usually used for RAIL timer synchronization.

Setting up PRS Signals Without PRS Debug Signal Support Component#

It can be also useful to set up the PRS signals directly from the source code. The implementation is different for the device generations.

For Series 1:

#include "em_cmu.h"
#include "em_prs.h"

// Useful Pins that work on most boards
// Pin,  Ch, Loc, Board gen     (conflict)  WSTK_P?     EXP_HEADER?
// PC10,  9,  15  Series1       (I2C)       WSTK_P12    EXP_HEADER15
// PC11, 10,   5  Series1       (I2C)       WSTK_P13    EXP_HEADER16
// PF02,  0,   2  xG1/xG13/xG14 (SWO)       WSTK_P28
// PF03,  1,   2  xG1/xG13/xG14 (TDI)       WSTK_P10    EXP_HEADER13
// PF04,  2,   2  xG1/xG13/xG14 (LED0)      WSTK_P8     EXP_HEADER11
// PF05,  3,   2  xG1/xG13/xG14 (LED1)      WSTK_P32
// PF06,  0,   6  xG1/xG13/xG14 (BTN0)      WSTK_P34
// PF07,  1,   6  xG1/xG13/xG14 (BTN1)      WSTK_P36
// PC09, 11,   2  xG12                      WSTK_P10    EXP_HEADER13
// PD09,  3,   8  xG12                      WSTK_P02    EXP_HEADER05
// PD10,  4,   1  xG12                      WSTK_P04    EXP_HEADER07
// PD11,  5,   1  xG12                      WSTK_P06    EXP_HEADER09
// PD12,  6,  14  xG12                      WSTK_P08    EXP_HEADER11

// Set PRS_RAC_TX to PC10
// EXP15: PC10, Ch9, Loc15
CMU_ClockEnable(cmuClock_PRS, true);
CMU_ClockEnable(cmuClock_GPIO, true);
GPIO_PinModeSet(gpioPortC, 10, gpioModePushPull, 0);
PRS_ConnectSignal(9, prsTypeAsync, PRS_RAC_TX);
PRS_GpioOutputLocation(9, 15);

For Series 2:

#include "em_cmu.h"
#include "em_prs.h"

// PRS Channel 0-5 can be routed to port A/B and Channel 6-11 to port C/D
// Set PRS_RACL_TX to PC04
CMU_ClockEnable(cmuClock_PRS, true);
CMU_ClockEnable(cmuClock_GPIO, true);
PRS_ConnectSignal(8, prsTypeAsync, PRS_RACL_TX);
PRS_PinOutput(8, prsTypeAsync, gpioPortC, 4);
GPIO_PinModeSet(gpioPortC, 4, gpioModePushPull, 0);

Setting up PRS Signals with RAILtest#

In RAILtest, you can set up the PRS signals using the setDebugSignal serial command. For example, to route TXACTIVE to pin PC11 use:

setDebugSignal PC11 TXACTIVE

You can use setDebugSignal help me to list available GPIOs and signals.

Radio PRS Signals#

For Series1:

Signal

RAILtest name

Summary

PRS_RAC_ACTIVE

RACACTIVE

Radio enabled

PRS_RAC_TX

TXACTIVE

Transmit mode enabled

PRS_RAC_RX

RXACTIVE

Receive mode enabled

PRS_RAC_LNAEN

LNAEN

LNA enabled for RX

PRS_RAC_PAEN

PAEN

PA enabled for TX

PRS_MODEM_FRAMEDET

FRAMEDETECT

Frame detected (Syncword received)

PRS_MODEM_PREDET

PREAMBLEDETECT

Preamble detected

PRS_MODEM_TIMDET

TIMINGDETECT

Timing detected

PRS_MODEM_FRAMESENT

FRAMESENT

Frame sent

PRS_MODEM_SYNCSENT

SYNCSENT

Syncword sent

PRS_MODEM_PRESENT

N/A

Preamble sent

PRS_MODEM_PRESENT+1

CUSTOM_PRS 0x56 0x6

Modem clock out

PRS_MODEM_PRESENT+2

CUSTOM_PRS 0x56 0x7

Modem data out

For Series2:

Signal

RAILtest name

Summary

PRS_RACL_ACTIVE

RACACTIVE

Radio enabled

PRS_RACL_TX

TXACTIVE

Transmit mode enabled

PRS_RACL_RX

RXACTIVE

Receive mode enabled

PRS_RACL_LNAEN

LNAEN

LNA enabled for Rx

PRS_RACL_PAEN

PAEN

PA enabled for Tx

PRS_MODEML_FRAMEDET

FRAMEDETECT

Frame detected (Syncword received)

PRS_MODEM_PREDET

PREAMBLEDETECT

Preamble detected

PRS_MODEMH_TIMDET

TIMINGDETECT

Timing detected (not valid for most PHYs)

PRS_MODEM_FRAMESENT

FRAMESENT

Frame sent

PRS_MODEMH_SYNCSENT

SYNCSENT

Syncword sent

OFDMFRAMEDETECT_PRSMUXLSB

OFDMFRAMEDETECT

OFDM Frame detected (Syncword received)

OFDMEOF_PRSMUXLSB

OFDMEOF

OFDM End of Frame

OFDMFRAMESENT_PRSMUXLSB

OFDMFRAMESENT

OFDM Frame sent

OFDMSYNCSENT_PRSMUXLSB

OFDMSYNCSENT

OFDM Syncword sent

OFDMSYMBOLCLK_PRSMUXLSB

OFDMSYMBOLCLK

OFDM Symbol clock out

PRS_MODEMH_PRESENT

N/A

Preamble sent

PRS_MODEML_DCLK

CUSTOM_PRS 0x56 0x5

Modem clock out

PRS_MODEML_DOUT

CUSTOM_PRS 0x56 0x6

Modem data out

The last two signals are direct outputs of the modem (just before modulation for Tx and after demodulation for RX). On Series 1 devices, they don't have proper names, so the recommended way to access them is to increment PRS_MODEM_PRESENT. If you are working with RAILtest, they can be accessed as custom PRS. In this case, instead of 0x56, use:

  • 0x26 on xG1,

  • 0x56 on xG12-xG14,

  • 0x2B on xG21,

  • 0x2A on xG22,

  • 0x29 on xG23 and newer

Note that especially on Series 2 devices, some debug signals might not work as expected, or even meaningless. PRS_MODEML_DOUT for example behaves differently on rx depending on the radio config while PRS_MODEMH_TIMDET also depends on the PHY but in most cases its behavior is undefined. For software debugging however, these signals are rarely needed.