RAIL_AntennaConfig_t Struct Reference

A configuration for antenna selection.

#include <rail_chip_specific.h>

Data Fields

bool ant0PinEn
 MODEM_ROUTEPEN fields.
 
bool ant1PinEn
 Antenna 1 Pin Enable.
 
uint8_t ant0Loc
 MODEM_ROUTELOC1 fields.
 
GPIO_Port_TypeDef ant0Port
 Antenna 0 output GPIO port.
 
uint8_t ant0Pin
 Antenna 0 output GPIO pin.
 
uint8_t ant1Loc
 Antenna 1 location for pin/port.
 
GPIO_Port_TypeDef ant1Port
 Antenna 1 output GPIO port.
 
uint8_t ant1Pin
 Antenna 1 output GPIO pin.

A configuration for antenna selection.

Definition at line 653 of file rail_chip_specific.h.

Field Documentation

uint8_t RAIL_AntennaConfig_t::ant0Loc

MODEM_ROUTELOC1 fields.

Antenna 0 location for pin/port

Definition at line 661 of file rail_chip_specific.h.

bool RAIL_AntennaConfig_t::ant0PinEn

MODEM_ROUTEPEN fields.

Antenna 0 Pin Enable

Definition at line 656 of file rail_chip_specific.h.


The documentation for this struct was generated from the following file:
  • chip/efr32/efr32xg1x/rail_chip_specific.h