RAIL_RfSenseSelectiveOokConfig_t Struct Reference

Structure to configure RFSENSE Selective(OOK) mode.

#include <rail_types.h>

Data Fields

RAIL_RfSenseBand_t band
 The frequency band(s) on which to sense the RF energy.
 
uint8_t syncWordNumBytes
 Syncword Length in bytes, 1-4 bytes.
 
uint32_t syncWord
 Sync Word Value.
 
RAIL_RfSense_CallbackPtr_t cb
 The callback function, called when RF is sensed.

Structure to configure RFSENSE Selective(OOK) mode.

Definition at line 2915 of file rail_types.h.

Field Documentation

◆ band

RAIL_RfSenseBand_t RAIL_RfSenseSelectiveOokConfig_t::band

The frequency band(s) on which to sense the RF energy.

To stop RF Sense, specify RAIL_RFSENSE_OFF.

Definition at line 2920 of file rail_types.h.

◆ syncWord

uint32_t RAIL_RfSenseSelectiveOokConfig_t::syncWord

Sync Word Value.

To use HW default sync word, set to RAIL_RFSENSE_USE_HW_SYNCWORD.

Definition at line 2932 of file rail_types.h.

◆ syncWordNumBytes

uint8_t RAIL_RfSenseSelectiveOokConfig_t::syncWordNumBytes

Syncword Length in bytes, 1-4 bytes.

Note
When syncWord is set to use RAIL_RFSENSE_USE_HW_SYNCWORD, the syncWordNumBytes value will be ignored since we rely on the HW default settings for sync word.

Definition at line 2927 of file rail_types.h.


The documentation for this struct was generated from the following file:
  • common/rail_types.h