RAIL_ScheduleTxConfig_t Struct Reference

A configuration structure for a scheduled transmit.

#include <rail_types.h>

Data Fields

RAIL_Time_t when
 The time when to transmit this packet.
 
RAIL_TimeMode_t mode
 The type of delay.
 
RAIL_ScheduledTxDuringRx_t txDuringRx
 Indicates which action to take with a scheduled TX if it occurs during RX.

A configuration structure for a scheduled transmit.

Definition at line 1723 of file rail_types.h.

Field Documentation

RAIL_TimeMode_t RAIL_ScheduleTxConfig_t::mode

The type of delay.

See the RAIL_TimeMode_t documentation for more information. Be sure to use RAIL_TIME_ABSOLUTE delays for time-critical protocols.

Definition at line 1734 of file rail_types.h.

RAIL_ScheduledTxDuringRx_t RAIL_ScheduleTxConfig_t::txDuringRx

Indicates which action to take with a scheduled TX if it occurs during RX.

See RAIL_ScheduledTxDuringRx_t structure for more information on potential options.

Definition at line 1740 of file rail_types.h.

RAIL_Time_t RAIL_ScheduleTxConfig_t::when

The time when to transmit this packet.

The exact interpretation of this value depends on the mode specified below.

Definition at line 1728 of file rail_types.h.


The documentation for this struct was generated from the following file:
  • common/rail_types.h